<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: SPI slave mode receive register settings</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/SPI-slave-mode-receive-register-settings/m-p/235332#M482</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now, I can see the received characters in RX FIFO with these settings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;SPI0_MCR &amp;amp;= ~SPI_MCR_MDIS_MASK;&lt;/TD&gt;&lt;TD&gt;// Disable the module&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;SPI0_MCR =&amp;nbsp; SPI_MCR_HALT_MASK| SPI_MCR_DOCNF_MASK // stop SPI&lt;/P&gt;&lt;P&gt;SPI0_RSER = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // disable interrupts&lt;/P&gt;&lt;P&gt;SPI0_RSER|= SPI_RSER_RFDF_RE_MASK;&amp;nbsp;&amp;nbsp; // Enable SPI receive int.&lt;/P&gt;&lt;P&gt;SPI0_SR =&amp;nbsp; SPI_SR_EOQF_MASK|SPI_SR_TFUF_MASK|SPI_SR_TFFF_MASK|SPI_SR_RFOF_MASK|SPI_SR_RFDF_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see the correct values when I connect the SIN pin to either 3.3V or GND in RX FIFO. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I initialized the DMA without error with following codes:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA0_ERQ = DMA_ERQ_ERQ1_MASK; //channel 2&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMAMUX1_CHCFG1 = DMAMUX_CHCFG_ENBL_MASK&lt;/P&gt;&lt;P&gt;&amp;nbsp; |DMAMUX_CHCFG_SOURCE(12) ; //Source 12 for SPI0 Rx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_SADDR = (uint32_t)&amp;amp;SPI0_POPR; /* Set the Source Address */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Destination address */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_DADDR = (uint32_t)(&amp;amp;dmaBuffer );&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Source offset disabled */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_SOFF = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Source and Destination Modulo off, source and destination size 2 = 32 bits */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_ATTR = DMA_ATTR_SMOD(0)|DMA_ATTR_SSIZE(2) | DMA_ATTR_DMOD(0)|DMA_ATTR_DSIZE(2);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Transfer 4 bytes per transaction */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_NBYTES_MLNO = 4; // 16 bytes?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* No adjust needed */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_SLAST = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Destination offset disabled */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_DOFF = 4;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* No link channel to channel, 1 transaction */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_CITER_ELINKNO = DMA_CITER_ELINKNO_CITER(16);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* No adjustment to destination address */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_DLASTSGA = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_BITER_ELINKNO = DMA_BITER_ELINKNO_BITER(16);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_CSR = DMA_CSR_DREQ_MASK|DMA_CSR_START_MASK; //One transfer only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I can not see anything in dmaBuffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 22 Feb 2014 10:59:40 GMT</pubDate>
    <dc:creator>MehmetAliIpin</dc:creator>
    <dc:date>2014-02-22T10:59:40Z</dc:date>
    <item>
      <title>SPI slave mode receive register settings</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SPI-slave-mode-receive-register-settings/m-p/235331#M481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir/Madam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to implement a SPI slave mode data reception from a SPI master for Vybrid VF3x. Since MQX does not support slave mode, I have to written the following SPI0_MCR and SPI0_CTAR register settings.&lt;/P&gt;&lt;P&gt;Of course, I tested it, but did not see any character in SPI0_POP register, or an error flag, or an interrupt flag is set. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can send characters either DMA or SPI in master mode, but I can not receive in slave mode.&lt;/P&gt;&lt;P&gt;I have added my code segment below, I would be grateful, if you have a look and check if something is wrong or some extra registers are also controlled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With my best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mehmet Ali Ipin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;SPI0_MCR &amp;amp;= ~SPI_MCR_MDIS_MASK;&lt;/TD&gt;&lt;TD&gt;// Disable the module to change some bits..&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;#ifdef SPI_SLAVE_MODE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;SPI0_MCR =&amp;nbsp; SPI_MCR_HALT_MASK&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_CLR_RXF_MASK&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_CLR_TXF_MASK&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_PCSIS(1)&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;//CS0 inactive state = high;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_ROOE_MASK&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;// Enable shift registers&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_DCONF_MASK;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#else&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;SPI0_MCR = SPI_MCR_MSTR_MASK&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_HALT_MASK&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_CLR_RXF_MASK&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_CLR_TXF_MASK&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_PCSIS(1)&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;//CS0 inactive state = high;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_ROOE_MASK&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;// Enable shift registers&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_MCR_DCONF_MASK;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;SPI0_MCR |= SPI_MCR_MDIS_MASK;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;SPI0_CTAR0 = SPI_CTAR_FMSZ(7)&lt;/TD&gt;&lt;TD&gt;// 8 bit data will be received/transferred&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_CTAR_DBR_MASK&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_CTAR_PDT(7)&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_CTAR_BR(2)&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_CTAR_CPHA_MASK&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; |SPI_CTAR_CPOL_MASK;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 09:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SPI-slave-mode-receive-register-settings/m-p/235331#M481</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2014-02-14T09:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: SPI slave mode receive register settings</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SPI-slave-mode-receive-register-settings/m-p/235332#M482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now, I can see the received characters in RX FIFO with these settings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;SPI0_MCR &amp;amp;= ~SPI_MCR_MDIS_MASK;&lt;/TD&gt;&lt;TD&gt;// Disable the module&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;SPI0_MCR =&amp;nbsp; SPI_MCR_HALT_MASK| SPI_MCR_DOCNF_MASK // stop SPI&lt;/P&gt;&lt;P&gt;SPI0_RSER = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // disable interrupts&lt;/P&gt;&lt;P&gt;SPI0_RSER|= SPI_RSER_RFDF_RE_MASK;&amp;nbsp;&amp;nbsp; // Enable SPI receive int.&lt;/P&gt;&lt;P&gt;SPI0_SR =&amp;nbsp; SPI_SR_EOQF_MASK|SPI_SR_TFUF_MASK|SPI_SR_TFFF_MASK|SPI_SR_RFOF_MASK|SPI_SR_RFDF_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see the correct values when I connect the SIN pin to either 3.3V or GND in RX FIFO. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I initialized the DMA without error with following codes:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA0_ERQ = DMA_ERQ_ERQ1_MASK; //channel 2&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMAMUX1_CHCFG1 = DMAMUX_CHCFG_ENBL_MASK&lt;/P&gt;&lt;P&gt;&amp;nbsp; |DMAMUX_CHCFG_SOURCE(12) ; //Source 12 for SPI0 Rx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_SADDR = (uint32_t)&amp;amp;SPI0_POPR; /* Set the Source Address */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Destination address */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_DADDR = (uint32_t)(&amp;amp;dmaBuffer );&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Source offset disabled */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_SOFF = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Source and Destination Modulo off, source and destination size 2 = 32 bits */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_ATTR = DMA_ATTR_SMOD(0)|DMA_ATTR_SSIZE(2) | DMA_ATTR_DMOD(0)|DMA_ATTR_DSIZE(2);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Transfer 4 bytes per transaction */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_NBYTES_MLNO = 4; // 16 bytes?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* No adjust needed */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_SLAST = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Destination offset disabled */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_DOFF = 4;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* No link channel to channel, 1 transaction */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_CITER_ELINKNO = DMA_CITER_ELINKNO_CITER(16);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* No adjustment to destination address */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_DLASTSGA = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_BITER_ELINKNO = DMA_BITER_ELINKNO_BITER(16);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA0_TCD1_CSR = DMA_CSR_DREQ_MASK|DMA_CSR_START_MASK; //One transfer only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I can not see anything in dmaBuffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Feb 2014 10:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SPI-slave-mode-receive-register-settings/m-p/235332#M482</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2014-02-22T10:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: Re: SPI slave mode receive register settings</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SPI-slave-mode-receive-register-settings/m-p/235333#M483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can check the code in MQX regarding the DMA or also check the files attached. They are not granted to work but it can work as reference for you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Mar 2014 20:20:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SPI-slave-mode-receive-register-settings/m-p/235333#M483</guid>
      <dc:creator>juangutierrez</dc:creator>
      <dc:date>2014-03-06T20:20:12Z</dc:date>
    </item>
  </channel>
</rss>