<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: SDR mode and DDR mode switch.</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/SDR-mode-and-DDR-mode-switch/m-p/436119#M4818</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DDR Mode is enabled by setting the QSPI_MCR[DDR_EN].&lt;/P&gt;&lt;P&gt;The sampling register (QSPI_SMPR) should also be configured. When the serial flashes function in DDR mode the time for which the data is actually valid is smaller than half a clock cycle, it requires that we provide closely spaced sampling points. &lt;/P&gt;&lt;P&gt;Note that some flash vendors provide the DQS signal to which the read data is aligned in DDR mode (Spansion for example). When the DQS signal is used, the&amp;nbsp; QSPI_MCR[DQS_EN] must be set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 May 2015 04:42:11 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2015-05-22T04:42:11Z</dc:date>
    <item>
      <title>SDR mode and DDR mode switch.</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDR-mode-and-DDR-mode-switch/m-p/436118#M4817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;VYBRIDRSERIESEC_Rev_7.PDF&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;p58&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;9.5.1&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;QuadSPI&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;timing&lt;/SPAN&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;description of &lt;/SPAN&gt;&lt;SPAN&gt;"SDR&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;mode&lt;/SPAN&gt;&lt;SPAN&gt;"or"&lt;/SPAN&gt;&lt;SPAN&gt;DDR&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;mode"&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;but&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;QSPIFlashROM&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;by&lt;/SPAN&gt;&lt;SPAN&gt; the &lt;/SPAN&gt;&lt;SPAN&gt;command&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;switches&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;DDR&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;and&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;SDR&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="hps"&gt;This&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;sheet &lt;/SPAN&gt;&lt;SPAN class="hps"&gt;described in the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;"SDR mode", "DDR mode"&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;is&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;bit7&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;QuadSPI0_MCR&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;register&lt;/SPAN&gt;: &lt;SPAN class="hps"&gt;will&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;be&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;set&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;to "1"&lt;/SPAN&gt;&amp;nbsp; of &lt;SPAN class="hps"&gt;DDR_EN?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;Or&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;refers&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;to&lt;/SPAN&gt;&lt;SPAN&gt; the &lt;/SPAN&gt;&lt;SPAN&gt;mode&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;of&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;behavior&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;when&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;using&lt;/SPAN&gt;&lt;SPAN&gt; the &lt;/SPAN&gt;&lt;SPAN&gt;DDRRead/Write&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;command&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;and&lt;/SPAN&gt;&lt;SPAN&gt; the &lt;/SPAN&gt;&lt;SPAN&gt;SDRRead/Write&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;command&lt;/SPAN&gt;&lt;SPAN&gt;?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2015 09:16:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDR-mode-and-DDR-mode-switch/m-p/436118#M4817</guid>
      <dc:creator>takashitakahash</dc:creator>
      <dc:date>2015-05-15T09:16:37Z</dc:date>
    </item>
    <item>
      <title>Re: SDR mode and DDR mode switch.</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDR-mode-and-DDR-mode-switch/m-p/436119#M4818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DDR Mode is enabled by setting the QSPI_MCR[DDR_EN].&lt;/P&gt;&lt;P&gt;The sampling register (QSPI_SMPR) should also be configured. When the serial flashes function in DDR mode the time for which the data is actually valid is smaller than half a clock cycle, it requires that we provide closely spaced sampling points. &lt;/P&gt;&lt;P&gt;Note that some flash vendors provide the DQS signal to which the read data is aligned in DDR mode (Spansion for example). When the DQS signal is used, the&amp;nbsp; QSPI_MCR[DQS_EN] must be set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2015 04:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDR-mode-and-DDR-mode-switch/m-p/436119#M4818</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2015-05-22T04:42:11Z</dc:date>
    </item>
  </channel>
</rss>