<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: Adding delay to Vybrid Quad SPI boot</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Adding-delay-to-Vybrid-Quad-SPI-boot/m-p/429525#M4779</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jefy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To clarify - this is not a Linux system running, but a bare-metal application flashed, booted, and copied from QSPI to DDR and executed to run?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jun 2015 14:23:11 GMT</pubDate>
    <dc:creator>timesyssupport</dc:creator>
    <dc:date>2015-06-09T14:23:11Z</dc:date>
    <item>
      <title>Adding delay to Vybrid Quad SPI boot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Adding-delay-to-Vybrid-Quad-SPI-boot/m-p/429523#M4777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on Vybrid tower VF65GS10_A5. I have an application which is configured to run from DDR in the linker script file. I am flashing the application to Quad SPI so that on power-on reset it would boot from Quad SPI and run from DDR. The application currently boots from Quad SPI and runs successfully from DDR. I don't have an explicit copy program to copy my application from QSPI to DDR, so I assume it would be copied from QSPI to DDR on boot-up automitically (Not sure how this works, any more detail on this would also be helpful)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I don't have a problem with booting from Quad SPI and executing from DDR. But the problem is that the application is actually a GUI application and has some graphics and font data which is not displayed on the screen properly. So I am thinking that on boot up these data are not copied to DDR completely due to which i am seeing incomplete and distorted graphics on the screen. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One probable solution to this which i am thinking would be to add some delay before booting from QuadSPI so that it gets enough time to copy the data completely to DDR. A&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;ny help on how to do this or any other options would be greatly appreciated&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Jefy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 18:13:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Adding-delay-to-Vybrid-Quad-SPI-boot/m-p/429523#M4777</guid>
      <dc:creator>jefy</dc:creator>
      <dc:date>2015-06-04T18:13:13Z</dc:date>
    </item>
    <item>
      <title>Re: Adding delay to Vybrid Quad SPI boot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Adding-delay-to-Vybrid-Quad-SPI-boot/m-p/429524#M4778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt;​ can you attend this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2015 21:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Adding-delay-to-Vybrid-Quad-SPI-boot/m-p/429524#M4778</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2015-06-08T21:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: Adding delay to Vybrid Quad SPI boot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Adding-delay-to-Vybrid-Quad-SPI-boot/m-p/429525#M4779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jefy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To clarify - this is not a Linux system running, but a bare-metal application flashed, booted, and copied from QSPI to DDR and executed to run?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 14:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Adding-delay-to-Vybrid-Quad-SPI-boot/m-p/429525#M4779</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2015-06-09T14:23:11Z</dc:date>
    </item>
    <item>
      <title>Re: Adding delay to Vybrid Quad SPI boot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Adding-delay-to-Vybrid-Quad-SPI-boot/m-p/429526#M4780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for looking into this. Yes, this isn't a Linux system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, i managed to make this work without adding a delay, by making some modifications to quadspi_boot.c and the linker script file.. The application now boots from QSPI and copies the application properly to DDR and runs from there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Jefy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2015 14:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Adding-delay-to-Vybrid-Quad-SPI-boot/m-p/429526#M4780</guid>
      <dc:creator>jefy</dc:creator>
      <dc:date>2015-06-10T14:44:34Z</dc:date>
    </item>
  </channel>
</rss>