<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 Re: QuadSPI0 cacheable write-back</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421977#M4587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our chip does not have the M core. We only use A5. Anyway, whe next chapter starts by saying that "The Quad Serial Peripheral Interface (QuadSPI) block acts as an interface to one single or two external serial flash devices...", with "flash" in every other sentence throughout the chapter. This probably means that either:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Non-flash devices are not going to work&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;2. The doc is incomplete&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Aug 2015 04:30:33 GMT</pubDate>
    <dc:creator>eugeneryabtsev</dc:creator>
    <dc:date>2015-08-11T04:30:33Z</dc:date>
    <item>
      <title>QuadSPI0 cacheable write-back</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421975#M4585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to page 1158 of Vybrid Reference Manual (F-Series; VYBRIDRM Rev 7, 06/2014), memory range from 0x20000000 to 0x2FFFFFFF is QuadSPI0 and "cacheable write-back".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is: "write-back" to &lt;EM&gt;what&lt;/EM&gt;? Probably not to flash. Can we put some ferromagnetic memory in there and work with it just like with normal memory, but non-volatile? Where do I read more about this kind of setup? Are there any examples?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or is does this mean something else?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2015 12:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421975#M4585</guid>
      <dc:creator>eugeneryabtsev</dc:creator>
      <dc:date>2015-08-07T12:49:56Z</dc:date>
    </item>
    <item>
      <title>Re: QuadSPI0 cacheable write-back</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421976#M4586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ARM defines that region in the Cortex M4 as executable and with cache write back attribute. &lt;/P&gt;&lt;P&gt;You can copy code there and execute it.&lt;/P&gt;&lt;P&gt;The next AppNote explains the QSPI module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejnadro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 21:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421976#M4586</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-08-10T21:04:36Z</dc:date>
    </item>
    <item>
      <title>Re: QuadSPI0 cacheable write-back</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421977#M4587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our chip does not have the M core. We only use A5. Anyway, whe next chapter starts by saying that "The Quad Serial Peripheral Interface (QuadSPI) block acts as an interface to one single or two external serial flash devices...", with "flash" in every other sentence throughout the chapter. This probably means that either:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Non-flash devices are not going to work&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;2. The doc is incomplete&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 04:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421977#M4587</guid>
      <dc:creator>eugeneryabtsev</dc:creator>
      <dc:date>2015-08-11T04:30:33Z</dc:date>
    </item>
    <item>
      <title>Re: QuadSPI0 cacheable write-back</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421978#M4588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;QSPI NOR Flash work for the Cortex-A5 too. Why it should not work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2015 16:26:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421978#M4588</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-08-17T16:26:17Z</dc:date>
    </item>
    <item>
      <title>Re: QuadSPI0 cacheable write-back</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421979#M4589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It works just fine, but it is not easily write-able without some procedure. I wonder if some QSPI FRAM or something can be WRITE-mapped into QSPI window. The doc says a lot about Flash, but not a lot about any other types of memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2015 16:44:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/421979#M4589</guid>
      <dc:creator>eugeneryabtsev</dc:creator>
      <dc:date>2015-08-17T16:44:31Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/1137415#M6094</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 17:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QuadSPI0-cacheable-write-back/m-p/1137415#M6094</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T17:07:04Z</dc:date>
    </item>
  </channel>
</rss>