<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error when attempting to install 10.4 Microcontroller Drivers Suite in latest DS-5 in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417476#M4571</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Processor Expert Driver Suite v10.4 is only up to Eclipse Kepler. The 10.4 plugin installer does not run in Eclipse Luna (4.4) due a compatibility issue.&lt;/P&gt;&lt;P&gt;There is a plugin for Eclipse Luna (4.4), it is for Kinetis, not for Vybrid.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53357iA6A26E4CC95B86EB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So this one should work with DS-5 (Luna based), but will not support Vybrid. And there are currently no plans to make an update for Vybrid. So if you are using Vybrid with DS-5 with Processor Expert, you have to use pre-4.4 Eclipse.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Aug 2015 06:04:28 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2015-08-12T06:04:28Z</dc:date>
    <item>
      <title>Error when attempting to install 10.4 Microcontroller Drivers Suite in latest DS-5</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417472#M4567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just received my Vybrid Tower Kit.&lt;/P&gt;&lt;P&gt;I installed the latest version of DS-5 (5.22).&lt;/P&gt;&lt;P&gt;When attempting to install 10.4 Microcontroller Drivers Suite for Processor Expert support, the install fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An error occurred while installing the items&lt;/P&gt;&lt;P&gt;session context was:(profile=SDKProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=null --&amp;gt; [R]com.freescale.processorexpert.standalone_root 10.4.0, action=com.fresscale.updater.customactions.actions.FreescaleInstall).&lt;/P&gt;&lt;P&gt;org/eclipse/core/runtime/adaptor/LocationManager&lt;/P&gt;&lt;P&gt;org/eclipse/core/runtime/adaptor/LocationManager&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The zip file for installing mentions Eclipse 3.7 and 4.2.&lt;/P&gt;&lt;P&gt;The latest version of DS-5 is Eclipse 4.4.2.&lt;/P&gt;&lt;P&gt;Is this the issue ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a version of the Microcontroller Drivers Suite that works in DS-5 (5.22) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Chandler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2015 18:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417472#M4567</guid>
      <dc:creator>dachancellor</dc:creator>
      <dc:date>2015-08-05T18:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: Error when attempting to install 10.4 Microcontroller Drivers Suite in latest DS-5</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417473#M4568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not know how you are trying to install PE. But the driver suite is delivered and installed as a comprehensive product with the Eclipse 4.2 (Juno) IDE. It is also available as an Eclipse plug-in for existing Eclipse 3.7 (Indigo) and Eclipse 4.2 (Juno) installations. I do not think it can be installed as a plug-in in DS-5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 19:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417473#M4568</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-08-10T19:33:51Z</dc:date>
    </item>
    <item>
      <title>Re: Error when attempting to install 10.4 Microcontroller Drivers Suite in latest DS-5</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417474#M4569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alejandro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was using the provided Plugins to install into DS-5, PExDrv 10.4 and 10.4 Update 3.&lt;/P&gt;&lt;P&gt;I installed an older version of DS-5 which runs Eclipse 3.7 (5.17.1), and the plugin installation worked fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question was if there were any updated plugin files or plans to support the later versions of DS-5, which run Eclipse 4.4+&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, you are correct that the driver suite runs fine as a standalone Eclipse 4.2 IDE capable of generating PE code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;V/r,&lt;/P&gt;&lt;P&gt;Chandler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 20:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417474#M4569</guid>
      <dc:creator>dachancellor</dc:creator>
      <dc:date>2015-08-11T20:40:55Z</dc:date>
    </item>
    <item>
      <title>Re: Error when attempting to install 10.4 Microcontroller Drivers Suite in latest DS-5</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417475#M4570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked for information regarding the PE roadmap but I had no success. &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/BlackNight"&gt;BlackNight&lt;/A&gt;​ sorry to trouble you, I wonder if you have information that may help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 22:24:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417475#M4570</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-08-11T22:24:46Z</dc:date>
    </item>
    <item>
      <title>Re: Error when attempting to install 10.4 Microcontroller Drivers Suite in latest DS-5</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417476#M4571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Processor Expert Driver Suite v10.4 is only up to Eclipse Kepler. The 10.4 plugin installer does not run in Eclipse Luna (4.4) due a compatibility issue.&lt;/P&gt;&lt;P&gt;There is a plugin for Eclipse Luna (4.4), it is for Kinetis, not for Vybrid.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53357iA6A26E4CC95B86EB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So this one should work with DS-5 (Luna based), but will not support Vybrid. And there are currently no plans to make an update for Vybrid. So if you are using Vybrid with DS-5 with Processor Expert, you have to use pre-4.4 Eclipse.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 06:04:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417476#M4571</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-08-12T06:04:28Z</dc:date>
    </item>
    <item>
      <title>Re: Error when attempting to install 10.4 Microcontroller Drivers Suite in latest DS-5</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417477#M4572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Erich !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 13:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Error-when-attempting-to-install-10-4-Microcontroller-Drivers/m-p/417477#M4572</guid>
      <dc:creator>dachancellor</dc:creator>
      <dc:date>2015-08-12T13:14:38Z</dc:date>
    </item>
  </channel>
</rss>