<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: MVF61NN151CMK50 maximum FlexTimer clock frequency (what the system clock is)?</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/414271#M4484</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; background-color: #ffffff;"&gt;&amp;gt; The system clock is fixed at &lt;/SPAN&gt;&lt;SPAN class="" style="color: #1f497d; background-color: #ffffff; border: 0px;"&gt;IPG_Clk&lt;/SPAN&gt;&lt;SPAN style="color: #1f497d; background-color: #ffffff;"&gt; divided by 2, so is 83 MHz is the IPG clock (or CM4 ) is running at 167MHz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; background-color: #ffffff;"&gt;Shoudn't this be IPG clock = Platform Bus or CM4 Clock / 2? &amp;nbsp; &amp;nbsp;(Table 6-6 Clocking Configuration).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; background-color: #ffffff;"&gt;And then the undefined 'system clock' in the manual is actually = IPG clock, not IPG / 2.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 May 2017 12:57:49 GMT</pubDate>
    <dc:creator>dry</dc:creator>
    <dc:date>2017-05-16T12:57:49Z</dc:date>
    <item>
      <title>MVF61NN151CMK50 maximum FlexTimer clock frequency (what the system clock is)?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/414268#M4481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going to use FTM capture mode for period measurement. Looking into the datasheet (VYBRIDRM.pdf), possible FTM clocks are: system clock, fixed frequency clock, external clock. I have not found a direct description of what the "system clock" is for FTM. I assumed that it is the System Core Clock for A5, that is, around 396MHz or so. But sample code showed that the real clock is only 66MHz (while A5 clocked at 396MHz). PDF references for other CPUs with FlexTimer explicitly tell that "FTM system closk is the bus clock, around 66MHz", but VYBRIDRM.pdf does not explain this (or I missed that). At the same time the table 9-10 (page 628) introduces "flex_root_clk" clock name, for which the maximum frequency is 85MHz. This flex_root_clk is found in the document just once, and no more references to it. It looks like FTM clock = Bus clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my questions are:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;What is the maximum frequency for FTM clock of MVF61NN151CMK50?&lt;/LI&gt;&lt;LI&gt;What the "system clock" for FTM is?&lt;/LI&gt;&lt;LI&gt;Where it is documented for this chip?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 09:43:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/414268#M4481</guid>
      <dc:creator>os-freescale-co</dc:creator>
      <dc:date>2015-07-15T09:43:05Z</dc:date>
    </item>
    <item>
      <title>Re: MVF61NN151CMK50 maximum FlexTimer clock frequency (what the system clock is)?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/414269#M4482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;The clocking of FTM is shown below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52186iEFBF6AEE83AA6A66/image-size/large?v=v2&amp;amp;px=999" title="image002.jpg" alt="image002.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;FTM has options for Fixed clock, System clock, and External clock. The system clock is fixed at &lt;SPAN class="SpellE"&gt;IPG_Clk&lt;/SPAN&gt; divided by 2, so is 83 MHz is the IPG clock (or CM4 ) is running at 167MHz. All other clocks have to follow the relation as stated in the Reference Manual. I am quoting them again below:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;The fixed frequency clock is an alternative clock source for the FTM counter that allows the selection of a clock other than the system clock or an external clock. This clock input is defined by chip integration.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;Due to the FTM hardware implementation limitations, the fixed frequency clock frequency &lt;SPAN style="background: yellow;"&gt;must not exceed 1/2 of the system&lt;/SPAN&gt; clock frequency.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;The frequency of the external clock source &lt;SPAN style="background: yellow;"&gt;must not exceed 1/4 of the system&lt;/SPAN&gt; clock frequency.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding: 0 0 1.0pt 0;"&gt;&lt;SPAN style="color: #1f497d;"&gt;As far as the IO speed is concerned, I don't think the IO's will have a problem propagating a 42MHz signal (half of 83 MHz).&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding: 0 0 1.0pt 0;"&gt;&lt;/P&gt;&lt;P style="padding: 0 0 1.0pt 0;"&gt;&lt;SPAN style="color: #1f497d;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding: 0 0 1.0pt 0;"&gt;&lt;SPAN style="color: #1f497d;"&gt;Alejandro&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 23:01:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/414269#M4482</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-07-22T23:01:49Z</dc:date>
    </item>
    <item>
      <title>Re: MVF61NN151CMK50 maximum FlexTimer clock frequency (what the system clock is)?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/414270#M4483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems to be correct, but FTM clocking diagram does NOT show "system clock". So could you please point me to the statement in a document where "&lt;SPAN style="color: #1f497d; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;The system clock is fixed at &lt;/SPAN&gt;&lt;SPAN class="SpellE" style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #1f497d;"&gt;IPG_Clk&lt;/SPAN&gt;&lt;SPAN style="color: #1f497d; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt; divided by 2"&lt;/SPAN&gt; is written? I did not find it so asked the question. Or, if it is not documented, then would be good to have it finally fixed in the manual. Still, I believe that I missed that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2015 12:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/414270#M4483</guid>
      <dc:creator>os-freescale-co</dc:creator>
      <dc:date>2015-08-07T12:21:26Z</dc:date>
    </item>
    <item>
      <title>Re: MVF61NN151CMK50 maximum FlexTimer clock frequency (what the system clock is)?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/414271#M4484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; background-color: #ffffff;"&gt;&amp;gt; The system clock is fixed at &lt;/SPAN&gt;&lt;SPAN class="" style="color: #1f497d; background-color: #ffffff; border: 0px;"&gt;IPG_Clk&lt;/SPAN&gt;&lt;SPAN style="color: #1f497d; background-color: #ffffff;"&gt; divided by 2, so is 83 MHz is the IPG clock (or CM4 ) is running at 167MHz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; background-color: #ffffff;"&gt;Shoudn't this be IPG clock = Platform Bus or CM4 Clock / 2? &amp;nbsp; &amp;nbsp;(Table 6-6 Clocking Configuration).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; background-color: #ffffff;"&gt;And then the undefined 'system clock' in the manual is actually = IPG clock, not IPG / 2.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 12:57:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/414271#M4484</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2017-05-16T12:57:49Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/1137287#M6089</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 16:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/MVF61NN151CMK50-maximum-FlexTimer-clock-frequency-what-the/m-p/1137287#M6089</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T16:55:27Z</dc:date>
    </item>
  </channel>
</rss>