<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 SFlash configuration header</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413613#M4476</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are working on a custom vybrid-based platform, and are attempting to boot from QSPI1(Spansion S25FL256S). The image we are attempting to boot have been tested and is known to work on the TWR-VF65GS10 kit using QSPI0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the Vybrid Manufacturing Tool, we extracted the following header which was contained it a pre-compiled image bundled with the tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;------------------------- SFLASH CONFIG HEADER START -------------------------&lt;/P&gt;&lt;P&gt;Hold delay: 0 (disabled)&lt;/P&gt;&lt;P&gt;Half Speed Phase Selection: 0 (Select sampling at non-inverted clock)&lt;/P&gt;&lt;P&gt;Half Speed Delay: 0 (One clock cycle delay)&lt;/P&gt;&lt;P&gt;Chip Select hold time: 0&lt;/P&gt;&lt;P&gt;Chip Select setup time: 0&lt;/P&gt;&lt;P&gt;Serial Flash A1 size: 0x01000000 (16MB)&lt;/P&gt;&lt;P&gt;Serial Flash A2 size: 0&lt;/P&gt;&lt;P&gt;Serial Flash B1 size: 0x01000000 (16MB)&lt;/P&gt;&lt;P&gt;Serial Flash B2 size: 0&lt;/P&gt;&lt;P&gt;Serial Clock Frequency: 1 (60 MHz)&lt;/P&gt;&lt;P&gt;Mode of operation of serial Flash: 4 (Quad 4-bit data)&lt;/P&gt;&lt;P&gt;Serial Flash Port B selection: 0 (Port B is not used)&lt;/P&gt;&lt;P&gt;Dual Data Rate mode enable: 0 (DDR mode is disabled)&lt;/P&gt;&lt;P&gt;Data Strobe Signal enable in Serial Flash: 0 (Disable DQS)&lt;/P&gt;&lt;P&gt;Parallel Mode enable: 0 (Disable Parallel Mode in QSPI)&lt;/P&gt;&lt;P&gt;CS1 on Port A: 0 (Disable CS1 on Port A)&lt;/P&gt;&lt;P&gt;CS1 on Port B: 0 (Disable CS1 on Port B)&lt;/P&gt;&lt;P&gt;Full Speed Phase Selection: 0 (Select sampling at non-inverted clock)&lt;/P&gt;&lt;P&gt;Full Speed Delay Selection: 0 (One clock cycle delay)&lt;/P&gt;&lt;P&gt;DDR Sampling Point: 0​&lt;/P&gt;&lt;P&gt;-------------------------- SFLASH CONFIG HEADER END --------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have attempted to change the "Serial Flash Port B selection" field to 1, set the size of A1 to 0x00 and B1 to 0x02000000, but unfortunately this does not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have set our card to boot from fuses, and set the bootconfig appropriately. Probing the QSPI-flash chip shows that there is traffic between the MCU and chip upon boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any input?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Sep 2015 06:36:41 GMT</pubDate>
    <dc:creator>tfe</dc:creator>
    <dc:date>2015-09-29T06:36:41Z</dc:date>
    <item>
      <title>SFlash configuration header</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413613#M4476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are working on a custom vybrid-based platform, and are attempting to boot from QSPI1(Spansion S25FL256S). The image we are attempting to boot have been tested and is known to work on the TWR-VF65GS10 kit using QSPI0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the Vybrid Manufacturing Tool, we extracted the following header which was contained it a pre-compiled image bundled with the tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;------------------------- SFLASH CONFIG HEADER START -------------------------&lt;/P&gt;&lt;P&gt;Hold delay: 0 (disabled)&lt;/P&gt;&lt;P&gt;Half Speed Phase Selection: 0 (Select sampling at non-inverted clock)&lt;/P&gt;&lt;P&gt;Half Speed Delay: 0 (One clock cycle delay)&lt;/P&gt;&lt;P&gt;Chip Select hold time: 0&lt;/P&gt;&lt;P&gt;Chip Select setup time: 0&lt;/P&gt;&lt;P&gt;Serial Flash A1 size: 0x01000000 (16MB)&lt;/P&gt;&lt;P&gt;Serial Flash A2 size: 0&lt;/P&gt;&lt;P&gt;Serial Flash B1 size: 0x01000000 (16MB)&lt;/P&gt;&lt;P&gt;Serial Flash B2 size: 0&lt;/P&gt;&lt;P&gt;Serial Clock Frequency: 1 (60 MHz)&lt;/P&gt;&lt;P&gt;Mode of operation of serial Flash: 4 (Quad 4-bit data)&lt;/P&gt;&lt;P&gt;Serial Flash Port B selection: 0 (Port B is not used)&lt;/P&gt;&lt;P&gt;Dual Data Rate mode enable: 0 (DDR mode is disabled)&lt;/P&gt;&lt;P&gt;Data Strobe Signal enable in Serial Flash: 0 (Disable DQS)&lt;/P&gt;&lt;P&gt;Parallel Mode enable: 0 (Disable Parallel Mode in QSPI)&lt;/P&gt;&lt;P&gt;CS1 on Port A: 0 (Disable CS1 on Port A)&lt;/P&gt;&lt;P&gt;CS1 on Port B: 0 (Disable CS1 on Port B)&lt;/P&gt;&lt;P&gt;Full Speed Phase Selection: 0 (Select sampling at non-inverted clock)&lt;/P&gt;&lt;P&gt;Full Speed Delay Selection: 0 (One clock cycle delay)&lt;/P&gt;&lt;P&gt;DDR Sampling Point: 0​&lt;/P&gt;&lt;P&gt;-------------------------- SFLASH CONFIG HEADER END --------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have attempted to change the "Serial Flash Port B selection" field to 1, set the size of A1 to 0x00 and B1 to 0x02000000, but unfortunately this does not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have set our card to boot from fuses, and set the bootconfig appropriately. Probing the QSPI-flash chip shows that there is traffic between the MCU and chip upon boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any input?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Sep 2015 06:36:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413613#M4476</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2015-09-29T06:36:41Z</dc:date>
    </item>
    <item>
      <title>Re: SFlash configuration header</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413614#M4477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt;​ are you able&amp;nbsp; to&amp;nbsp; attend this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 16:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413614#M4477</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2015-10-05T16:15:51Z</dc:date>
    </item>
    <item>
      <title>Re: SFlash configuration header</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413615#M4478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are currently looking into this, and attempting to determine a cause. We will follow up when we have some insight.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Oct 2015 19:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413615#M4478</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2015-10-06T19:01:59Z</dc:date>
    </item>
    <item>
      <title>Re: SFlash configuration header</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413616#M4479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt;​ do you have an update?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Oct 2015 17:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413616#M4479</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2015-10-12T17:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: SFlash configuration header</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413617#M4480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I eventually figured this out myself. Only a small modification was necessary:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;------------------------- SFLASH CONFIG HEADER START -------------------------&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Hold delay: 0 (disabled)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Half Speed Phase Selection: 0 (Select sampling at non-inverted clock)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Half Speed Delay: 0 (One clock cycle delay)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Chip Select hold time: 0&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Chip Select setup time: 0&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Serial Flash A1 size: 0x02000000 (32MB)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Serial Flash A2 size: 0&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Serial Flash B1 size: 0&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Serial Flash B2 size: 0&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Serial Clock Frequency: 1 (60 MHz)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Mode of operation of serial Flash: 4 (Quad 4-bit data)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Serial Flash Port B selection: 0 (Port B is not used)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Dual Data Rate mode enable: 0 (DDR mode is disabled)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Data Strobe Signal enable in Serial Flash: 0 (Disable DQS)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Parallel Mode enable: 0 (Disable Parallel Mode in QSPI)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;CS1 on Port A: 0 (Disable CS1 on Port A)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;CS1 on Port B: 0 (Disable CS1 on Port B)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Full Speed Phase Selection: 0 (Select sampling at non-inverted clock)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Full Speed Delay Selection: 0 (One clock cycle delay)&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;DDR Sampling Point: 0&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;-------------------------- SFLASH CONFIG HEADER END --------------------------&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Cheers&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Oct 2015 06:24:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SFlash-configuration-header/m-p/413617#M4480</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2015-10-13T06:24:35Z</dc:date>
    </item>
  </channel>
</rss>