<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: Can't pass float variables between A5 and M4 core using MCC</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Can-t-pass-float-variables-between-A5-and-M4-core-using-MCC/m-p/411462#M4466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any updates/inputs regarding above mentioned issue ?&lt;/P&gt;&lt;P&gt;Because a simple printf() is also not working for float variables.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Swapnil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Aug 2015 05:21:02 GMT</pubDate>
    <dc:creator>swapnilv</dc:creator>
    <dc:date>2015-08-06T05:21:02Z</dc:date>
    <item>
      <title>Can't pass float variables between A5 and M4 core using MCC</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Can-t-pass-float-variables-between-A5-and-M4-core-using-MCC/m-p/411461#M4465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have MQX 4.0.1 installed on my pc.&lt;/P&gt;&lt;P&gt;I tried to flash the sample pingpong example given for MCC demo for twrvf65gs10 tower board on Vybrid evaluation kit.&lt;/P&gt;&lt;P&gt;I am able to see the desired output on terminal.&lt;/P&gt;&lt;P&gt;But when I try to pass float variable value&amp;nbsp; between A5 and M4 core; those values are not getting passed.&lt;/P&gt;&lt;P&gt;Even simple printf is not showing the float variable value.&lt;/P&gt;&lt;P&gt;I tried to declare simple float variable in main_task in file mcc.c and print the variable value on terminal as explained below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; float myTemp = 50.00;&lt;/P&gt;&lt;P&gt; printf("Test flt Variable: %f \n",myTemp);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the float variable values are not shown on terminal window.&lt;/P&gt;&lt;P&gt;Output of print command is as shown below on terminal window:&lt;/P&gt;&lt;P&gt;Test flt Variable: f&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Expected output is:&lt;/P&gt;&lt;P&gt;Test flt Variable: 50.000000;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly look into it and let me know the solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Swapnil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2015 15:08:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Can-t-pass-float-variables-between-A5-and-M4-core-using-MCC/m-p/411461#M4465</guid>
      <dc:creator>swapnilv</dc:creator>
      <dc:date>2015-08-04T15:08:31Z</dc:date>
    </item>
    <item>
      <title>Re: Can't pass float variables between A5 and M4 core using MCC</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Can-t-pass-float-variables-between-A5-and-M4-core-using-MCC/m-p/411462#M4466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any updates/inputs regarding above mentioned issue ?&lt;/P&gt;&lt;P&gt;Because a simple printf() is also not working for float variables.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Swapnil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 05:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Can-t-pass-float-variables-between-A5-and-M4-core-using-MCC/m-p/411462#M4466</guid>
      <dc:creator>swapnilv</dc:creator>
      <dc:date>2015-08-06T05:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: Can't pass float variables between A5 and M4 core using MCC</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Can-t-pass-float-variables-between-A5-and-M4-core-using-MCC/m-p/411463#M4467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below flag was set to 0 in twrvf65gs10_a5 project "user_config.h" file.&lt;/P&gt;&lt;P&gt;#define MQX_INCLUDE_FLOATING_POINT_IO&amp;nbsp;&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;I changed it to 1 and now I can see the float values correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Swapnil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 13:34:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Can-t-pass-float-variables-between-A5-and-M4-core-using-MCC/m-p/411463#M4467</guid>
      <dc:creator>swapnilv</dc:creator>
      <dc:date>2015-08-06T13:34:38Z</dc:date>
    </item>
  </channel>
</rss>