<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic vybrid Processor Expert selects multiple pins for I2C0 SCL in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/410449#M4442</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Processor Expert 10.4 to configure a Vybrid&lt;/P&gt;&lt;P&gt;Problem I have is that when I select pin B14 for I2C0 SCL, the tool also checks pins K18 and L3 (which I need for other things)&amp;nbsp; -see attachment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i2C1 behaves as I would expect (I can select any one of the available pins)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a bug in the tool, or is there some strange dependency in the chip I'm not aware of ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Apr 2015 10:12:04 GMT</pubDate>
    <dc:creator>alanball</dc:creator>
    <dc:date>2015-04-15T10:12:04Z</dc:date>
    <item>
      <title>vybrid Processor Expert selects multiple pins for I2C0 SCL</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/410449#M4442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Processor Expert 10.4 to configure a Vybrid&lt;/P&gt;&lt;P&gt;Problem I have is that when I select pin B14 for I2C0 SCL, the tool also checks pins K18 and L3 (which I need for other things)&amp;nbsp; -see attachment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i2C1 behaves as I would expect (I can select any one of the available pins)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a bug in the tool, or is there some strange dependency in the chip I'm not aware of ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2015 10:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/410449#M4442</guid>
      <dc:creator>alanball</dc:creator>
      <dc:date>2015-04-15T10:12:04Z</dc:date>
    </item>
    <item>
      <title>Re: vybrid Processor Expert selects multiple pins for I2C0 SCL</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/410450#M4443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alan,&lt;/P&gt;&lt;P&gt;I tried select only pin B14 on PEx in new project and it was work. I attaching screen. I think, that i can be affected by other things.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Vilem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2015 07:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/410450#M4443</guid>
      <dc:creator>VilemZ</dc:creator>
      <dc:date>2015-04-21T07:19:58Z</dc:date>
    </item>
    <item>
      <title>Re: vybrid Processor Expert selects multiple pins for I2C0 SCL</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/410451#M4444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same behavior as Vilem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The version I have is the next:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49444iBF677234930D2942/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if there is any difference. I am not sure if there is an update package you need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The installation details are the next:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49653iC1E339FAA7AD1780/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 00:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/410451#M4444</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-04-22T00:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: vybrid Processor Expert selects multiple pins for I2C0 SCL</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/410452#M4445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alejandro &amp;amp; Vilem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like there is a later version of PE - I will check&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the meantime, since I was still able to change my hardware design, I changed from I2C0 to I2C1, which does not have any issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 07:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/410452#M4445</guid>
      <dc:creator>alanball</dc:creator>
      <dc:date>2015-04-22T07:13:23Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/1137214#M6085</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 16:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/vybrid-Processor-Expert-selects-multiple-pins-for-I2C0-SCL/m-p/1137214#M6085</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T16:50:37Z</dc:date>
    </item>
  </channel>
</rss>