<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Linux kernel 3.13 blocks PIT interrupt on M4 on PCM052 in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Linux-kernel-3-13-blocks-PIT-interrupt-on-M4-on-PCM052/m-p/406821#M4396</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a PIT running every millisecond on my Cortex-M4. This works fine while a Linux with kernel 3.0 is running on the A5. However, after switching to kernel 3.13 the PIT interrupt on the M4 is not triggered anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I enable the PIT in Linux(&lt;/P&gt;&lt;P&gt; System Type-&amp;gt; Freescale i.MX family-&amp;gt; Freescale i.MX support-&amp;gt;Vybrid Family VF610 support-&amp;gt;Clocksource for scheduler clock (Use PIT timer)&lt;/P&gt;&lt;P&gt;) the interrupt is also triggered on the M4, but Linux crashes regularly. The shell simply doesn't react anymore. I guess it doesn't like that the scheduler clock is used by someone else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I prevent Linux from disabling interrupts that it doesn't use? Linux should only touch the registers of the interrupts it uses and leave all other vectors to the M4.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Aug 2015 15:09:25 GMT</pubDate>
    <dc:creator>mpfgregory</dc:creator>
    <dc:date>2015-08-03T15:09:25Z</dc:date>
    <item>
      <title>Linux kernel 3.13 blocks PIT interrupt on M4 on PCM052</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Linux-kernel-3-13-blocks-PIT-interrupt-on-M4-on-PCM052/m-p/406821#M4396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a PIT running every millisecond on my Cortex-M4. This works fine while a Linux with kernel 3.0 is running on the A5. However, after switching to kernel 3.13 the PIT interrupt on the M4 is not triggered anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I enable the PIT in Linux(&lt;/P&gt;&lt;P&gt; System Type-&amp;gt; Freescale i.MX family-&amp;gt; Freescale i.MX support-&amp;gt;Vybrid Family VF610 support-&amp;gt;Clocksource for scheduler clock (Use PIT timer)&lt;/P&gt;&lt;P&gt;) the interrupt is also triggered on the M4, but Linux crashes regularly. The shell simply doesn't react anymore. I guess it doesn't like that the scheduler clock is used by someone else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I prevent Linux from disabling interrupts that it doesn't use? Linux should only touch the registers of the interrupts it uses and leave all other vectors to the M4.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2015 15:09:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Linux-kernel-3-13-blocks-PIT-interrupt-on-M4-on-PCM052/m-p/406821#M4396</guid>
      <dc:creator>mpfgregory</dc:creator>
      <dc:date>2015-08-03T15:09:25Z</dc:date>
    </item>
    <item>
      <title>Re: Linux kernel 3.13 blocks PIT interrupt on M4 on PCM052</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Linux-kernel-3-13-blocks-PIT-interrupt-on-M4-on-PCM052/m-p/406822#M4397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt;​ can you help with this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2015 17:19:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Linux-kernel-3-13-blocks-PIT-interrupt-on-M4-on-PCM052/m-p/406822#M4397</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2015-08-03T17:19:07Z</dc:date>
    </item>
    <item>
      <title>Re: Linux kernel 3.13 blocks PIT interrupt on M4 on PCM052</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Linux-kernel-3-13-blocks-PIT-interrupt-on-M4-on-PCM052/m-p/406823#M4398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have exchanged the hwtimer driver in the MQX 4.0.1 BSP with the one from the MQX 4.1 BSP. Now it works with the 3.13 kernel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2015 10:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Linux-kernel-3-13-blocks-PIT-interrupt-on-M4-on-PCM052/m-p/406823#M4398</guid>
      <dc:creator>mpfgregory</dc:creator>
      <dc:date>2015-08-05T10:09:37Z</dc:date>
    </item>
  </channel>
</rss>