<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 About QSPI clock setting .</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/About-QSPI-clock-setting/m-p/404825#M4386</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I refered VYBRIDRSERIESEC_Rev_7.pdf of p58"9.5.1 QuadSPI timing".&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps atn"&gt;The QSPI_MCR [DDR_EN] &lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a set&lt;/SPAN&gt; (to &lt;SPAN class="hps"&gt;1b)&lt;/SPAN&gt;&lt;SPAN class="hps"&gt;in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;state&lt;/SPAN&gt;, &lt;SPAN class="hps"&gt;if &lt;/SPAN&gt; &lt;SPAN class="hps"&gt;sent&amp;nbsp; the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;command&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Programing&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;"SDR", then &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am &lt;SPAN class="hps"&gt;recognized as&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the operation&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of &lt;SPAN class="hps"&gt;p59&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;"QuadSPI Output / Write timing (SDR mode)"&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;whether I should refer to either the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;operating conditions&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;this&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;case&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&lt;SPAN title="p59の”QuadSPI Output/Write timing (SDR mode)”とp61の”QuadSPI Output/Write timing (DDR mode)”のどちらを参照すればよいのでしょうか？"&gt;Of p59 "QuadSPI Output / Write timing (SDR mode)" or of p61 "QuadSPI Output / Write timing (DDR mode)"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN title="p59の”QuadSPI Output/Write timing (SDR mode)”とp61の”QuadSPI Output/Write timing (DDR mode)”のどちらを参照すればよいのでしょうか？"&gt;Whitch referred to either of?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN title="動作的に”SDR mode”では、SCKはMAX80MHzで現状の69.88MHzの設定で範囲内ですが、"&gt;In operatively "SDR mode", SCK&amp;nbsp; is within the range in the current setting of 69.88MHz in MAX80MHz,&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN title="しかし”DDR mode”を参照すると、MAXが45MHzとなっている為、上限を超えてしまいます。"&gt;However, when referring to "DDR mode", since the MAX has a 45MHz, it will over the upper limit.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN title="しかし”DDR mode”を参照すると、MAXが45MHzとなっている為、上限を超えてしまいます。"&gt;Please teach me SCK setting is no problem at 69.88MHz.&lt;SPAN title="しかし”DDR mode”を参照すると、MAXが45MHzとなっている為、上限を超えてしまいます。"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN title="しかし”DDR mode”を参照すると、MAXが45MHzとなっている為、上限を超えてしまいます。"&gt;And would you please replay of previous question of ( &lt;A _jive_internal="true" class="title" data-content-finding="Community" href="https://community.nxp.com/thread/355603?sr=stream"&gt;I want to calculate&amp;nbsp; of&amp;nbsp; ”Read freaquency calculations", "Max read frequency", "Hold timing"&lt;/A&gt;).&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 May 2015 07:01:41 GMT</pubDate>
    <dc:creator>takashitakahash</dc:creator>
    <dc:date>2015-05-28T07:01:41Z</dc:date>
    <item>
      <title>About QSPI clock setting .</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/About-QSPI-clock-setting/m-p/404825#M4386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I refered VYBRIDRSERIESEC_Rev_7.pdf of p58"9.5.1 QuadSPI timing".&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps atn"&gt;The QSPI_MCR [DDR_EN] &lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a set&lt;/SPAN&gt; (to &lt;SPAN class="hps"&gt;1b)&lt;/SPAN&gt;&lt;SPAN class="hps"&gt;in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;state&lt;/SPAN&gt;, &lt;SPAN class="hps"&gt;if &lt;/SPAN&gt; &lt;SPAN class="hps"&gt;sent&amp;nbsp; the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;command&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Programing&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;"SDR", then &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am &lt;SPAN class="hps"&gt;recognized as&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the operation&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of &lt;SPAN class="hps"&gt;p59&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;"QuadSPI Output / Write timing (SDR mode)"&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;whether I should refer to either the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;operating conditions&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;this&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;case&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&lt;SPAN title="p59の”QuadSPI Output/Write timing (SDR mode)”とp61の”QuadSPI Output/Write timing (DDR mode)”のどちらを参照すればよいのでしょうか？"&gt;Of p59 "QuadSPI Output / Write timing (SDR mode)" or of p61 "QuadSPI Output / Write timing (DDR mode)"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN title="p59の”QuadSPI Output/Write timing (SDR mode)”とp61の”QuadSPI Output/Write timing (DDR mode)”のどちらを参照すればよいのでしょうか？"&gt;Whitch referred to either of?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN title="動作的に”SDR mode”では、SCKはMAX80MHzで現状の69.88MHzの設定で範囲内ですが、"&gt;In operatively "SDR mode", SCK&amp;nbsp; is within the range in the current setting of 69.88MHz in MAX80MHz,&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN title="しかし”DDR mode”を参照すると、MAXが45MHzとなっている為、上限を超えてしまいます。"&gt;However, when referring to "DDR mode", since the MAX has a 45MHz, it will over the upper limit.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN title="しかし”DDR mode”を参照すると、MAXが45MHzとなっている為、上限を超えてしまいます。"&gt;Please teach me SCK setting is no problem at 69.88MHz.&lt;SPAN title="しかし”DDR mode”を参照すると、MAXが45MHzとなっている為、上限を超えてしまいます。"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN title="しかし”DDR mode”を参照すると、MAXが45MHzとなっている為、上限を超えてしまいます。"&gt;And would you please replay of previous question of ( &lt;A _jive_internal="true" class="title" data-content-finding="Community" href="https://community.nxp.com/thread/355603?sr=stream"&gt;I want to calculate&amp;nbsp; of&amp;nbsp; ”Read freaquency calculations", "Max read frequency", "Hold timing"&lt;/A&gt;).&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2015 07:01:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/About-QSPI-clock-setting/m-p/404825#M4386</guid>
      <dc:creator>takashitakahash</dc:creator>
      <dc:date>2015-05-28T07:01:41Z</dc:date>
    </item>
    <item>
      <title>Re: About QSPI clock setting .</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/About-QSPI-clock-setting/m-p/404826#M4387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Takashi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you are configuring the QSPI module in SDR you should refer to table 49 which states that the max SCK frequency is 80MHz. Therefore the 69.88MHz won't be an issue as long as you are working in SDR mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2015 22:17:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/About-QSPI-clock-setting/m-p/404826#M4387</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-06-17T22:17:09Z</dc:date>
    </item>
  </channel>
</rss>