<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックSDHC with simple DMA?</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-with-simple-DMA/m-p/233218#M430</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; hi,I use the simple DMA mode of the SDHC' internal DMA with Vybrid Tower.The OS is MQX 4.0.2.When I select "DDR debug" with IAR,the file in the SD card was not written or readed correctly.But,when I select "Int Ram debug",the file was written or readed correctly.On the datasheet &amp;lt;vybrid Reference manual&amp;gt; page 2742,it say "the SDHC internal DMA does support&amp;nbsp; a virtual memory system".I want to know ,how to use simple DMA in DDR mode with Vybrid Tower system?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Nov 2013 01:40:35 GMT</pubDate>
    <dc:creator>lizhenq</dc:creator>
    <dc:date>2013-11-28T01:40:35Z</dc:date>
    <item>
      <title>SDHC with simple DMA?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-with-simple-DMA/m-p/233218#M430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; hi,I use the simple DMA mode of the SDHC' internal DMA with Vybrid Tower.The OS is MQX 4.0.2.When I select "DDR debug" with IAR,the file in the SD card was not written or readed correctly.But,when I select "Int Ram debug",the file was written or readed correctly.On the datasheet &amp;lt;vybrid Reference manual&amp;gt; page 2742,it say "the SDHC internal DMA does support&amp;nbsp; a virtual memory system".I want to know ,how to use simple DMA in DDR mode with Vybrid Tower system?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Nov 2013 01:40:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDHC-with-simple-DMA/m-p/233218#M430</guid>
      <dc:creator>lizhenq</dc:creator>
      <dc:date>2013-11-28T01:40:35Z</dc:date>
    </item>
    <item>
      <title>Re: SDHC with simple DMA?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-with-simple-DMA/m-p/233219#M431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; I find the reason.The function&amp;nbsp; fopen(ptr,flags)&amp;nbsp; in MFS,.The "flags" is only suport "r" "r+" "w" "w+",so when use "rb+",it will not write data to file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Nov 2013 08:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDHC-with-simple-DMA/m-p/233219#M431</guid>
      <dc:creator>lizhenq</dc:creator>
      <dc:date>2013-11-28T08:10:35Z</dc:date>
    </item>
  </channel>
</rss>