<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 Re: Calculating Vybrid CPU core temperature with the internal temperature sensor</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391903#M4227</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri,&lt;/P&gt;&lt;P&gt;&amp;gt; Slope coefficient remains. Only offset at 25°C is little bit higher &lt;SPAN class="GramE"&gt;696&amp;nbsp; -&lt;/SPAN&gt;&amp;gt; 699 mV when 3.3V is used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok, thanks for the confirmation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Bhuvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Sep 2015 07:04:17 GMT</pubDate>
    <dc:creator>bhuvanchandradv</dc:creator>
    <dc:date>2015-09-23T07:04:17Z</dc:date>
    <item>
      <title>Calculating Vybrid CPU core temperature with the internal temperature sensor</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391899#M4223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the moment the internal temperature sensor readings are calculated using the formula[ &lt;EM&gt;&lt;STRONG&gt;Temp = 25 - ( (Vtemp -Vtemp25) / m)&lt;/STRONG&gt;&lt;/EM&gt; ]&lt;/P&gt;&lt;P&gt;with optimal slope-coefficient constant at all temperatures provided in Vybrid datasheet, we observe a difference of ~20 'C from&lt;/P&gt;&lt;P&gt;the internal temperature reading and the external temperature on SoC package. We believe there could not be much temperature&lt;/P&gt;&lt;P&gt;differnce. When using the cold/hot slope-coefficients constants provided in AN3031[1] there is ~4'C difference between the internal&lt;/P&gt;&lt;P&gt;cpu temperature and the external temperature on SoC package. Can some one please confirm the temperature difference between&lt;/P&gt;&lt;P&gt;the internal CPU core and the external SoC temperature on package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[1] &lt;A href="https://www.google.co.in/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=1&amp;amp;cad=rja&amp;amp;uact=8&amp;amp;ved=0CBwQFjAAahUKEwjW-amA1f_HAhXLppQKHa86A9I&amp;amp;url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fmicrocontrollers%2Fdoc%2Fapp_note%2FAN3031.pdf&amp;amp;usg=AFQjCNFkvJr6RqQ8J4uWlYR72yHUS7TKTQ&amp;amp;sig2=9CJTQ1bqtHLRoPxn8nziyQ&amp;amp;bvm=bv.102829193,d.dGo" title="https://www.google.co.in/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=1&amp;amp;cad=rja&amp;amp;uact=8&amp;amp;ved=0CBwQFjAAahUKEwjW-amA1f_HAhXLppQKHa86A9I&amp;amp;url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fmicrocontrollers%2Fdoc%2Fapp_note%2FAN3031.pdf&amp;amp;usg=AFQjCNFkvJr6RqQ8J4uWlYR72yHUS7TKTQ&amp;amp;sig2=9CJTQ1bqtHLRoPxn8nziyQ&amp;amp;bvm=bv.102829193,d.dGo"&gt;https://www.google.co.in/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=1&amp;amp;cad=rja&amp;amp;uact=8&amp;amp;ved=0CBwQFjAAahUKEwjW-amA1f_HAhXLppQKHa…&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Bhuvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 04:42:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391899#M4223</guid>
      <dc:creator>bhuvanchandradv</dc:creator>
      <dc:date>2015-09-18T04:42:56Z</dc:date>
    </item>
    <item>
      <title>Re: Calculating Vybrid CPU core temperature with the internal temperature sensor</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391900#M4224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bhuvan,&lt;/P&gt;&lt;P&gt;1. Temperature sensor is specified at 3.0V VDDAD. Do you use 3.0V or 3.3V?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54705iAB96296533030523/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Data from 2 samples shows this voltage at 3.3V is slightly different.&lt;/P&gt;&lt;P&gt;Sample 6&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.69851V&lt;/P&gt;&lt;P&gt;Sample 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.70012V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Second think is ADC precision. For 10 bits 1LSB is 3.2mV. Which are 2-3 °C. But precision of ADC is less. For example for -+3LSB it will be +-5°C due to ADC. Presume that you use hardware filtering on ADC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Internal temp sensor is dedicated for approximate internal temperature measurement - not for precise measurement. Anyway by calibration you can achieve precision in °C.&lt;/P&gt;&lt;P&gt;/Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 07:47:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391900#M4224</guid>
      <dc:creator>jiri-b36968</dc:creator>
      <dc:date>2015-09-22T07:47:44Z</dc:date>
    </item>
    <item>
      <title>Re: Calculating Vybrid CPU core temperature with the internal temperature sensor</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391901#M4225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; 1. Temperature sensor is specified at 3.0V VDDAD. Do you use 3.0V or 3.3V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use 3.3V as reference.&lt;/P&gt;&lt;P&gt;Seems the slope coefficients provided in AN3031 doc is also considering VDD as 3.0V.&lt;/P&gt;&lt;P&gt;How can we calculate the slope coefficients when VDD of 3.3V is considered.&lt;/P&gt;&lt;P&gt;There is no data available in An3031 doc for calculating slope coefficient with VDD as 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Data from 2 samples shows this voltage at 3.3V is slightly different.&lt;/P&gt;&lt;P&gt;&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Sample 6&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.69851V&lt;/P&gt;&lt;P&gt;&amp;gt; &lt;/P&gt;&lt;P&gt;&amp;gt; Sample 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.70012V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sorry, i didn't understand this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; 2. Second think is ADC precision. For 10 bits 1LSB is 3.2mV. Which are 2-3 °C. But precision&lt;/P&gt;&lt;P&gt;&amp;gt; of ADC is less. For example for -+3LSB it will be +-5°C due to ADC. Presume that you use&lt;/P&gt;&lt;P&gt;&amp;gt; hardware filtering on ADC.&lt;/P&gt;&lt;P&gt;&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Internal temp sensor is dedicated for approximate internal temperature measurement - not for&lt;/P&gt;&lt;P&gt;&amp;gt; precise measurement. Anyway by calibration you can achieve precision in °C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Agreed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Bhuvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 12:04:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391901#M4225</guid>
      <dc:creator>bhuvanchandradv</dc:creator>
      <dc:date>2015-09-22T12:04:41Z</dc:date>
    </item>
    <item>
      <title>Re: Calculating Vybrid CPU core temperature with the internal temperature sensor</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391902#M4226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hi &lt;SPAN&gt;Bhuvan&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;Slope coefficient remains. Only offset at 25&lt;SPAN lang="CS" style="mso-ansi-language: CS;"&gt;°C&lt;/SPAN&gt;&lt;SPAN lang="CS"&gt; &lt;/SPAN&gt;is little bit higher &lt;SPAN class="GramE"&gt;696 &lt;SPAN style="mso-spacerun: yes;"&gt;&amp;nbsp;&lt;/SPAN&gt;-&lt;/SPAN&gt;&amp;gt; 699 mV when 3.3V is used.&lt;/P&gt;&lt;P&gt;/Jiri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 13:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391902#M4226</guid>
      <dc:creator>jiri-b36968</dc:creator>
      <dc:date>2015-09-22T13:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: Calculating Vybrid CPU core temperature with the internal temperature sensor</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391903#M4227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri,&lt;/P&gt;&lt;P&gt;&amp;gt; Slope coefficient remains. Only offset at 25°C is little bit higher &lt;SPAN class="GramE"&gt;696&amp;nbsp; -&lt;/SPAN&gt;&amp;gt; 699 mV when 3.3V is used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok, thanks for the confirmation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Bhuvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 07:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391903#M4227</guid>
      <dc:creator>bhuvanchandradv</dc:creator>
      <dc:date>2015-09-23T07:04:17Z</dc:date>
    </item>
    <item>
      <title>Re: Calculating Vybrid CPU core temperature with the internal temperature sensor</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391904#M4228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hi &lt;SPAN&gt;Bhuvan&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;You are welcome - please close the thread by clicking on correct answer button. &lt;/P&gt;&lt;P&gt;/Jiri&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 07:26:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Calculating-Vybrid-CPU-core-temperature-with-the-internal/m-p/391904#M4228</guid>
      <dc:creator>jiri-b36968</dc:creator>
      <dc:date>2015-09-23T07:26:17Z</dc:date>
    </item>
  </channel>
</rss>