<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 Quartz Linux UARTs</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Quartz-Linux-UARTs/m-p/371142#M3882</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Recently I started working with a devicesolutions quartz development board and I have some issues with the UART ports. I'm using the factory build system (factory-20150202) and I atached my .config (It's quite similar to the default one) file to reproduce the error if someone wants to help me. U-boot uses the UART0 serial port (DB-9 connector) by default and Linux also uses it as the console terminal (ttymxc0), besides the operative system register two more serial ports ttymxc1 and ttymxc3. When I try to write to these ports (both using echo hello &amp;gt; /dev/ttymxc3, or using picocom), the system does not respond and crashes after some time because of a watchdog signaling.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone knows whats going wrong? When booting the board with the default SD card, I can see that it only registers two serial ports (ttymxc0 and ttymxc1) and both are working properly.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for you support,&lt;/P&gt;&lt;P&gt;Ibai Erkiaga&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338513"&gt;config.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Feb 2015 14:51:39 GMT</pubDate>
    <dc:creator>ierkiaga</dc:creator>
    <dc:date>2015-02-12T14:51:39Z</dc:date>
    <item>
      <title>Quartz Linux UARTs</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Quartz-Linux-UARTs/m-p/371142#M3882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Recently I started working with a devicesolutions quartz development board and I have some issues with the UART ports. I'm using the factory build system (factory-20150202) and I atached my .config (It's quite similar to the default one) file to reproduce the error if someone wants to help me. U-boot uses the UART0 serial port (DB-9 connector) by default and Linux also uses it as the console terminal (ttymxc0), besides the operative system register two more serial ports ttymxc1 and ttymxc3. When I try to write to these ports (both using echo hello &amp;gt; /dev/ttymxc3, or using picocom), the system does not respond and crashes after some time because of a watchdog signaling.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone knows whats going wrong? When booting the board with the default SD card, I can see that it only registers two serial ports (ttymxc0 and ttymxc1) and both are working properly.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for you support,&lt;/P&gt;&lt;P&gt;Ibai Erkiaga&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338513"&gt;config.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 14:51:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Quartz-Linux-UARTs/m-p/371142#M3882</guid>
      <dc:creator>ierkiaga</dc:creator>
      <dc:date>2015-02-12T14:51:39Z</dc:date>
    </item>
    <item>
      <title>Re: Quartz Linux UARTs</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Quartz-Linux-UARTs/m-p/371143#M3883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt; can you take this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Feb 2015 18:36:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Quartz-Linux-UARTs/m-p/371143#M3883</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2015-02-16T18:36:23Z</dc:date>
    </item>
    <item>
      <title>Re: Quartz Linux UARTs</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Quartz-Linux-UARTs/m-p/371144#M3884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ibai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working this same request which you submitted to the Timesys Support portal. We will follow up there, and please, do the same with any additional information you may have.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Feb 2015 18:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Quartz-Linux-UARTs/m-p/371144#M3884</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2015-02-20T18:01:27Z</dc:date>
    </item>
  </channel>
</rss>