<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 Re: Re: Vybrid TCON Configuration</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361275#M3712</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;Michael,&amp;nbsp; thanks for the email.&amp;nbsp; Hope the App note AN4635 I sent and our email discussion was helpful.&amp;nbsp; For your follow questions below I will provide my interpretation and ask Naoum &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/naoumgitnik"&gt;naoumgitnik&lt;/A&gt;&amp;nbsp; and also Melissa &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/melissah"&gt;melissah&lt;/A&gt; (author of AN4635, also copied) to confirm or clarify this if needed.....&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757;"&gt;---from Michael/Harris&amp;nbsp; via email------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757;"&gt;I looked through the app note and noticed this statement: “When the TCON is enabled, we will lose all of the DCU signals.” Is this only the clock timing signals or are the RGB signals lost as well?….&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757;"&gt;From the app note, it looks like the H_SYNC and V_SYNC signals need to be regenerated using the TCON comparators and pulse generators.&amp;nbsp; What about the pixel clock and the RGB signals?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757;"&gt;---------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; It looks like all DCU signals, Timing and RGB,&amp;nbsp; are routed thru TCON.&amp;nbsp; There are TCON settings and features to control the blanking of RGB data&amp;nbsp; and also drive the RGB data to either a "1"or "0" during blanking.&amp;nbsp; There are also several quotes in the reference manual that when the TCON is not in Bypass mode and is in active TTL mode....."TCON is functional, driving parallel RGB output and the TCON timing signals". .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For timing... the TCON accepts the HSYNC and VSYNC from the display interface, which go into the hcount and vcount registers, which are then used as the time base for generating all timing signals.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&amp;nbsp;&amp;nbsp; TCON also controls the Bit Mapping Control (BMC) to remap the Color Order&amp;nbsp; (RBG, BRG, GBR, etc) to the output pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;-Gordy&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Dec 2014 22:13:17 GMT</pubDate>
    <dc:creator>GordyCarlson</dc:creator>
    <dc:date>2014-12-01T22:13:17Z</dc:date>
    <item>
      <title>Vybrid TCON Configuration</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361271#M3708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Due to a hardware design issue, I need to bit swap the RGB lines coming out of the DCU to the LCD display.&amp;nbsp; There is configuration in the TCON to handle this, but I'm not sure what other configuration is needed to ensure all the display data lines are passed through.&amp;nbsp; Normally, we run the TCON in bypass mode, but since we need to swap the bit order of the RGB lines, I can no longer run with this module in bypass.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone successfully configured the TCON module, or do most people just run with it in bypass mode.&amp;nbsp; Is there any additional documentation on configuring the TCON module?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael Wilkerson-Barker&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Nov 2014 16:09:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361271#M3708</guid>
      <dc:creator>michaelwilkerso</dc:creator>
      <dc:date>2014-11-21T16:09:23Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid TCON Configuration</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361272#M3709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Michael,&lt;/P&gt;&lt;P&gt;We do not have any additional documentation just for the TCON module - only the Reference Manual document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dear &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt;, &lt;/P&gt;&lt;P&gt;May you comment on the customer's question if "&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 12.7272720336914px;"&gt;anyone successfully configured the TCON module" for the mode he interested in, please? Do you have anything to share here, please?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Nov 2014 20:53:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361272#M3709</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-11-21T20:53:32Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid TCON Configuration</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361273#M3710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently we are not able to offer immediate assistance, only that information provided in the reference manual document is immediately at hand.&lt;/P&gt;&lt;P&gt;We are not immediately aware of prior efforts to configure this module beyond it's default.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Nov 2014 14:51:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361273#M3710</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2014-11-24T14:51:12Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid TCON Configuration</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361274#M3711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you - I will reach out to our contacts at TI to see if they can provide assistance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael Wilkerson-Barker&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Nov 2014 14:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361274#M3711</guid>
      <dc:creator>michaelwilkerso</dc:creator>
      <dc:date>2014-11-24T14:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Vybrid TCON Configuration</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361275#M3712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;Michael,&amp;nbsp; thanks for the email.&amp;nbsp; Hope the App note AN4635 I sent and our email discussion was helpful.&amp;nbsp; For your follow questions below I will provide my interpretation and ask Naoum &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/naoumgitnik"&gt;naoumgitnik&lt;/A&gt;&amp;nbsp; and also Melissa &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/melissah"&gt;melissah&lt;/A&gt; (author of AN4635, also copied) to confirm or clarify this if needed.....&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757;"&gt;---from Michael/Harris&amp;nbsp; via email------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757;"&gt;I looked through the app note and noticed this statement: “When the TCON is enabled, we will lose all of the DCU signals.” Is this only the clock timing signals or are the RGB signals lost as well?….&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757;"&gt;From the app note, it looks like the H_SYNC and V_SYNC signals need to be regenerated using the TCON comparators and pulse generators.&amp;nbsp; What about the pixel clock and the RGB signals?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757;"&gt;---------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; It looks like all DCU signals, Timing and RGB,&amp;nbsp; are routed thru TCON.&amp;nbsp; There are TCON settings and features to control the blanking of RGB data&amp;nbsp; and also drive the RGB data to either a "1"or "0" during blanking.&amp;nbsp; There are also several quotes in the reference manual that when the TCON is not in Bypass mode and is in active TTL mode....."TCON is functional, driving parallel RGB output and the TCON timing signals". .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For timing... the TCON accepts the HSYNC and VSYNC from the display interface, which go into the hcount and vcount registers, which are then used as the time base for generating all timing signals.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000080;"&gt;&amp;nbsp;&amp;nbsp; TCON also controls the Bit Mapping Control (BMC) to remap the Color Order&amp;nbsp; (RBG, BRG, GBR, etc) to the output pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;-Gordy&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 22:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-TCON-Configuration/m-p/361275#M3712</guid>
      <dc:creator>GordyCarlson</dc:creator>
      <dc:date>2014-12-01T22:13:17Z</dc:date>
    </item>
  </channel>
</rss>