<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: QSPI_MCR[ISDnFx]</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353943#M3621</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Spansion QSPI memory used in Vybrid Tower card, has nonvolatile QUAD bit. Once you program it to 1, /HOLD and /WP pin functions are not used any more. It only matters how do you do initial Spansion memory programming. And for initial programming you can either drive /HOLD and /WP to required levels or set Vybrid pads to pull pads to the right direction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Oct 2014 08:49:35 GMT</pubDate>
    <dc:creator>kef2</dc:creator>
    <dc:date>2014-10-01T08:49:35Z</dc:date>
    <item>
      <title>QSPI_MCR[ISDnFx]</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353938#M3616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Vybrid manual claims that during QuadSPI commands IOFx[3:2] are "driven all the time, values taken from QSPI_MCR[ISDnFx]".&lt;/P&gt;&lt;P&gt;I can not find any information on these two bits in the documentation of the QSPIx_MCR register. Where can I find this information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other question is how to drive these two pins to HIGH during QuadSPI boot? Are there any undocumented eFuses for this purpose?&lt;/P&gt;&lt;P&gt;Currently, these pins are low during boot and thus the HOLD# pin is active, which leads to no data being transferred.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Adam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Sep 2014 12:37:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353938#M3616</guid>
      <dc:creator>adamszalkowski</dc:creator>
      <dc:date>2014-09-29T12:37:41Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI_MCR[ISDnFx]</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353939#M3617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Adam,&lt;/P&gt;&lt;P&gt;Please, take a look at the &lt;A href="https://community.nxp.com/message/352056"&gt;Re: QSPI I/03 Diven Low during all Single bit accesses&lt;/A&gt; thread.&lt;/P&gt;&lt;P&gt;Regards, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Sep 2014 20:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353939#M3617</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-09-29T20:13:46Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI_MCR[ISDnFx]</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353940#M3618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, apparently this means that IOF[3:2] pads are not driven in 1- and 2-bit modes.&lt;/P&gt;&lt;P&gt;I wonder how this is solved on the TWR-VF65GS10. There, IOF[3] is driven high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I doubt this is done by the PI3B3257QE. This part seems to only multiplex between SPI or QSPI.&lt;/P&gt;&lt;P&gt;I can not spot any pull-ups either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Sep 2014 07:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353940#M3618</guid>
      <dc:creator>adamszalkowski</dc:creator>
      <dc:date>2014-09-30T07:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI_MCR[ISDnFx]</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353941#M3619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Adam,&lt;/P&gt;&lt;P&gt;It might be high due to the Vybrid built-in pull-up being active... If you need all these details, it makes sense for your team to look into the Vybrid tower module's SW code; it is linked to on the Freescale &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 12.8000001907349px;"&gt;TWR-VF65GS10 web page as well as its location mentioned in the &lt;A href="https://community.nxp.com/message/436215"&gt;Re: Re: Re: Can I get working sources of U-BOOT 2013.07, nand?&lt;/A&gt;&lt;/SPAN&gt; and &lt;A href="https://community.nxp.com/message/378625"&gt;Re: Re: Using PLL5 for RMII-Clock&lt;/A&gt; threads.&lt;/P&gt;&lt;P&gt;Regards, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Sep 2014 20:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353941#M3619</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-09-30T20:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI_MCR[ISDnFx]</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353942#M3620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Naoum,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are talking here about the state during boot i.e. the boot ROM code. Do you have sources for that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Adam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2014 06:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353942#M3620</guid>
      <dc:creator>adamszalkowski</dc:creator>
      <dc:date>2014-10-01T06:08:27Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI_MCR[ISDnFx]</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353943#M3621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Spansion QSPI memory used in Vybrid Tower card, has nonvolatile QUAD bit. Once you program it to 1, /HOLD and /WP pin functions are not used any more. It only matters how do you do initial Spansion memory programming. And for initial programming you can either drive /HOLD and /WP to required levels or set Vybrid pads to pull pads to the right direction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2014 08:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353943#M3621</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2014-10-01T08:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI_MCR[ISDnFx]</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353944#M3622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Edward, thanks for the workaround.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway, still curious why QSPI0_A_D3 is driven high on the tower board during boot. Undocumented eFuses?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2014 09:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353944#M3622</guid>
      <dc:creator>adamszalkowski</dc:creator>
      <dc:date>2014-10-01T09:05:50Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI_MCR[ISDnFx]</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353945#M3623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Adam,&lt;/P&gt;&lt;P&gt;I guess it is caused by the bootROM code, and since in the mode of interest this bit is ignored by the memory chip, nobody worried about its configuration.&lt;/P&gt;&lt;P&gt;Sincerely, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 17:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/QSPI-MCR-ISDnFx/m-p/353945#M3623</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-10-02T17:08:36Z</dc:date>
    </item>
  </channel>
</rss>