<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 BootLoader Check</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/344129#M3470</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to do a first run on our carrier boards with PCM052 installed.&lt;/P&gt;&lt;P&gt;I then configured the SOM in the Phytec development board to boot from NAND flash it boots properly.&lt;/P&gt;&lt;P&gt;When I&amp;nbsp; place this SOM in our carrier board, it does not boot no traffic is seen in the RS232 TX or RX pins.&lt;/P&gt;&lt;P&gt;What the team observed on the TX line of the RS232 we see +6 rather than -6 as we would expect(this is what we observed in the Phytec development board), we see no outputs.&lt;/P&gt;&lt;P&gt;We have checked the reset sequence.&amp;nbsp; The external reset signal goes high about 25ms after power is applied.&amp;nbsp; Signals look clean.&lt;/P&gt;&lt;P&gt;The 3.3V for the SOM looks good. The 24MHz oscillator is running. &lt;/P&gt;&lt;P&gt;The signal level look the same as when it is running in the Phytec development board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Are there any test points to check to determine the SOM is properly booted aside from RS232?&lt;/P&gt;&lt;P&gt;- What needs to be check that might help me debug the issue.&lt;/P&gt;&lt;P&gt;- What other means to check the bootloader is loaded and booted correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help and advise would be greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Mar 2015 07:25:27 GMT</pubDate>
    <dc:creator>carlovalgocela</dc:creator>
    <dc:date>2015-03-24T07:25:27Z</dc:date>
    <item>
      <title>BootLoader Check</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/344129#M3470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to do a first run on our carrier boards with PCM052 installed.&lt;/P&gt;&lt;P&gt;I then configured the SOM in the Phytec development board to boot from NAND flash it boots properly.&lt;/P&gt;&lt;P&gt;When I&amp;nbsp; place this SOM in our carrier board, it does not boot no traffic is seen in the RS232 TX or RX pins.&lt;/P&gt;&lt;P&gt;What the team observed on the TX line of the RS232 we see +6 rather than -6 as we would expect(this is what we observed in the Phytec development board), we see no outputs.&lt;/P&gt;&lt;P&gt;We have checked the reset sequence.&amp;nbsp; The external reset signal goes high about 25ms after power is applied.&amp;nbsp; Signals look clean.&lt;/P&gt;&lt;P&gt;The 3.3V for the SOM looks good. The 24MHz oscillator is running. &lt;/P&gt;&lt;P&gt;The signal level look the same as when it is running in the Phytec development board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Are there any test points to check to determine the SOM is properly booted aside from RS232?&lt;/P&gt;&lt;P&gt;- What needs to be check that might help me debug the issue.&lt;/P&gt;&lt;P&gt;- What other means to check the bootloader is loaded and booted correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help and advise would be greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 07:25:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/344129#M3470</guid>
      <dc:creator>carlovalgocela</dc:creator>
      <dc:date>2015-03-24T07:25:27Z</dc:date>
    </item>
    <item>
      <title>Re: BootLoader Check</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/344130#M3471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt; can you help here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 18:36:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/344130#M3471</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2015-03-30T18:36:23Z</dc:date>
    </item>
    <item>
      <title>Re: BootLoader Check</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/344131#M3472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Carlo,&lt;/P&gt;&lt;P&gt;please check boot config pins: There are couple of them in table2-2 to 2-4 of &lt;A href="http://phytec.com/site/assets/files/1593/vybrid_hardware_manual_l-783e.pdf" title="http://phytec.com/site/assets/files/1593/vybrid_hardware_manual_l-783e.pdf"&gt;http://phytec.com/site/assets/files/1593/vybrid_hardware_manual_l-783e.pdf &lt;/A&gt;&lt;/P&gt;&lt;P&gt;MCU_PTB2, ....&lt;/P&gt;&lt;P&gt;/Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Mar 2015 06:25:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/344131#M3472</guid>
      <dc:creator>jiri-b36968</dc:creator>
      <dc:date>2015-03-31T06:25:40Z</dc:date>
    </item>
    <item>
      <title>Re: BootLoader Check</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/344132#M3473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;Good Day!&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;We fixed the issue by connecting MCU_PTB2 is set to GND.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;We missed this one because we haven't seen a documentation saying it needs to be controlled during boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Mar 2015 06:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/344132#M3473</guid>
      <dc:creator>carlovalgocela</dc:creator>
      <dc:date>2015-03-31T06:35:19Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/1135933#M6056</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 15:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BootLoader-Check/m-p/1135933#M6056</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T15:00:45Z</dc:date>
    </item>
  </channel>
</rss>