<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340264#M3350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt; do you have an update of this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jan 2015 16:59:18 GMT</pubDate>
    <dc:creator>karina_valencia</dc:creator>
    <dc:date>2015-01-16T16:59:18Z</dc:date>
    <item>
      <title>Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340253#M3339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Referring to&amp;nbsp; VYBRIDRM Rev 7, 06/2014:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Page 860: NAND Boot eFuse config appears to allow only 2 or 3 address cycles. Larger NAND devices require 4 or 5 cycles - does this mean I can't boot from them ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 14:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340253#M3339</guid>
      <dc:creator>alanball</dc:creator>
      <dc:date>2015-01-13T14:12:06Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340254#M3340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you have a data sheet on the 4/5 cycle chips?&amp;nbsp; Is it possible that they support a 3 cycle that only reads the first ~16MB.&amp;nbsp; You need to use a 3 cycle read command (also read command fues) and the boot code must be in the first ~16MB.&amp;nbsp; After you boot, you could try to access &amp;gt; 16MB with a 4/5 cycle command.&amp;nbsp; At least that is just some guessing and not an official answer, but seems to make some technical sense.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 15:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340254#M3340</guid>
      <dc:creator>billpringlemeir</dc:creator>
      <dc:date>2015-01-13T15:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340255#M3341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bill&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Datasheet (these are Spansion parts as it happens) says :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The Address Input bus operation allows the insertion of the memory address. For the S34ML02G1 and &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;S34ML04G1 devices, five write cycles are needed to input the addresses. For the S34ML01G1, four write &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;cycles are needed to input the addresses&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fair enough, the last one or two cycles are for high order row address, but there's nothing that states you can do a short load and the upper bits will then default to zero.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I note the Vybrid Tower uses a NAND chip (Micron) that implies the same thing , and I *assume* that must work...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 16:19:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340255#M3341</guid>
      <dc:creator>alanball</dc:creator>
      <dc:date>2015-01-13T16:19:29Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340256#M3342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alan,&lt;/P&gt;&lt;P&gt;I am not a SW person but the first question coming to my mind is "How does Freescale's code operate in this case"? If help needed with that, I hope &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt; (i.e. the code author) will be able to help you with that.&lt;/P&gt;&lt;P&gt;Sincerely, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 16:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340256#M3342</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2015-01-13T16:51:19Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340257#M3343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alan&lt;/P&gt;&lt;P&gt;&lt;SPAN class="n fn"&gt;Stefan Agner has some good experience &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="n fn"&gt;on Vybrid NAND. You might want to ping&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="n fn"&gt;him as well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="n fn"&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="n fn"&gt;Sinan Akman&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 17:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340257#M3343</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2015-01-13T17:03:18Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340258#M3344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry I did not reflect on your question enough, I am not certain what the &lt;EM&gt;Page 860: NAND Boot eFuse&lt;/EM&gt; refers to.&amp;nbsp; I think that the NFC controller always runs a five address cycle for normal reads.&amp;nbsp; See for instance, pg 1297 and &lt;EM&gt;NFC_CMD2:CODE&lt;/EM&gt;.&amp;nbsp; Nand Flash boot on the Vybrid tower does work without changing any fuses.&amp;nbsp; I am pretty sure that the JEDEC NAND standard will specify a read like this (5 cycles).&amp;nbsp; The low level details are completely controlled by the NFC and there is no documented programmer control of this besides the 'NFC_CMD2:CODE'.&amp;nbsp; Ie, most of the raw cycles are outside the ARM/software control.&amp;nbsp; Other Nand controller issue each cycle individually.&amp;nbsp; All of the different Linux/U-boot/MQX 'NFC' drivers use the same 'NFC_CMD2:CODE' value (so five cycle read).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question would be what does 'cycle' refer to in the Boot/eFuse document.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 21:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340258#M3344</guid>
      <dc:creator>billpringlemeir</dc:creator>
      <dc:date>2015-01-13T21:42:21Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340259#M3345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In RM rev. 5, there was a document attached with the name "Fuse-RCON Mapping.xlsx". In this document, you find the following descrption regarding this fuse (BOOT_CFG1[1:0]):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nand_Row_address_bytes:&lt;/P&gt;&lt;P&gt;00 - 3&lt;/P&gt;&lt;P&gt;01 - 2&lt;/P&gt;&lt;P&gt;10 - Reserved&lt;/P&gt;&lt;P&gt;11 - Reserved&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think this is not the cycle count of reads... Bill, you probably have a better understanding what this exactly means...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 23:34:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340259#M3345</guid>
      <dc:creator>falstaff</dc:creator>
      <dc:date>2015-01-13T23:34:48Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340260#M3346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I am not really sure Fuse-RCON Mapping.xlsx is much more helpful; the info is a lot the same as &lt;EM&gt;Page 860: NAND Boot eFuse&lt;/EM&gt;.&amp;nbsp; There are these threads,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/350133"&gt;Understanding VYBRID NAND Boot&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/341855"&gt;Re: Vybrid NAND boot&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Arrgh.&amp;nbsp; I guess the 'Fuse-RCON' may have the secret sauce if you read really carefully,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 0x00 col1 col2&amp;nbsp; row1 row2 row3 0x30&amp;nbsp; -&amp;gt; Five cycle (or 3 &lt;STRONG&gt;ROWS&lt;/STRONG&gt;)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 0x00 col1 col2&amp;nbsp; row1 row2 0x30&amp;nbsp; -&amp;gt; Four cycle (or 2 &lt;STRONG&gt;ROWS&lt;/STRONG&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I think that the Spansion 1G is 2 cycle, but the others are three.&amp;nbsp; That is just a guess.&amp;nbsp; Fuse defaults are zero and the Micron chip on the tower board with NAND boot with things setup as "3 Row cycles".&amp;nbsp; Pg860 should definitely mention &lt;STRONG&gt;ROWS&lt;/STRONG&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 00:07:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340260#M3346</guid>
      <dc:creator>billpringlemeir</dc:creator>
      <dc:date>2015-01-14T00:07:25Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340261#M3347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks - it starts to make sense&lt;/P&gt;&lt;P&gt;Do you know where I can get hold of Fuse-RCON_Mapping - it appears to not be attached to v7 of the manual ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 08:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340261#M3347</guid>
      <dc:creator>alanball</dc:creator>
      <dc:date>2015-01-14T08:48:21Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340262#M3348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Bill for the clarification. Fwiw, we use 00 for Macronix 1Gb/4Gb NAND chips.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;File is attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 09:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340262#M3348</guid>
      <dc:creator>falstaff</dc:creator>
      <dc:date>2015-01-14T09:52:52Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340263#M3349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Stefan (and Bill) - good to know there's lively, helpful support backing these parts :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 10:37:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340263#M3349</guid>
      <dc:creator>alanball</dc:creator>
      <dc:date>2015-01-14T10:37:43Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340264#M3350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt; do you have an update of this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 16:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340264#M3350</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2015-01-16T16:59:18Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340265#M3351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karina.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the issue is solved, but the original poster (Alan) doesn't know who solved it (and neither do I).&amp;nbsp; Also, it seems that the Freescale Vybrid document dropped an XLS spreadsheet and &lt;STRONG&gt;Page 860: NAND Boot eFuse&lt;/STRONG&gt; should probably be more specific about 'address cycle'.&amp;nbsp; Memory people often think of devices as an array with Columns and rows, but most of the rest of us think of it as a linear device.&amp;nbsp; So if you want to follow up, a ticket/SR to the documentation people is probably better.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Page 860: NAND Boot eFuse&amp;nbsp; - 2 &lt;STRONG&gt;ROW&lt;/STRONG&gt; address cycles (four address cycles total)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - 3 &lt;STRONG&gt;ROW&lt;/STRONG&gt; address cycles (five address cycles total)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would also appreciate a 'ping' in this thread,&lt;/P&gt;&lt;P&gt; &lt;A href="https://community.nxp.com/message/369202"&gt;VF6xxx NFC (NAND) module clocking&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I still don't think we have an answer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 17:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340265#M3351</guid>
      <dc:creator>billpringlemeir</dc:creator>
      <dc:date>2015-01-16T17:35:23Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid NAND Flash Controller (NFC) documentation ambiguity</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340266#M3352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank&amp;nbsp; Bill for your update on this&amp;nbsp; case. Based to the other&amp;nbsp; case you mentioned, can you create a new case with&amp;nbsp; this link as a reference and&amp;nbsp;&amp;nbsp; add the current status please?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 18:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-NAND-Flash-Controller-NFC-documentation-ambiguity/m-p/340266#M3352</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2015-01-16T18:06:53Z</dc:date>
    </item>
  </channel>
</rss>