<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 Synchronous Mode settings.</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/329094#M3189</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I refer Vybrid RM of Table 9-6. Synchronous Mode.&lt;/P&gt;&lt;P&gt;There are 4settings are &lt;SPAN class="hps"&gt;described&lt;/SPAN&gt;.. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN class="hps"&gt;Is&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;this&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the 4&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;settings&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;example&lt;/SPAN&gt;?&lt;/P&gt;&lt;P&gt; &lt;SPAN class="hps"&gt;Do&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Will&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Do not&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;other&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;settings&lt;/SPAN&gt;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to &lt;SPAN class="hps"&gt;the&lt;/SPAN&gt; &lt;SPAN&gt;connect&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;to&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;I2C &lt;/SPAN&gt;&lt;SPAN class="hps"&gt;rating&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of the destination &lt;/SPAN&gt;&lt;SPAN class="hps"&gt;will need to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;IPG&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;below&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;20MHz.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN class="hps"&gt;For example&lt;/SPAN&gt;,The&lt;SPAN class="hps"&gt;parameter&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;set is &lt;/SPAN&gt;PLL1-&amp;gt; PFD3 (396MHz), ARM_DIV = 1, BUS_DIV = 5, &lt;SPAN class="hps"&gt;IPG_DIV = 4 ,&lt;/SPAN&gt;&lt;SPAN class="hps"&gt;will be &lt;/SPAN&gt; &lt;SPAN class="hps"&gt;IPG = 19.8MHz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;But this settings not&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;stated&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Table 9-6.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;&lt;SPAN class="hps"&gt;Do&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the above&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;setting is&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;possible&lt;/SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN class="hps"&gt;For the use of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;there is no&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;parameter set&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;forth in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Table 9-6,&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;or&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;there is no&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;concern&lt;/SPAN&gt;?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2015 01:22:26 GMT</pubDate>
    <dc:creator>takashitakahash</dc:creator>
    <dc:date>2015-03-19T01:22:26Z</dc:date>
    <item>
      <title>Synchronous Mode settings.</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/329094#M3189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I refer Vybrid RM of Table 9-6. Synchronous Mode.&lt;/P&gt;&lt;P&gt;There are 4settings are &lt;SPAN class="hps"&gt;described&lt;/SPAN&gt;.. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN class="hps"&gt;Is&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;this&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the 4&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;settings&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;example&lt;/SPAN&gt;?&lt;/P&gt;&lt;P&gt; &lt;SPAN class="hps"&gt;Do&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Will&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Do not&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;other&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;settings&lt;/SPAN&gt;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to &lt;SPAN class="hps"&gt;the&lt;/SPAN&gt; &lt;SPAN&gt;connect&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;to&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN&gt;I2C &lt;/SPAN&gt;&lt;SPAN class="hps"&gt;rating&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of the destination &lt;/SPAN&gt;&lt;SPAN class="hps"&gt;will need to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;IPG&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;below&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;20MHz.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN class="hps"&gt;For example&lt;/SPAN&gt;,The&lt;SPAN class="hps"&gt;parameter&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;set is &lt;/SPAN&gt;PLL1-&amp;gt; PFD3 (396MHz), ARM_DIV = 1, BUS_DIV = 5, &lt;SPAN class="hps"&gt;IPG_DIV = 4 ,&lt;/SPAN&gt;&lt;SPAN class="hps"&gt;will be &lt;/SPAN&gt; &lt;SPAN class="hps"&gt;IPG = 19.8MHz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;But this settings not&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;stated&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Table 9-6.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;&lt;SPAN class="hps"&gt;Do&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the above&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;setting is&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;possible&lt;/SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN class="hps"&gt;For the use of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;there is no&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;parameter set&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;forth in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Table 9-6,&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;or&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;there is no&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;concern&lt;/SPAN&gt;?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2015 01:22:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/329094#M3189</guid>
      <dc:creator>takashitakahash</dc:creator>
      <dc:date>2015-03-19T01:22:26Z</dc:date>
    </item>
    <item>
      <title>Re: Synchronous Mode settings.</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/329095#M3190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked the documetation and those are just examples of clock settings.&lt;/P&gt;&lt;P&gt;But you can for sure set the IPG_CLK_DIV to 4, BUS_DIV to 5 too. This means that you can set the IPG clock below 20MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that helps,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 01:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/329095#M3190</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-03-26T01:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: Synchronous Mode settings.</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/329096#M3191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Takashi-san,&lt;/P&gt;&lt;P&gt;Synchronous setting requires that the platform clock (usually 133-166MHz) have to be half of SDRAM clock.&lt;/P&gt;&lt;P&gt;So first line in table is not correct (it should be deleted in next RM revision.)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50173i67B5213922AF9B68/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Synchronous mode is important only when is used SDRAM. If you not using SDRAM then you can use default asynchronous mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For I2C clock is important peripheral clock (IPS bus clock). It can be divided by CCM_CACRR [IPG_CLK_DIV]&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50176i3A0603AA5CA549E3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So if you need 20MHz then platform would have to be 80MHz only and CA5 and SDRAM 160MHz. This we degrade performance significantly.&lt;/P&gt;&lt;P&gt;If not used SDRAM than you can divide also platform clock.&lt;/P&gt;&lt;P&gt;But why you need just low IPS bus clock? I2C CLOCK divider can be set up to 15360 using MUL and divider.&lt;/P&gt;&lt;P&gt;/Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2015 08:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/329096#M3191</guid>
      <dc:creator>jiri-b36968</dc:creator>
      <dc:date>2015-03-27T08:53:37Z</dc:date>
    </item>
    <item>
      <title>Re: Synchronous Mode settings.</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/329097#M3192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lor for clarifying this Jiri!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 22:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/329097#M3192</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-03-30T22:20:27Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/1135628#M6043</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 14:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Synchronous-Mode-settings/m-p/1135628#M6043</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T14:41:10Z</dc:date>
    </item>
  </channel>
</rss>