<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 VADC on VF6xx</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317333#M3062</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I'm trying to use the module VADC of Vybrid intending to capture some video PAL frames.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are the test conditions:&lt;BR /&gt;- I used the Vybrid Reference Manual Rev. 5, 07/2013 to configure all the registers&lt;BR /&gt;- Toradex Module VF61 with a MVF61NS151CMK50 chip&lt;BR /&gt;- 4 Input VADC discoupled with 47nF e 75ohm to ground signal &lt;BR /&gt;- A standard PAL signal on each input channel originated from a SONY videocamera&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Modules configuration:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- PLL6 configured to 1064 MHz according to the 9-3 RM table&lt;BR /&gt;- PLL6 divided by 2 through the CCM_CACRR[PLL6_DIV_CLOCK] register&lt;BR /&gt;- PLL6 configured as a source of the VADC through the CCM_CSCMR1[VADC_CLK_SEL]register&lt;BR /&gt;- Clock of the VADC divided by 4 through the CCM_CSCDR1[VADC_DIV] register to obtain 133MHz&lt;BR /&gt;- Chosen VCAFE_VIN_0 through the AFE_INPFLT[mux_enlf] register&lt;BR /&gt;- Set pull-down VCAFE_VIN_1, VCAFE_VIN_2, VCAFE_VIN_3 through the AFE_OFFDRV[input_pulldown_en] register&lt;BR /&gt;- Enabled the clock to VADC through the CCM_CSCDR1[VADC_EN] register&lt;BR /&gt;- Introduced a 500ms delay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reading the&amp;nbsp; VDEC_VIDMOD[PAL detected] register I always obtain a 0 value: unrecognized PAL .&lt;BR /&gt;Furthermore I read the VDEC_VIDMOD[m625] register always active, with or without input signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, why is the VDEC_VIDMOD[PAL detected] register always null, nevertheless I connected a signal?&lt;BR /&gt;Is it necessary to configure some other register (AFE or VDEC) so that the VADC system could recognize the PAL standard?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Greetings&lt;BR /&gt;Antonio Boi &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jun 2014 12:10:40 GMT</pubDate>
    <dc:creator>antonioboi</dc:creator>
    <dc:date>2014-06-11T12:10:40Z</dc:date>
    <item>
      <title>VADC on VF6xx</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317333#M3062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I'm trying to use the module VADC of Vybrid intending to capture some video PAL frames.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are the test conditions:&lt;BR /&gt;- I used the Vybrid Reference Manual Rev. 5, 07/2013 to configure all the registers&lt;BR /&gt;- Toradex Module VF61 with a MVF61NS151CMK50 chip&lt;BR /&gt;- 4 Input VADC discoupled with 47nF e 75ohm to ground signal &lt;BR /&gt;- A standard PAL signal on each input channel originated from a SONY videocamera&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Modules configuration:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- PLL6 configured to 1064 MHz according to the 9-3 RM table&lt;BR /&gt;- PLL6 divided by 2 through the CCM_CACRR[PLL6_DIV_CLOCK] register&lt;BR /&gt;- PLL6 configured as a source of the VADC through the CCM_CSCMR1[VADC_CLK_SEL]register&lt;BR /&gt;- Clock of the VADC divided by 4 through the CCM_CSCDR1[VADC_DIV] register to obtain 133MHz&lt;BR /&gt;- Chosen VCAFE_VIN_0 through the AFE_INPFLT[mux_enlf] register&lt;BR /&gt;- Set pull-down VCAFE_VIN_1, VCAFE_VIN_2, VCAFE_VIN_3 through the AFE_OFFDRV[input_pulldown_en] register&lt;BR /&gt;- Enabled the clock to VADC through the CCM_CSCDR1[VADC_EN] register&lt;BR /&gt;- Introduced a 500ms delay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reading the&amp;nbsp; VDEC_VIDMOD[PAL detected] register I always obtain a 0 value: unrecognized PAL .&lt;BR /&gt;Furthermore I read the VDEC_VIDMOD[m625] register always active, with or without input signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, why is the VDEC_VIDMOD[PAL detected] register always null, nevertheless I connected a signal?&lt;BR /&gt;Is it necessary to configure some other register (AFE or VDEC) so that the VADC system could recognize the PAL standard?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Greetings&lt;BR /&gt;Antonio Boi &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 12:10:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317333#M3062</guid>
      <dc:creator>antonioboi</dc:creator>
      <dc:date>2014-06-11T12:10:40Z</dc:date>
    </item>
    <item>
      <title>Re: VADC on VF6xx</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317334#M3063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;May you refer Antonio to the code used on the Vybrid Automotive board - the one that also has 4 video inputs, please?&lt;/P&gt;&lt;P&gt;Sincerely, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 15:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317334#M3063</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-06-11T15:33:44Z</dc:date>
    </item>
    <item>
      <title>Re: VADC on VF6xx</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317335#M3064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, we do not have code for the Vybrid Automotive or the Toradex board for a VADC driver in Linux. I also checked MQX, and found related code at mqx/source/io/lwadc/, but I am not sure if this is what you are looking for.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 16:20:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317335#M3064</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2014-06-11T16:20:39Z</dc:date>
    </item>
    <item>
      <title>Re: VADC on VF6xx</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317336#M3065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #575757; font-size: 10pt; font-family: arial, helvetica, sans-serif;"&gt;Dear Antonio,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt; color: #575757;"&gt;Please, take a look at the attached simplified test code pieces - most likely they contain all the settings you are looking for.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt; color: #575757;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt; color: #575757;"&gt;I am not a SW person, but below is a comment of how to use the attached code (again, not sure how relevant it i but still...):&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757;"&gt;&lt;SPAN style="font-size: 11pt; font-family: Calibri, sans-serif;"&gt;“&lt;/SPAN&gt;&lt;SPAN style="font-size: 9.5pt; font-family: Helvetica, sans-serif;"&gt;I placed your code into my project, but it could not build. However, I removed Boot directly and changed build option to "Debug". Then I could build without errors. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757; font-size: 9.5pt; font-family: Helvetica, sans-serif;"&gt;I will download this project and run it.”&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt; color: #575757;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #575757; font-size: 10pt; font-family: arial, helvetica, sans-serif;"&gt;Regards, Naoum Gitnik.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 17:14:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317336#M3065</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-06-11T17:14:24Z</dc:date>
    </item>
    <item>
      <title>Re: VADC on VF6xx</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317337#M3066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;&lt;SPAN class="alt-edited hps"&gt;Thanks a lot &lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Naoum&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;&lt;SPAN class="hps"&gt;I will try&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;to use the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;code&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;that you shared&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;as a starting point&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;to test the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;module&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;VADC&lt;/SPAN&gt;. &lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class="hps"&gt;Regards,&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Antonio&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Boi&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 19:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VADC-on-VF6xx/m-p/317337#M3066</guid>
      <dc:creator>antonioboi</dc:creator>
      <dc:date>2014-06-12T19:31:26Z</dc:date>
    </item>
  </channel>
</rss>