<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flexcan with Vybrid VF6x and MQX4.1 in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Flexcan-with-Vybrid-VF6x-and-MQX4-1/m-p/311795#M2951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use the Flexcan for the BSP_VYBRID_AUTOEVB_A5.&lt;/P&gt;&lt;P&gt;I am using the the MQX 4.1 fsl_flexcan_driver, fsl_flexcan_hal and fsl_flexcan_int files.&lt;/P&gt;&lt;P&gt;The example code does not install the interrupt for the BSP_VYBRID_AUTOEVB_A5.&lt;/P&gt;&lt;P&gt;If I install the flexcan_irq_handler by using the FLEXCAN_Install_isr/FLEXCAN_Int_enable functions it constantly triggers the interrupt function but there are no Flags (IFLAG1 or ESR1) set for the trigger of the interrupt.&amp;nbsp; &lt;/P&gt;&lt;P&gt;No other code can run as the interrupt is constanly re-executed.&lt;/P&gt;&lt;P&gt;Are there any other triggers for the interrupt I am missing that are not cleared by the irq_handler - or any one any ideas ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Apr 2014 10:50:24 GMT</pubDate>
    <dc:creator>adrianverity</dc:creator>
    <dc:date>2014-04-07T10:50:24Z</dc:date>
    <item>
      <title>Flexcan with Vybrid VF6x and MQX4.1</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Flexcan-with-Vybrid-VF6x-and-MQX4-1/m-p/311795#M2951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use the Flexcan for the BSP_VYBRID_AUTOEVB_A5.&lt;/P&gt;&lt;P&gt;I am using the the MQX 4.1 fsl_flexcan_driver, fsl_flexcan_hal and fsl_flexcan_int files.&lt;/P&gt;&lt;P&gt;The example code does not install the interrupt for the BSP_VYBRID_AUTOEVB_A5.&lt;/P&gt;&lt;P&gt;If I install the flexcan_irq_handler by using the FLEXCAN_Install_isr/FLEXCAN_Int_enable functions it constantly triggers the interrupt function but there are no Flags (IFLAG1 or ESR1) set for the trigger of the interrupt.&amp;nbsp; &lt;/P&gt;&lt;P&gt;No other code can run as the interrupt is constanly re-executed.&lt;/P&gt;&lt;P&gt;Are there any other triggers for the interrupt I am missing that are not cleared by the irq_handler - or any one any ideas ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Apr 2014 10:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Flexcan-with-Vybrid-VF6x-and-MQX4-1/m-p/311795#M2951</guid>
      <dc:creator>adrianverity</dc:creator>
      <dc:date>2014-04-07T10:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: Flexcan with Vybrid VF6x and MQX4.1</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Flexcan-with-Vybrid-VF6x-and-MQX4-1/m-p/311796#M2952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For anyone else's informaiton, it was the Memory Error Detection and Correction Interrupts that were causing me the issue - these aren't implmeneted and therefore not cleared in the fsl_flexcan_driver code.. &lt;/P&gt;&lt;P&gt;CAN is now working..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Apr 2014 16:12:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Flexcan-with-Vybrid-VF6x-and-MQX4-1/m-p/311796#M2952</guid>
      <dc:creator>adrianverity</dc:creator>
      <dc:date>2014-04-07T16:12:37Z</dc:date>
    </item>
  </channel>
</rss>