<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB ports on VF65GS10 in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311182#M2933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Jiri. It works now. :)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 May 2014 01:39:47 GMT</pubDate>
    <dc:creator>zixet</dc:creator>
    <dc:date>2014-05-13T01:39:47Z</dc:date>
    <item>
      <title>USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311173#M2924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed Linux on sdcard using &lt;A href="http://eewiki.net/display/linuxonarm/TWR-VF65GS10"&gt;this&lt;/A&gt; instruction. When, I connect a USB flash to the board(J12), nothing happend! No device will be added to /dev directory.&lt;/P&gt;&lt;P&gt;Also, I have changed both J20 and J20 configuration but no luck!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know what's wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 May 2014 20:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311173#M2924</guid>
      <dc:creator>zixet</dc:creator>
      <dc:date>2014-05-06T20:58:51Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311174#M2925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Amir,&lt;/P&gt;&lt;P&gt;May you be a bit more specific, please, about the J21 jumper setting on the board (refer to its schematic)? E.g. the first thing to verify is if 5V power (USB1_VBUS) comes to your USB Flash drive and what voltage value.&lt;/P&gt;&lt;P&gt;Regards, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 May 2014 18:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311174#M2925</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-05-07T18:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311175#M2926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Naoum,&lt;/P&gt;&lt;P&gt;Jumper 21 has 4 pins. when I use wire jumper to connect pins 1-2 &amp;amp; pins 3-4, I can get 4.2v from USB1_VBUS. But, when I connect a USB stick which has a LED, it does not blink.&lt;/P&gt;&lt;P&gt;I want to use my USB as rootfs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 May 2014 21:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311175#M2926</guid>
      <dc:creator>zixet</dc:creator>
      <dc:date>2014-05-08T21:10:12Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311176#M2927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P style="margin:0in;margin-bottom:.0001pt;line-height:18.0pt"&gt;&lt;SPAN style="font-size:11.0pt;font-family: Calibri , sans-serif "&gt;Dear Amir, &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin:0in;margin-bottom:.0001pt;line-height:18.0pt;outline: 0;font-weight:inherit;font-style:inherit"&gt;&lt;SPAN style="font-size:11.0pt;font-family: Calibri , sans-serif "&gt;As I suspected, the voltage appeared to be too low to meet the USB specification (5.00±0.25 V). It is due to that the 5V rail in this case is powered from a PC via the on-board circuits with their voltage drops (refer to the schematic), and quite often that PC itself provides on its USB connector voltage quite low, although still within the specification limits. &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin:0in;margin-bottom:.0001pt;line-height:18.0pt"&gt;&lt;SPAN style="font-size:11.0pt;font-family: Calibri , sans-serif "&gt;We also observed such behavior; e.g. you may try to have a shunt between J21.1 and J21.2 (for Vybrid itself) but connect an external 5V source to J21.3 (for the USB Flash drive).&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin:0in;margin-bottom:.0001pt;line-height:18.0pt"&gt;&lt;SPAN style="font-size:11.0pt;font-family: Calibri , sans-serif "&gt;Unfortunately, this is a negative by-product of the compact, USB-powered Tower board topology. This issue is partially taken into account for the case when it is used as a part of the Tower kit - in this case the kit as a whole has special terminals to be connected to an external 5V source.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin:0in;margin-bottom:.0001pt;line-height:18.0pt"&gt;&lt;SPAN style="font-size:11.0pt;font-family: Calibri , sans-serif "&gt;Please, let me know if it helps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin:0in;margin-bottom:.0001pt;line-height:18.0pt"&gt;&lt;SPAN style="font-size:11.0pt;font-family: Calibri , sans-serif "&gt;Regards, Naoum Gitnik. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 May 2014 23:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311176#M2927</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-05-08T23:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311177#M2928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the answer.&lt;/P&gt;&lt;P&gt;Is there any header(pin) on the board that I can connect the ground wire of the external source to it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 May 2014 14:24:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311177#M2928</guid>
      <dc:creator>zixet</dc:creator>
      <dc:date>2014-05-09T14:24:36Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311178#M2929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN style="mso-bidi-font-family:Calibri"&gt;Dear Amir,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="mso-bidi-font-family:Calibri"&gt;You may use the TP13 or TP16 test points connected to GND.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="mso-bidi-font-family:Calibri"&gt;Regards, Naoum Gitnik.&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 May 2014 15:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311178#M2929</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-05-09T15:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311179#M2930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Naoum,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apply 4.94V to J21.3 and put a shunt between J21.1 and J21.2. But, the light does not blink and no message is shown in dmesg.&lt;/P&gt;&lt;P&gt;Also, I have checked the USB port voltage again.(4.94V)&lt;/P&gt;&lt;P&gt;Here is the picture of the current configuration.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMG_20140509_143412.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43995i2E41FAD91C8579B8/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMG_20140509_143412.jpg" alt="IMG_20140509_143412.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Amir&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 May 2014 18:39:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311179#M2930</guid>
      <dc:creator>zixet</dc:creator>
      <dc:date>2014-05-09T18:39:37Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311180#M2931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Dear Amir,&lt;/P&gt;&lt;P&gt;Just a couple comments:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;It is clear now that you are using a Tower kit, so it would be better to apply 5V not to the Vybrid board directly but through the terminal block (black, with 2 screws, marked Power and 5V) on one of the Elevator boards. For details, refer to Freescale materials about the Tower kit approach.&lt;/LI&gt;&lt;LI&gt;Do you see any signals on the two Data lines of the USB connector used? - If there is no activity there, the issue is rather software than hardware.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Regards, Naoum Gitnik.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(&lt;A __default_attr="209275" _jive_internal="true" data-objecttype="3" href="https://community.nxp.com/people/jiri-b36968" jivemacro="user"&gt;Jiri Kotzian&lt;/A&gt; - FYI)&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 May 2014 21:08:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311180#M2931</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2014-05-09T21:08:23Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311181#M2932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Amir,&lt;/P&gt;&lt;P&gt;1. Tower module have all necessary power for J12. Use default configuration of J21 1-2, 3-4 no other wires. J12 is powered from USB1_VBUS. This is sourced from U8/P5V_USB1 - output is enabled by default (Linux can disable it).&lt;/P&gt;&lt;P&gt;2. to USB stick working properly, you need &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;g_file_storage gadget. &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;The kernel module does not get built by default. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;not sure if it is in your SDK. If you use desktop factory, navigate to your top-level Factory directory and run 'make kernel-menuconfig'. Navigate to: &lt;/P&gt;&lt;P&gt;Device Drivers &amp;gt; USB support &amp;gt; USB Gadget Support &amp;gt; File-backed Storage Gadget &lt;/P&gt;&lt;P&gt;And select this option as 'M'. Save and exit kernel configuration, and run 'make' to rebuild. The RFS image at build_*/images/rfs/ will now have the g_file_storage gadget.&lt;/P&gt;&lt;P&gt;/Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 May 2014 07:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311181#M2932</guid>
      <dc:creator>jiri-b36968</dc:creator>
      <dc:date>2014-05-12T07:41:09Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311182#M2933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Jiri. It works now. :)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 May 2014 01:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311182#M2933</guid>
      <dc:creator>zixet</dc:creator>
      <dc:date>2014-05-13T01:39:47Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311183#M2934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jiri, I tried to update the Kernel version to the newer one like 3.10 but I could not find "File-backed Storage Gadget" option anymore. Why has it been removed? Did they change the name? I check all of the options under "USB Gadget Support" but seems none of them lets USB to appear as SCSI disk drive. Could you please help me with that?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 May 2014 17:35:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311183#M2934</guid>
      <dc:creator>zixet</dc:creator>
      <dc:date>2014-05-28T17:35:51Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311184#M2935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, I found the problem. It seems that the kernel that TimeSys customized for Vybrid Tower has one extra option in menuconfig that if I disable them, USB controller does not work.&lt;BR /&gt;I have marked those two extra options in the attached image.&lt;/P&gt;&lt;P&gt;Now, the question is how can add that module to my new kernel?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="vybrid_kernel.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44174i6729BF4B42006E60/image-size/large?v=v2&amp;amp;px=999" role="button" title="vybrid_kernel.png" alt="vybrid_kernel.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 May 2014 22:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311184#M2935</guid>
      <dc:creator>zixet</dc:creator>
      <dc:date>2014-05-28T22:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: USB ports on VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311185#M2936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amir,&lt;/P&gt;&lt;P&gt;module can be added after boot using modprobe. For example modprobe g_ether&lt;/P&gt;&lt;P&gt;But please look at timesys web page - they are SW specialist. &lt;/P&gt;&lt;P&gt;/Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 May 2014 09:31:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-ports-on-VF65GS10/m-p/311185#M2936</guid>
      <dc:creator>jiri-b36968</dc:creator>
      <dc:date>2014-05-29T09:31:02Z</dc:date>
    </item>
  </channel>
</rss>