<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: Do I need two USB connection for MFGToolkit?</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Do-I-need-two-USB-connection-for-MFGToolkit/m-p/305440#M2772</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My board is selfpowered, not USB bus powered.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Apr 2014 13:52:53 GMT</pubDate>
    <dc:creator>kef2</dc:creator>
    <dc:date>2014-04-28T13:52:53Z</dc:date>
    <item>
      <title>Do I need two USB connection for MFGToolkit?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Do-I-need-two-USB-connection-for-MFGToolkit/m-p/305437#M2769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have VF3x prototype, which we could program the on board QSPI chips with last MFGtoolkit SW. I noticed that I if I connect only VF3x USB(0), MFGtoolkit gives "no device connected message". If we also connect the openSDA USB, then MFGToolkit can identify the VF3x and can program it. This may be tolerable for prototype;&lt;/P&gt;&lt;P&gt;but for the production, Do I need both USB's?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 12:35:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Do-I-need-two-USB-connection-for-MFGToolkit/m-p/305437#M2769</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2014-04-28T12:35:14Z</dc:date>
    </item>
    <item>
      <title>Re: Do I need two USB connection for MFGToolkit?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Do-I-need-two-USB-connection-for-MFGToolkit/m-p/305438#M2770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mehmet,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is your board powered via OpenSDA USB?&lt;/P&gt;&lt;P&gt;I believe it is not required. I managed to program with MFGtoolkit my own board via USB0. Blank Spansion QSPI memory programs well. There's no OpenSDA on board, USB1 port is not used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 13:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Do-I-need-two-USB-connection-for-MFGToolkit/m-p/305438#M2770</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2014-04-28T13:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: Do I need two USB connection for MFGToolkit?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Do-I-need-two-USB-connection-for-MFGToolkit/m-p/305439#M2771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Edward,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes I have both USB and a 5 Volt connector; There is only USB power(not openSDA, but USB0 of VF3x) at the moment. Did you use seperate power supply?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 13:39:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Do-I-need-two-USB-connection-for-MFGToolkit/m-p/305439#M2771</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2014-04-28T13:39:05Z</dc:date>
    </item>
    <item>
      <title>Re: Do I need two USB connection for MFGToolkit?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Do-I-need-two-USB-connection-for-MFGToolkit/m-p/305440#M2772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My board is selfpowered, not USB bus powered.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 13:52:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Do-I-need-two-USB-connection-for-MFGToolkit/m-p/305440#M2772</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2014-04-28T13:52:53Z</dc:date>
    </item>
  </channel>
</rss>