<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VF3x USB connection in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-USB-connection/m-p/293580#M2425</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mehmet,&lt;/P&gt;&lt;P&gt;One of the 2 USB ports (refer to the documentation which one) can be used for booting, so when connected to a PC, it enumerates, and Vybrid appears among the devices on the Device Manager list.&lt;/P&gt;&lt;P&gt;Regards, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Sep 2013 21:00:21 GMT</pubDate>
    <dc:creator>naoumgitnik</dc:creator>
    <dc:date>2013-09-10T21:00:21Z</dc:date>
    <item>
      <title>VF3x USB connection</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-USB-connection/m-p/293579#M2424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Vybrid support team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a VF3x board which has UART and USB interface. I have connected the UART interface to the PC with terminal SW, and its responding 0x23454523 sequence.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How should I test the USB interface? &lt;/P&gt;&lt;P&gt;Which parameters should I measure/check?&lt;/P&gt;&lt;P&gt;If hardware is correct, Is it a plug and play interface to the PC, so that should I see a new device connection in Windows?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am drawing about 100 mA from 5Volts power supply. May I draw this amount of current from PC's USB port? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mehmet Ali Ipin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2013 11:16:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-USB-connection/m-p/293579#M2424</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2013-09-09T11:16:20Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x USB connection</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-USB-connection/m-p/293580#M2425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mehmet,&lt;/P&gt;&lt;P&gt;One of the 2 USB ports (refer to the documentation which one) can be used for booting, so when connected to a PC, it enumerates, and Vybrid appears among the devices on the Device Manager list.&lt;/P&gt;&lt;P&gt;Regards, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Sep 2013 21:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-USB-connection/m-p/293580#M2425</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2013-09-10T21:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x USB connection</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-USB-connection/m-p/293581#M2426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Naoum,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your helps. When I removed pull up resistors on USB_0 DM and USB0_DP lines, windows recognized my VF3x board, I saw Vybrid message and our hardware is connected as HID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you any idea if PC allow 500 mA from its USB_VBUS port pin to USB device, without USB device going to suspend mode? I don't want to use extra power supply,&amp;nbsp; I mean, may I use USB port VBUS pin as a 5V and 500 mA power supply?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and with my best regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mehmet Ali Ipin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2013 12:11:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-USB-connection/m-p/293581#M2426</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2013-09-11T12:11:14Z</dc:date>
    </item>
  </channel>
</rss>