<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid Processors中的主题 Re: Vybrid USB OTG ID</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-USB-OTG-ID/m-p/292733#M2357</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Craig,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe the documentation says that the USB controller is not a full OTG controller. It is dual role and can be used either as peripheral controller or as Host controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ID bit is present in the OTGSC register because the controller IP does support full OTG functionality. It is just not implemented in Vybrid. Considder this a documentation issue. I'll mark it for correction in the next revision of the manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your application does need to know whether an A- or B-type plug is inserted, you can use a GPIO imput with a pull-up resistor to determine the state of the connector's ID pin and configure the controller accordingly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Richard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 May 2013 21:10:02 GMT</pubDate>
    <dc:creator>richard_stulens</dc:creator>
    <dc:date>2013-05-24T21:10:02Z</dc:date>
    <item>
      <title>Vybrid USB OTG ID</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-USB-OTG-ID/m-p/292732#M2356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could anyone designing with the Vybrid family of processors tell me if there is any hardware mechanism for setting/clearing the USB ID bit in the USBx_OTGSC register using an externally accessible signal?&amp;nbsp; I have not been able to find any reference to an OTG ID pin in the preliminary documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If there isn't any mechanism, why is this bit here? How is it used?&amp;nbsp; How do you inform the processor of the presence of an A or B type device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Craig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Mar 2013 00:51:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-USB-OTG-ID/m-p/292732#M2356</guid>
      <dc:creator>CraigL</dc:creator>
      <dc:date>2013-03-13T00:51:48Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid USB OTG ID</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-USB-OTG-ID/m-p/292733#M2357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Craig,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe the documentation says that the USB controller is not a full OTG controller. It is dual role and can be used either as peripheral controller or as Host controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ID bit is present in the OTGSC register because the controller IP does support full OTG functionality. It is just not implemented in Vybrid. Considder this a documentation issue. I'll mark it for correction in the next revision of the manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your application does need to know whether an A- or B-type plug is inserted, you can use a GPIO imput with a pull-up resistor to determine the state of the connector's ID pin and configure the controller accordingly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Richard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 May 2013 21:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-USB-OTG-ID/m-p/292733#M2357</guid>
      <dc:creator>richard_stulens</dc:creator>
      <dc:date>2013-05-24T21:10:02Z</dc:date>
    </item>
  </channel>
</rss>