<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VF61/Vybrid, is this semaphore function in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/VF61-Vybrid-is-this-semaphore-function/m-p/291866#M2326</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, there are hardware semaphores that can be (are intended to be) used between the M4 and A5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case of MQX on both the A5 and M4 or Linux on the A5 and MQX on the M4, there are demos available in the Timesys BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCC (multicore communication system) between MQX on both or Linux / MQX also uses them to protect shared memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One nice feature is that if access is denied, you can program the semaphore to issue an interrupt when it is freed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Sep 2013 17:39:08 GMT</pubDate>
    <dc:creator>ed_nash</dc:creator>
    <dc:date>2013-09-05T17:39:08Z</dc:date>
    <item>
      <title>VF61/Vybrid, is this semaphore function</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF61-Vybrid-is-this-semaphore-function/m-p/291865#M2325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about A3.4 Synchronization and semaphores(A3-12)/ DDI0406BJ_arm_architecture_reference_manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="popupW"&gt;In &lt;SPAN class="popupW"&gt;the&lt;/SPAN&gt; multi-core (A5+M4) &lt;SPAN class="popupW"&gt;of&lt;/SPAN&gt; &lt;SPAN class="popupW"&gt;Vybrid&lt;/SPAN&gt;, &lt;SPAN class="popupW"&gt;is&lt;/SPAN&gt; &lt;SPAN class="popupW"&gt;this&lt;/SPAN&gt; &lt;SPAN class="popupW"&gt;semaphore&lt;/SPAN&gt; &lt;SPAN class="popupW"&gt;function&lt;/SPAN&gt; &lt;SPAN class="popupW"&gt;usable&lt;/SPAN&gt;?&lt;BR /&gt;&lt;SPAN class="popupW" style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="popupW"&gt;&lt;SPAN class="popupW" style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="popupW"&gt;&lt;SPAN class="popupW" style="font-size: 10pt; line-height: 1.5em;"&gt;And&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; &lt;/SPAN&gt;&lt;SPAN class="popupW" style="font-size: 10pt; line-height: 1.5em;"&gt;is&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; &lt;/SPAN&gt;&lt;SPAN class="popupW" style="font-size: 10pt; line-height: 1.5em;"&gt;exclusive&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; &lt;/SPAN&gt;&lt;SPAN class="popupW" style="font-size: 10pt; line-height: 1.5em;"&gt;control&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; &lt;/SPAN&gt;&lt;SPAN class="popupW" style="font-size: 10pt; line-height: 1.5em;"&gt;possible&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; &lt;/SPAN&gt;&lt;SPAN class="popupW" style="font-size: 10pt; line-height: 1.5em;"&gt;between&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; multi-core(A5+M4) ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;soichi yamamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 10:27:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF61-Vybrid-is-this-semaphore-function/m-p/291865#M2325</guid>
      <dc:creator>soichiyamamoto</dc:creator>
      <dc:date>2013-09-05T10:27:43Z</dc:date>
    </item>
    <item>
      <title>Re: VF61/Vybrid, is this semaphore function</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF61-Vybrid-is-this-semaphore-function/m-p/291866#M2326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, there are hardware semaphores that can be (are intended to be) used between the M4 and A5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case of MQX on both the A5 and M4 or Linux on the A5 and MQX on the M4, there are demos available in the Timesys BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCC (multicore communication system) between MQX on both or Linux / MQX also uses them to protect shared memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One nice feature is that if access is denied, you can program the semaphore to issue an interrupt when it is freed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 17:39:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF61-Vybrid-is-this-semaphore-function/m-p/291866#M2326</guid>
      <dc:creator>ed_nash</dc:creator>
      <dc:date>2013-09-05T17:39:08Z</dc:date>
    </item>
  </channel>
</rss>