<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックInstallation for Vybrid VF65GS10</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Installation-for-Vybrid-VF65GS10/m-p/290533#M2270</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Hello, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;OP: I'm working on the Vybrid (TWR-VF65GS10) and am currently installing the hardware with the help of the "Quick Start Guide" (Doc # TWRVF65GS10QSG Rev 0). On pages 5 and 7, there's a reference to installation software at "Jump Start Your Design" and a lab guide, respectively, both at freescale.com/TWR- VF65GS10. However, I can't find either at the website, and I'm having trouble getting the tower module to connect to the computer. Also, the micro-USB-to-USB cable that came with the kit has two USB heads on the USB end of the cable. What are the two heads for?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Update: I mostly fixed the problem by connecting the microUSB-USB to J3 and the computer in order to supply power to the board, and am using a J-link for debugging. However, if it's possible to use just the microUSB-USB, I'd prefer to do that. There's also some mention in the lab guide of drivers that should be automatically installed when I connect the tower to the computer via microUSB-USB. However, I haven't been able to get that work. If it helps, I'm using Windows XP and IAR for debugging.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Thanks.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jun 2013 16:58:53 GMT</pubDate>
    <dc:creator>n00b1024</dc:creator>
    <dc:date>2013-06-13T16:58:53Z</dc:date>
    <item>
      <title>Installation for Vybrid VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Installation-for-Vybrid-VF65GS10/m-p/290533#M2270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Hello, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;OP: I'm working on the Vybrid (TWR-VF65GS10) and am currently installing the hardware with the help of the "Quick Start Guide" (Doc # TWRVF65GS10QSG Rev 0). On pages 5 and 7, there's a reference to installation software at "Jump Start Your Design" and a lab guide, respectively, both at freescale.com/TWR- VF65GS10. However, I can't find either at the website, and I'm having trouble getting the tower module to connect to the computer. Also, the micro-USB-to-USB cable that came with the kit has two USB heads on the USB end of the cable. What are the two heads for?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Update: I mostly fixed the problem by connecting the microUSB-USB to J3 and the computer in order to supply power to the board, and am using a J-link for debugging. However, if it's possible to use just the microUSB-USB, I'd prefer to do that. There's also some mention in the lab guide of drivers that should be automatically installed when I connect the tower to the computer via microUSB-USB. However, I haven't been able to get that work. If it helps, I'm using Windows XP and IAR for debugging.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Thanks.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 16:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Installation-for-Vybrid-VF65GS10/m-p/290533#M2270</guid>
      <dc:creator>n00b1024</dc:creator>
      <dc:date>2013-06-13T16:58:53Z</dc:date>
    </item>
    <item>
      <title>Re: Installation for Vybrid VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Installation-for-Vybrid-VF65GS10/m-p/290534#M2271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; You didn't have access to this before now, but the &lt;A href="https://community.nxp.com/docs/DOC-94802"&gt;Vybrid FAQ &lt;/A&gt;will answer most of your questions. The website is not launched yet, but will work when Vybrid is public. The two heads are to provide extra current if needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; And you have to use a JLink if debugging with IAR. An OpenSDA app for emulating a JLink that works with Vybrid is being worked on though, so that won't always be a requirement in the future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; If it didn't cover something, let us know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 18:05:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Installation-for-Vybrid-VF65GS10/m-p/290534#M2271</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2013-06-13T18:05:30Z</dc:date>
    </item>
  </channel>
</rss>