<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Processor expert project for the Vybrid Tower board TWR-VF65GS10 in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280494#M1993</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I suspect that these examples were based on the VF5xx parts instead of the VF6xx because when these examples were created, the VF6xx parts may not have been available yet. The dates on the example PEx-Generated code is Feb 27, 2013.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I imported those examples into my Workspace in DS-5 (Ubuntu), but I am not able to build it - those examples are targeted for the IAR tool chain on Windows. However, I used them as examples to build my own PEx project. They were useful because they allowed me to see how the parameters of the components are configured etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Feb 2014 22:00:18 GMT</pubDate>
    <dc:creator>jackblather</dc:creator>
    <dc:date>2014-02-07T22:00:18Z</dc:date>
    <item>
      <title>Processor expert project for the Vybrid Tower board TWR-VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280489#M1988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a Processor Expert sample project for the Vybrid Tower board TWR-VF65GS10?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2014 23:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280489#M1988</guid>
      <dc:creator>adiroot</dc:creator>
      <dc:date>2014-02-05T23:48:28Z</dc:date>
    </item>
    <item>
      <title>Re: Processor expert project for the Vybrid Tower board TWR-VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280490#M1989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Look here: &lt;A href="https://community.nxp.com/docs/DOC-95073"&gt;Where can I find Processor Expert examples and tutorials in Driver Suite?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you're using Linux as a development host, go to this directory:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~/.ds-5/workbench/ProcessorExpert/Projects/TWR-VF65GS10&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Processor Expert on the TWR-VF65GS10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2014 23:54:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280490#M1989</guid>
      <dc:creator>jackblather</dc:creator>
      <dc:date>2014-02-05T23:54:03Z</dc:date>
    </item>
    <item>
      <title>Re: Processor expert project for the Vybrid Tower board TWR-VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280491#M1990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jack.&amp;nbsp; However, despite the fact that the folder is called TWR-VF65GS10, those projects are not for that tower!.&amp;nbsp; &lt;/P&gt;&lt;P&gt;The example projects all call out to the SVF512R3MK4 CPU.&amp;nbsp; The TWR-VF65GS10 tower board has the VF61GS151CMK50 CPU on it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2014 18:01:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280491#M1990</guid>
      <dc:creator>adiroot</dc:creator>
      <dc:date>2014-02-06T18:01:35Z</dc:date>
    </item>
    <item>
      <title>Re: Processor expert project for the Vybrid Tower board TWR-VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280492#M1991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt; can you help with this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2014 22:51:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280492#M1991</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2014-02-06T22:51:09Z</dc:date>
    </item>
    <item>
      <title>Re: Processor expert project for the Vybrid Tower board TWR-VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280493#M1992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using the Microcontrollers Driver Suite v10.3 plug-in for existing Eclipse via the following link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PE_DRIVER_SUITE&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PE_DRIVER_SUITE&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;PE_DRIVER_SUITE: Processor Expert Software, Microcontroller Driver Suite&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We can confirm that the SVF512R3MK4 CPU is used for projects under ~/.ds-5/workbench/ProcessorExpert/Projects/TWR-VF65GS10. &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jackblather"&gt;jackblather&lt;/A&gt; have you used these sample projects with the Vybrid Tower? Do you know why the CPU for these projects differs from that which is on the tower?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2014 21:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280493#M1992</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2014-02-07T21:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: Processor expert project for the Vybrid Tower board TWR-VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280494#M1993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I suspect that these examples were based on the VF5xx parts instead of the VF6xx because when these examples were created, the VF6xx parts may not have been available yet. The dates on the example PEx-Generated code is Feb 27, 2013.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I imported those examples into my Workspace in DS-5 (Ubuntu), but I am not able to build it - those examples are targeted for the IAR tool chain on Windows. However, I used them as examples to build my own PEx project. They were useful because they allowed me to see how the parameters of the components are configured etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2014 22:00:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280494#M1993</guid>
      <dc:creator>jackblather</dc:creator>
      <dc:date>2014-02-07T22:00:18Z</dc:date>
    </item>
    <item>
      <title>Re: Processor expert project for the Vybrid Tower board TWR-VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280495#M1994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt; can you continue with the follow up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 22:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280495#M1994</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2014-02-13T22:25:38Z</dc:date>
    </item>
    <item>
      <title>Re: Processor expert project for the Vybrid Tower board TWR-VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280496#M1995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As Jack has said, it does not appear that the VF6xx PEx projects are available at this time. You may use them as a guideline to build your own PEx project for the Vybrid.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 15:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280496#M1995</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2014-02-14T15:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: Processor expert project for the Vybrid Tower board TWR-VF65GS10</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280497#M1996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am curious, are the VF6xx PEx projects are available now?&lt;/P&gt;&lt;P&gt;if yes then can someone point me out to them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 15:57:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Processor-expert-project-for-the-Vybrid-Tower-board-TWR-VF65GS10/m-p/280497#M1996</guid>
      <dc:creator>harshadlele</dc:creator>
      <dc:date>2016-07-20T15:57:05Z</dc:date>
    </item>
  </channel>
</rss>