<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can Vybrid boot from the only QSPI_B? in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Can-Vybrid-boot-from-the-only-QSPI-B/m-p/279825#M1965</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hiroki,&lt;/P&gt;&lt;P&gt;&amp;nbsp; That's correct, you must always boot from QSPI_A. You can use QuadSPI0 or QuadSPI1, as that is selected by fuses, but on QuadSPI0 you have to have all the information in QuadSPI0_A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; See this thread for more information on QuadSPI booting. &lt;A href="https://community.nxp.com/message/337277"&gt;Parallel QuadSPI&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jul 2013 17:54:19 GMT</pubDate>
    <dc:creator>anthony_huereca</dc:creator>
    <dc:date>2013-07-23T17:54:19Z</dc:date>
    <item>
      <title>Can Vybrid boot from the only QSPI_B?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Can-Vybrid-boot-from-the-only-QSPI-B/m-p/279824#M1964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can Vybrid boot from a QSPI Flash connected only the QSPI_B?&lt;/P&gt;&lt;P&gt;When the QSPI boot, First, the Vybrid set the pin mux and tries to get the QSPI configuration parameter from all Flash.&lt;/P&gt;&lt;P&gt;QSPI_A is always enabled but the optional configuration is that QSPI_B is enabled. So I think the Vybrid cannot boot from the only QSPI_B flash. Is it correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2013 09:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Can-Vybrid-boot-from-the-only-QSPI-B/m-p/279824#M1964</guid>
      <dc:creator>Hiroki</dc:creator>
      <dc:date>2013-07-18T09:15:22Z</dc:date>
    </item>
    <item>
      <title>Re: Can Vybrid boot from the only QSPI_B?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Can-Vybrid-boot-from-the-only-QSPI-B/m-p/279825#M1965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hiroki,&lt;/P&gt;&lt;P&gt;&amp;nbsp; That's correct, you must always boot from QSPI_A. You can use QuadSPI0 or QuadSPI1, as that is selected by fuses, but on QuadSPI0 you have to have all the information in QuadSPI0_A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; See this thread for more information on QuadSPI booting. &lt;A href="https://community.nxp.com/message/337277"&gt;Parallel QuadSPI&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2013 17:54:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Can-Vybrid-boot-from-the-only-QSPI-B/m-p/279825#M1965</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2013-07-23T17:54:19Z</dc:date>
    </item>
  </channel>
</rss>