<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: VF3x reset, serial bootload</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277038#M1836</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Naoum,&lt;/P&gt;&lt;P&gt;Thank you for your helps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. We are using our Own design&lt;/P&gt;&lt;P&gt;2. I checked the power sequence, and saw that the USB_V0 has the only 10 micro second after the 5 Volt is applied, while the 1.1V Vdd has 100 microsecond delay. There was a load switch between external 5 Volts to USB_V0, which was controlled by BCTRL signal. But it was not working, so I removed it, but I could not see any improvement.&lt;/P&gt;&lt;P&gt;3. blue line is for XTAL. I noticed that the voltage level (600 mVolt) is below then the requirement (Vdd*0.75= 825 mVolt), and re-measured the voltages with another calibrated oscilloscope as 850 mVolts and 888 mVolts. So the voltage levels are in the acceptable range. I am not using the exact crystal in the reference design, instead, I am using NX3225SA-24.000000MHZ which was for i.mx258 ref. design&lt;/P&gt;&lt;P&gt;4. If it does not stop the processor reset/boot, I don't care the slow start-up at the moment, but I also added 1 MOhms, but could not bootloader to start.&lt;/P&gt;&lt;P&gt;6. I have an UART/RS232 chip (ADM3101E) for UART_0, and set the BOOT_MODE_1=0 and BOOT_MODE_0=1 for serial bootload, and RCON21=RCON20=0 for UART_0. I am using PTB10,PTB11 pins for UART_0. I saw 0x23454523 pattern is coming to the RX pin, but nothing is in TX pin. I am not using RTS and CTS pins of UART_0, I wonder if bootloader needs them? I am using same 74LC541 chips for bootloader config pins, and checked that the config pins status are applied to the processor during 1 miliseconds reset.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40576i650A25B11E5F9D32/image-size/large?v=v2&amp;amp;px=999" title="XTAL_EXTAL.JPG.jpg" alt="XTAL_EXTAL.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mehmet Ali &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Aug 2013 12:02:06 GMT</pubDate>
    <dc:creator>MehmetAliIpin</dc:creator>
    <dc:date>2013-08-29T12:02:06Z</dc:date>
    <item>
      <title>VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277036#M1834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to have our VF3x to reset and accept the 0x23454523 command from the serial channel and transmit back to the terminal. &lt;/P&gt;&lt;P&gt;I measured: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;3.25 Volt on VBAT pin &lt;/LI&gt;&lt;LI&gt;3.3 Volt on VDD_LDOIN ( about 100 milihundred volt noise) &lt;/LI&gt;&lt;LI&gt;1.13 Volt on DCAP_V11_LDO_OUT &lt;/LI&gt;&lt;LI&gt;2.52 Volt on DCAP_V25_LDO_OUT &lt;/LI&gt;&lt;LI&gt;3.3 Volt on VDD33 &lt;/LI&gt;&lt;LI&gt;3.3 Volt on VDDREG &lt;/LI&gt;&lt;LI&gt;1.2 Volt on VDD &lt;/LI&gt;&lt;LI&gt;5.2 Volt on USB_VBUS &lt;/LI&gt;&lt;LI&gt;3.1 Volt on USB_DCAP &lt;/LI&gt;&lt;LI&gt;1.8 Volt on VBCTRL &lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;23.99 MHz on XTAL-EXTAL pins ( XTAL pin has perfect sine wave, while EXTAL pin has a periodic signal between sine wave and triangle wave) &lt;/P&gt;&lt;P&gt;There are a 2.2 MOhm parallel resistor in ref design for XTAL pins' series capacitor. Why it is used?&lt;/P&gt;&lt;P&gt;The PCB draws 86 mAmperes from 3.3 Volt supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My RCON Mappings are adjusted for serial boot loader from UART 0. But I could not get answer to 0x23454523 message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do these voltage values and osc. value proof that chip has reset?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What else I could check?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2013 10:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277036#M1834</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2013-08-27T10:28:25Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277037#M1835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Dear Mehmet,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;1.&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Are you using our Tower Reference Board or your own design?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;2.&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;At the first glance the voltages are looking alright.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;3.&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Regarding the &lt;SPAN style="color: #3d3d3d;"&gt;XTAL-EXTAL pins&lt;/SPAN&gt; - may I see the oscilloscope screenshots, please?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;4. &lt;/SPAN&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Regarding the &lt;SPAN style="color: #3d3d3d;"&gt;2.2 MOhm resistor - mentioned i the Errata (&lt;/SPAN&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/errata/VYBRID_1N02G.pdf?fsrch=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;sr=1" title="http://cache.freescale.com/files/32bit/doc/errata/VYBRID_1N02G.pdf?fsrch=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;sr=1"&gt;http://cache.freescale.com/files/32bit/doc/errata/VYBRID_1N02G.pdf?fsrch=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FO…&lt;/A&gt;):&lt;/SPAN&gt;&lt;/P&gt;&lt;UL style="list-style-type: disc;"&gt;&lt;LI&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;e7128: XTAL: In some cases the 24MHz oscillator start-up is slow.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Workaround: A 2.2 MΩ resistor from XTAL to ground will make the startup times reasonable.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;5. &lt;/SPAN&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Regarding the 86mA current – hard to judge without knowing your configuration settings details, but definitely nothing catastrophic.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;6. &lt;/SPAN&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Except for UART, what other possible “boot sources” do you have - SD, FLASH, etc.? If Vybrid is not configured properly, it boots from another “source” – have you seen activity on any of the related buses, especially the UART &lt;SPAN style="font-family: Arial, sans-serif;"&gt;one&lt;/SPAN&gt; (I guess, in your case it is USB)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: 2.4pt; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Sincerely, Naoum Gitnik.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2013 17:48:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277037#M1835</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2013-08-27T17:48:30Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277038#M1836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Naoum,&lt;/P&gt;&lt;P&gt;Thank you for your helps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. We are using our Own design&lt;/P&gt;&lt;P&gt;2. I checked the power sequence, and saw that the USB_V0 has the only 10 micro second after the 5 Volt is applied, while the 1.1V Vdd has 100 microsecond delay. There was a load switch between external 5 Volts to USB_V0, which was controlled by BCTRL signal. But it was not working, so I removed it, but I could not see any improvement.&lt;/P&gt;&lt;P&gt;3. blue line is for XTAL. I noticed that the voltage level (600 mVolt) is below then the requirement (Vdd*0.75= 825 mVolt), and re-measured the voltages with another calibrated oscilloscope as 850 mVolts and 888 mVolts. So the voltage levels are in the acceptable range. I am not using the exact crystal in the reference design, instead, I am using NX3225SA-24.000000MHZ which was for i.mx258 ref. design&lt;/P&gt;&lt;P&gt;4. If it does not stop the processor reset/boot, I don't care the slow start-up at the moment, but I also added 1 MOhms, but could not bootloader to start.&lt;/P&gt;&lt;P&gt;6. I have an UART/RS232 chip (ADM3101E) for UART_0, and set the BOOT_MODE_1=0 and BOOT_MODE_0=1 for serial bootload, and RCON21=RCON20=0 for UART_0. I am using PTB10,PTB11 pins for UART_0. I saw 0x23454523 pattern is coming to the RX pin, but nothing is in TX pin. I am not using RTS and CTS pins of UART_0, I wonder if bootloader needs them? I am using same 74LC541 chips for bootloader config pins, and checked that the config pins status are applied to the processor during 1 miliseconds reset.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40576i650A25B11E5F9D32/image-size/large?v=v2&amp;amp;px=999" title="XTAL_EXTAL.JPG.jpg" alt="XTAL_EXTAL.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mehmet Ali &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2013 12:02:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277038#M1836</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2013-08-29T12:02:06Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277039#M1837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;Dear Mehmet,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;Based on the data provided, I do not think your issue is related to the crystal oscillator.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;Nowadays, with highly configurable devices, the vast majority of debug issues are due to incorrect configuration settings. Quite often the registers do not accept values they are supposed to get, so I would recommend you to always verify their values (read back) every time you write them.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;If the device’s boot source is configured but you still do not see anything on the TX line, please, verify if your UART flow control is configured properly (see ‘&lt;/SPAN&gt;49.4.1.6 Hardware flow control’, ‘49.4.1.7 Transceiver driver enable’, and ‘49.4.2.7 Hardware flow control’). &lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;If the flow control signals, &lt;SPAN style="color: #3d3d3d;"&gt;RTS and CTS&lt;/SPAN&gt;, are involved, you will have to “cheat” Vybrid by pulling them up or down (see the UART physical layer details), either with external resistors or better with the built-in ones. &lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;Just to confirm, &lt;/SPAN&gt;the &lt;SPAN style="color: #3d3d3d;"&gt;RTS and CTS&lt;/SPAN&gt; (flow control) line do not come to the DB9 connector&lt;SPAN style="color: #3d3d3d;"&gt; on one of our boards&lt;/SPAN&gt;.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;You may also take a look at our MQX drivers to see how the UART is handled – our SW is usually commented quite well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;(BTW, the ADM3101E&lt;/SPAN&gt; is just a level-shifter in this case.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt; background: white;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;Sincerely, Naoum Gitnik.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2013 22:04:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277039#M1837</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2013-09-03T22:04:09Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277040#M1838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Naoum&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I connected the RTS pin to CTS pin, the Vybrid answered the 0x23454523 pattern.&lt;/P&gt;&lt;P&gt;Now we need serial downloader SW like ATK for i.mx. in order to download and run our SW from internal RAM. &lt;/P&gt;&lt;P&gt;Do you know is it ready, or when it will be ready?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for all your helps and best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2013 07:56:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277040#M1838</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2013-09-04T07:56:17Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277041#M1839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mehmet,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe Freescale is working on an SDP serial downloader, but it is not released yet (see &lt;A href="https://community.nxp.com/message/337588"&gt;Vybrid USB Loading Utility&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the meantime, you might find the Toradex utility useful, at &lt;A href="https://github.com/toradex/imx_loader" title="https://github.com/toradex/imx_loader"&gt;toradex/imx_loader · GitHub&lt;/A&gt;. It is licenced under the GPLv3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Richard Donkin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 May 2014 06:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277041#M1839</guid>
      <dc:creator>richarddonkin</dc:creator>
      <dc:date>2014-05-21T06:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277042#M1840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Richard ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your helps. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now we can download our image files with last version of MFGToolkit over USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 May 2014 12:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277042#M1840</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2014-05-21T12:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277043#M1841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mehmet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You mentioned above that when you 'connected the RTS pin to CTS pin, the Vybrid answered the 0x23454523 pattern'. May I ask what UART parameters you used ? I am attempting the same thing with 1 start bit and 1 stop bit for each byte in the pattern at a baud rate of 115200bps, but I dont seem to be getting a response from the Vybrid.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2015 10:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277043#M1841</guid>
      <dc:creator>danielbasilio</dc:creator>
      <dc:date>2015-04-10T10:14:45Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277044#M1842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used the same UART parameters: 1 start,1 stop bits, no parity, 115200. Send 0x23, 0x45,0x45,0x23 (Hex bytes).&lt;/P&gt;&lt;P&gt;Make sure (with Oscilloscope ) you send these 4 bytes,&lt;/P&gt;&lt;P&gt;If you send them, but not receive back them&lt;/P&gt;&lt;P&gt;Check if processor generates the LDO output voltages,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.3333330154419px;"&gt;Check if your reset pulse is correct&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Check the processor generates the clock pulses at the clock pins&lt;/P&gt;&lt;P&gt;Check if your power sequence is correct (first 3.3V, then 1.2 V).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2015 14:20:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277044#M1842</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2015-04-10T14:20:54Z</dc:date>
    </item>
    <item>
      <title>Re: VF3x reset, serial bootload</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277045#M1843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mehmet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your help and quick response. I am getting a response from the Vybrid now. I was waiting too long after startup before sending down the 0x23454523 pattern.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2015 15:18:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF3x-reset-serial-bootload/m-p/277045#M1843</guid>
      <dc:creator>danielbasilio</dc:creator>
      <dc:date>2015-04-10T15:18:27Z</dc:date>
    </item>
  </channel>
</rss>