<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VF6 and 8bit-NAND Flash memory in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/VF6-and-8bit-NAND-Flash-memory/m-p/274839#M1804</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear George,&lt;/P&gt;&lt;P&gt;Below are excerpts from the NAND FLASH operation descriptions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;"This 8-bit bus acts as a multiplexed bus to transfer data, address, and instructions."&lt;/LI&gt;&lt;LI&gt;" Bidirectional 8-bit multiplexed bus used to send data/command/address to their respective registers in the NAND flash device. The data read from the NAND flash device is also available on these lines."&lt;/LI&gt;&lt;LI&gt;"For 16-bit devices, commands and addresses use the lower 8 bits (7:0). &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;The upper 8 &lt;/SPAN&gt;bits of the 16-bit data bus are used only during data-transfer cycles."&lt;/LI&gt;&lt;LI&gt;Etc.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;So, it is the lower 8 bits; they are always used - for both 8- and 16-bit devices.&lt;/P&gt;&lt;P&gt;Sincerely, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jul 2013 22:19:18 GMT</pubDate>
    <dc:creator>naoumgitnik</dc:creator>
    <dc:date>2013-07-22T22:19:18Z</dc:date>
    <item>
      <title>VF6 and 8bit-NAND Flash memory</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF6-and-8bit-NAND-Flash-memory/m-p/274838#M1803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wish to connect &lt;STRONG&gt;VF6&lt;/STRONG&gt; series and &lt;STRONG&gt;8bit-NAND&lt;/STRONG&gt; of Vybrid.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, it is not known whether it is correct to use which 8 bits of NF_IO [15:0].&lt;/P&gt;&lt;P&gt;Is my understanding correct although it seems that NF_IO [7:0] is correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2013 14:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF6-and-8bit-NAND-Flash-memory/m-p/274838#M1803</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2013-07-16T14:12:51Z</dc:date>
    </item>
    <item>
      <title>Re: VF6 and 8bit-NAND Flash memory</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF6-and-8bit-NAND-Flash-memory/m-p/274839#M1804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear George,&lt;/P&gt;&lt;P&gt;Below are excerpts from the NAND FLASH operation descriptions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;"This 8-bit bus acts as a multiplexed bus to transfer data, address, and instructions."&lt;/LI&gt;&lt;LI&gt;" Bidirectional 8-bit multiplexed bus used to send data/command/address to their respective registers in the NAND flash device. The data read from the NAND flash device is also available on these lines."&lt;/LI&gt;&lt;LI&gt;"For 16-bit devices, commands and addresses use the lower 8 bits (7:0). &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;The upper 8 &lt;/SPAN&gt;bits of the 16-bit data bus are used only during data-transfer cycles."&lt;/LI&gt;&lt;LI&gt;Etc.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;So, it is the lower 8 bits; they are always used - for both 8- and 16-bit devices.&lt;/P&gt;&lt;P&gt;Sincerely, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jul 2013 22:19:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF6-and-8bit-NAND-Flash-memory/m-p/274839#M1804</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2013-07-22T22:19:18Z</dc:date>
    </item>
    <item>
      <title>Re: VF6 and 8bit-NAND Flash memory</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/VF6-and-8bit-NAND-Flash-memory/m-p/274840#M1805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Naoum,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Fukutomi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jul 2013 08:42:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/VF6-and-8bit-NAND-Flash-memory/m-p/274840#M1805</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2013-07-24T08:42:41Z</dc:date>
    </item>
  </channel>
</rss>