<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: Composite VADC?</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Composite-VADC/m-p/252652#M1067</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bill,&lt;/P&gt;&lt;P&gt;Just a correction - according to one of the Freescale development platforms, the VF5xx flavor does have VADC inputs (see schematic fragments attached).&lt;/P&gt;&lt;P&gt;Sincerely, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Jan 2015 18:22:38 GMT</pubDate>
    <dc:creator>naoumgitnik</dc:creator>
    <dc:date>2015-01-02T18:22:38Z</dc:date>
    <item>
      <title>Composite VADC?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Composite-VADC/m-p/252650#M1065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In Section 8.9.5 of the Vybrid Reference manual, it has some information on the VADC interface.&amp;nbsp; Register &lt;EM&gt;misc2&lt;/EM&gt; bit 9 is used to toggle the source the the VIU.&amp;nbsp; Is this feature still supported by the Vybrid?&amp;nbsp; Only particular models (Auto)?&amp;nbsp; What kind of input signals are appropriate?&amp;nbsp; Component NTSC?&amp;nbsp; Is there some sort of NDA process for this?&amp;nbsp; Oddly the diagram has four ADC inputs?&amp;nbsp; I don't know of any color standards with four inputs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2013 17:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Composite-VADC/m-p/252650#M1065</guid>
      <dc:creator>billpringlemeir</dc:creator>
      <dc:date>2013-11-01T17:14:00Z</dc:date>
    </item>
    <item>
      <title>Re: Composite VADC?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Composite-VADC/m-p/252651#M1066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Chapter 60 &lt;STRONG&gt;Video Sub-system&lt;/STRONG&gt; contains documentation on this feature.&amp;nbsp; They are just not titled with &lt;STRONG&gt;VADC&lt;/STRONG&gt; and the overview doesn't provide a reference to these chapters.&amp;nbsp; Section &lt;STRONG&gt;60.5 Video decoder &lt;/STRONG&gt;gives information on the &lt;A href="http://en.wikipedia.org/wiki/Composite_video"&gt;supported input formats&lt;/A&gt;.&amp;nbsp; Each &lt;STRONG&gt;VADC&lt;/STRONG&gt; input can be a separate&amp;nbsp; &lt;EM&gt;composite &lt;/EM&gt;image channel and the interface is not &lt;EM&gt;component&lt;/EM&gt; based.&amp;nbsp; Also, these &lt;STRONG&gt;VADC &lt;/STRONG&gt;inputs are only available on the &lt;STRONG&gt;VF6xx&lt;/STRONG&gt; parts, not in &lt;STRONG&gt;VF5xx&lt;/STRONG&gt; or &lt;STRONG&gt;VF3xx&lt;/STRONG&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2013 17:27:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Composite-VADC/m-p/252651#M1066</guid>
      <dc:creator>billpringlemeir</dc:creator>
      <dc:date>2013-11-01T17:27:35Z</dc:date>
    </item>
    <item>
      <title>Re: Composite VADC?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Composite-VADC/m-p/252652#M1067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bill,&lt;/P&gt;&lt;P&gt;Just a correction - according to one of the Freescale development platforms, the VF5xx flavor does have VADC inputs (see schematic fragments attached).&lt;/P&gt;&lt;P&gt;Sincerely, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jan 2015 18:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Composite-VADC/m-p/252652#M1067</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2015-01-02T18:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: Composite VADC?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Composite-VADC/m-p/252653#M1068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Naoum,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This would be a nice surprise.&amp;nbsp; I was told by an FAE that the VF5xx didn't have the video ADC.&amp;nbsp; There is also this &lt;A href="http://www.freescale.com/webapp/sps/components/displayCollateral.jsp?code=VYBRID_PORTFOLIO_BDIMG&amp;amp;keepThis=true&amp;amp;TB_iframe=true&amp;amp;height=490&amp;amp;width=810"&gt;Vybrid F series link&lt;/A&gt; which seems to say on the VF6xx part has the inputs.&amp;nbsp; Certainly, a PCB may have components to support both the VF5xx and VF6xx chips.&amp;nbsp; Perhaps the Vybrid R 5 part has the VADC?&amp;nbsp; It also seems to have an M4 CPU as well.&amp;nbsp; There is also &lt;A href="http://cache.freescale.com/files/32bit/doc/brochure/FREESCALEARM.pdf"&gt;this PDF on Freescale technology&lt;/A&gt; and on page 31 it shows only the VF6xx series has the VADC inputs.&amp;nbsp; Are you sure that the VF5xx has the VADC inputs?&amp;nbsp; It most likely only has the digital portion; some camera portions are present but not the Analog Camera decode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is very weird.&amp;nbsp; I was told by some Freescale support in our area that the iMx6 did not have a secure part.&amp;nbsp; However, I see various Freescale programmers putting CAAM support in Linux.&amp;nbsp; It seems that the iMx6 can have security features; but they are not as in-depth as the Vybrid Secure parts.&amp;nbsp; I had to get the manuals and read this myself.&amp;nbsp; I would be glad if the VF5xx parts have the analog inputs.&amp;nbsp; We have given up several pins for a digital camera interface in our design.&amp;nbsp; Can you double check that this is correct that the VF5xx does support the VADC inputs?&amp;nbsp; Have you actually used those inputs with a VF5xx part?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2015 15:51:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Composite-VADC/m-p/252653#M1068</guid>
      <dc:creator>billpringlemeir</dc:creator>
      <dc:date>2015-01-05T15:51:39Z</dc:date>
    </item>
  </channel>
</rss>