<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: Dual Eth on u-boot</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Dual-Eth-on-u-boot/m-p/252172#M1054</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bruno,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As of today, there are no plans to add Dual Eth on u-boot, though it could be added in the future.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Aug 2013 16:00:30 GMT</pubDate>
    <dc:creator>SergioSolis</dc:creator>
    <dc:date>2013-08-22T16:00:30Z</dc:date>
    <item>
      <title>Dual Eth on u-boot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Dual-Eth-on-u-boot/m-p/252171#M1053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our customer needs to have access to both Vybrid eth ports on u-boot due to safety boot strategy of the system (the system is on 2 different networks at the same time).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Doing tests we have noticed only one eth is supported on u-boot, but when the system boots the kernel, both work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a plan to have the 2 eth controllers functional on u-boot?&lt;/P&gt;&lt;P&gt;Does u-boot support it if configured to do it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using timesys BSP with tower card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tks!&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Aug 2013 12:15:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Dual-Eth-on-u-boot/m-p/252171#M1053</guid>
      <dc:creator>bfac</dc:creator>
      <dc:date>2013-08-13T12:15:07Z</dc:date>
    </item>
    <item>
      <title>Re: Dual Eth on u-boot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Dual-Eth-on-u-boot/m-p/252172#M1054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bruno,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As of today, there are no plans to add Dual Eth on u-boot, though it could be added in the future.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2013 16:00:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Dual-Eth-on-u-boot/m-p/252172#M1054</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2013-08-22T16:00:30Z</dc:date>
    </item>
  </channel>
</rss>