<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinic中的主题 Re: S32K144: IAR SW issue</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/S32K144-IAR-SW-issue/m-p/2269488#M595</link>
    <description>&lt;P&gt;In IAR Embedded Workbench, debugging works with a relocated interrupt vector table because the CPU supports vector table relocation (e.g., via a VTOR register on ARM Cortex-M). The debugger reads the current vector table base address from the CPU, maps the interrupt vectors to the corresponding ISR symbols, and uses the linker-generated symbol table to resolve addresses. Similar to how a &lt;A href="https://middler.com/" target="_self"&gt;USA paint estimator&lt;/A&gt; helps calculate coverage and cost accurately, the debugger aligns with the relocated vector table at startup, allowing breakpoints and step-through debugging to function normally even when the table is not at address 0.&lt;/P&gt;</description>
    <pubDate>Mon, 29 Dec 2025 06:09:25 GMT</pubDate>
    <dc:creator>yisey</dc:creator>
    <dc:date>2025-12-29T06:09:25Z</dc:date>
    <item>
      <title>S32K144: IAR SW issue</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/S32K144-IAR-SW-issue/m-p/2183450#M570</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Under IAR, debugging can still be done when the interrupt vector table is not at position 0. What are the specific principles and processes?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Oct 2025 02:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/S32K144-IAR-SW-issue/m-p/2183450#M570</guid>
      <dc:creator>Alex28</dc:creator>
      <dc:date>2025-10-10T02:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144: IAR SW issue</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/S32K144-IAR-SW-issue/m-p/2269488#M595</link>
      <description>&lt;P&gt;In IAR Embedded Workbench, debugging works with a relocated interrupt vector table because the CPU supports vector table relocation (e.g., via a VTOR register on ARM Cortex-M). The debugger reads the current vector table base address from the CPU, maps the interrupt vectors to the corresponding ISR symbols, and uses the linker-generated symbol table to resolve addresses. Similar to how a &lt;A href="https://middler.com/" target="_self"&gt;USA paint estimator&lt;/A&gt; helps calculate coverage and cost accurately, the debugger aligns with the relocated vector table at startup, allowing breakpoints and step-through debugging to function normally even when the table is not at address 0.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Dec 2025 06:09:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/S32K144-IAR-SW-issue/m-p/2269488#M595</guid>
      <dc:creator>yisey</dc:creator>
      <dc:date>2025-12-29T06:09:25Z</dc:date>
    </item>
  </channel>
</rss>