<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinic中的主题 Re: Error using Config Tool via MCUXpresso for VS Code</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Error-using-Config-Tool-via-MCUXpresso-for-VS-Code/m-p/1896819#M502</link>
    <description>&lt;P&gt;I solved this...&amp;nbsp; &amp;nbsp; The MCUXpresso for VScode "import" function put in a custom toolchain path (of simply "armgcc").&amp;nbsp; &amp;nbsp; Browsing to the project folder for project toolchain path fixed this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The import function also duplicated some of the flags (which caused errors), so these had to be manually fixed...&lt;/P&gt;</description>
    <pubDate>Mon, 01 Jul 2024 17:37:01 GMT</pubDate>
    <dc:creator>CktDesigner</dc:creator>
    <dc:date>2024-07-01T17:37:01Z</dc:date>
    <item>
      <title>Error using Config Tool via MCUXpresso for VS Code</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Error-using-Config-Tool-via-MCUXpresso-for-VS-Code/m-p/1895419#M500</link>
      <description>&lt;P&gt;I converted a project from the MCUXpresso IDE to MCUXpresso for VS code.&lt;/P&gt;&lt;P&gt;The project is for a custom board that uses the MIMXRT1062CVL5B processor.&lt;/P&gt;&lt;P&gt;The project compiles using the MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;I'm using MCUXpresso Config Tools Version 15.0&lt;/P&gt;&lt;P&gt;I'm using Visual Studio Code Version 1.90.2 with Version 1.9 of MCUXpresso for VS Code extension&lt;/P&gt;&lt;P&gt;After importing the project into VScode (and manually modifying a couple of things that didn't convert properly), it now compiles in VScode.&lt;/P&gt;&lt;P&gt;I configured the project pins and peripherals using the Config Tool in MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;When I open the Config Tool via VScode, I get errors stating that some drivers are not found in the toolchain/IDE project.&amp;nbsp; &amp;nbsp; These errors don't show up when using the IDE version.&lt;/P&gt;&lt;P&gt;Yet the drivers are there and the code compiles!&lt;/P&gt;&lt;P&gt;Right-clicking over the error simply pops up a "Problem Details" box that "The SDK component is required by the generated code from the tool.&amp;nbsp; If it is not included in the toolchain project, the source code will not be compilable."&lt;/P&gt;&lt;P&gt;I'd like to clear these errors, but am out of ideas of things to try...&amp;nbsp; &amp;nbsp;The project does compile though!&lt;/P&gt;&lt;P&gt;In a related issue, I no longer need a peripheral and removed it using the Config Tool, but the drivers still show up in the Project Explorer.&amp;nbsp; &amp;nbsp;Do these have to be removed manually, or is there a way to have the tool remove all of the appropriate files?&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 21:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/Error-using-Config-Tool-via-MCUXpresso-for-VS-Code/m-p/1895419#M500</guid>
      <dc:creator>CktDesigner</dc:creator>
      <dc:date>2024-06-27T21:19:27Z</dc:date>
    </item>
    <item>
      <title>Re: Error using Config Tool via MCUXpresso for VS Code</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Error-using-Config-Tool-via-MCUXpresso-for-VS-Code/m-p/1896819#M502</link>
      <description>&lt;P&gt;I solved this...&amp;nbsp; &amp;nbsp; The MCUXpresso for VScode "import" function put in a custom toolchain path (of simply "armgcc").&amp;nbsp; &amp;nbsp; Browsing to the project folder for project toolchain path fixed this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The import function also duplicated some of the flags (which caused errors), so these had to be manually fixed...&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 17:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/Error-using-Config-Tool-via-MCUXpresso-for-VS-Code/m-p/1896819#M502</guid>
      <dc:creator>CktDesigner</dc:creator>
      <dc:date>2024-07-01T17:37:01Z</dc:date>
    </item>
  </channel>
</rss>