<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMXRT1060 endless SPI SCK in Embedded Software and Tools Clinic</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/IMXRT1060-endless-SPI-SCK/m-p/1893836#M499</link>
    <description>&lt;P&gt;Using IMXRT1060 we send 16 bits SPI as master and everything works fine. We have a 20 ohm resistor on the SCK signal.&lt;/P&gt;&lt;P&gt;When we remove the resistor, the NXP does not stop after 16 clocks, but rather keep on until the FIFO's are full.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using the exact same code for both scenarios.&lt;/P&gt;&lt;P&gt;I am wondering how does a resistor on SCK (which is a master output pin) cause the master to keep on clocking past the transaction boundaries?&lt;/P&gt;&lt;P&gt;We never touch the CONT/CONTC bits and not using DMA or interrupts.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Following is an image of a good and bad flow:&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jun 2024 18:48:56 GMT</pubDate>
    <dc:creator>omrif</dc:creator>
    <dc:date>2024-06-25T18:48:56Z</dc:date>
    <item>
      <title>IMXRT1060 endless SPI SCK</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/IMXRT1060-endless-SPI-SCK/m-p/1893836#M499</link>
      <description>&lt;P&gt;Using IMXRT1060 we send 16 bits SPI as master and everything works fine. We have a 20 ohm resistor on the SCK signal.&lt;/P&gt;&lt;P&gt;When we remove the resistor, the NXP does not stop after 16 clocks, but rather keep on until the FIFO's are full.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using the exact same code for both scenarios.&lt;/P&gt;&lt;P&gt;I am wondering how does a resistor on SCK (which is a master output pin) cause the master to keep on clocking past the transaction boundaries?&lt;/P&gt;&lt;P&gt;We never touch the CONT/CONTC bits and not using DMA or interrupts.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Following is an image of a good and bad flow:&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 18:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/IMXRT1060-endless-SPI-SCK/m-p/1893836#M499</guid>
      <dc:creator>omrif</dc:creator>
      <dc:date>2024-06-25T18:48:56Z</dc:date>
    </item>
  </channel>
</rss>