<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinic中的主题 Image actual partition size is different from the WKS file. Why?</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Image-actual-partition-size-is-different-from-the-WKS-file-Why/m-p/1835342#M476</link>
    <description>&lt;P&gt;I have a question about the partition size of an image generated by Yocto.&lt;/P&gt;&lt;P&gt;I am bulding for MACHINE=imx8mpevk using Yocto mickledore. The target is imx-image-core.&lt;/P&gt;&lt;P&gt;According to the wks file (in my case, the NXP's recipe chooses meta-freescale/wic/imx-imx-boot-bootpart.wks.in), the VFAT boot partion is 64MiB but the generated wic file says it's 83.2MB.&lt;/P&gt;&lt;P&gt;Likewise, when I manually set IMAGE_ROOTFS_SIZE to 2GiB or 3GiB, the actual root FS partition sizes are 2.6GiB or 3.9GiB, respectively.&lt;/P&gt;&lt;P&gt;I confirmed that the env file given to wic (/tmp/sysroots/&amp;lt;MACHINE&amp;gt;/imgdata/&amp;lt;IMAGE&amp;gt;.env) contains correct numbers.&lt;/P&gt;&lt;P&gt;Why every partiton is about 30% larger??&lt;/P&gt;</description>
    <pubDate>Tue, 26 Mar 2024 09:51:18 GMT</pubDate>
    <dc:creator>takashi-t</dc:creator>
    <dc:date>2024-03-26T09:51:18Z</dc:date>
    <item>
      <title>Image actual partition size is different from the WKS file. Why?</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Image-actual-partition-size-is-different-from-the-WKS-file-Why/m-p/1835342#M476</link>
      <description>&lt;P&gt;I have a question about the partition size of an image generated by Yocto.&lt;/P&gt;&lt;P&gt;I am bulding for MACHINE=imx8mpevk using Yocto mickledore. The target is imx-image-core.&lt;/P&gt;&lt;P&gt;According to the wks file (in my case, the NXP's recipe chooses meta-freescale/wic/imx-imx-boot-bootpart.wks.in), the VFAT boot partion is 64MiB but the generated wic file says it's 83.2MB.&lt;/P&gt;&lt;P&gt;Likewise, when I manually set IMAGE_ROOTFS_SIZE to 2GiB or 3GiB, the actual root FS partition sizes are 2.6GiB or 3.9GiB, respectively.&lt;/P&gt;&lt;P&gt;I confirmed that the env file given to wic (/tmp/sysroots/&amp;lt;MACHINE&amp;gt;/imgdata/&amp;lt;IMAGE&amp;gt;.env) contains correct numbers.&lt;/P&gt;&lt;P&gt;Why every partiton is about 30% larger??&lt;/P&gt;</description>
      <pubDate>Tue, 26 Mar 2024 09:51:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/Image-actual-partition-size-is-different-from-the-WKS-file-Why/m-p/1835342#M476</guid>
      <dc:creator>takashi-t</dc:creator>
      <dc:date>2024-03-26T09:51:18Z</dc:date>
    </item>
  </channel>
</rss>