<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinic中的主题 CRC32 S32K144</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/CRC32-S32K144/m-p/1649355#M379</link>
    <description>&lt;P&gt;I have tried to implement the CRC32 found in a S32K144_Project_CRC example, but it is calculating wrong.&lt;/P&gt;&lt;P&gt;uint8_t test = 0x41;&lt;BR /&gt;uint32_t crc = 0x00000000;&lt;BR /&gt;crc = CRC_32bits_calculate(&amp;amp;test, 1);&lt;BR /&gt;Result: 0x209FAE1A&lt;BR /&gt;If I check the result online it should be 0xD3D99E8B.&lt;/P&gt;&lt;P&gt;The code in crc.c is unchanged:&lt;BR /&gt;define POLY (0x04C11DB7)&amp;nbsp;&lt;BR /&gt;uint32_t CRC_32bits_calculate(uint8_t *data, uint32_t size)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;PCC-&amp;gt;PCCn[PCC_CRC_INDEX] |= PCC_PCCn_CGC_MASK; /* enable CRC clock */&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_TCRC(1); /* enable 32-bit CRC protocol */&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_TOT(1); /* Bits in a byte are transposed, while bytes are not transposed. */&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_TOTR(2); /* Both bits in bytes and bytes are transposed. */&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_FXOR(1); /* XOR on reading. */&lt;BR /&gt;CRC-&amp;gt;GPOLY = POLY;&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_WAS_MASK; /* Set CRC_CTRL[WAS] to program the seed value. */&lt;BR /&gt;CRC-&amp;gt;DATAu.DATA = 0xFFFFFFFF; /* seed value */&lt;BR /&gt;CRC-&amp;gt;CTRL &amp;amp;= ~CRC_CTRL_WAS_MASK; /* Clear CRC_CTRL[WAS] to start writing data values. */&lt;BR /&gt;for(;size--;)&lt;BR /&gt;CRC-&amp;gt;DATAu.DATA = *data++; /* write data values */&lt;BR /&gt;return (uint32_t) CRC-&amp;gt;DATAu.DATA;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Can any explain the difference.&lt;/P&gt;</description>
    <pubDate>Fri, 12 May 2023 10:55:37 GMT</pubDate>
    <dc:creator>MadsNE</dc:creator>
    <dc:date>2023-05-12T10:55:37Z</dc:date>
    <item>
      <title>CRC32 S32K144</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/CRC32-S32K144/m-p/1649355#M379</link>
      <description>&lt;P&gt;I have tried to implement the CRC32 found in a S32K144_Project_CRC example, but it is calculating wrong.&lt;/P&gt;&lt;P&gt;uint8_t test = 0x41;&lt;BR /&gt;uint32_t crc = 0x00000000;&lt;BR /&gt;crc = CRC_32bits_calculate(&amp;amp;test, 1);&lt;BR /&gt;Result: 0x209FAE1A&lt;BR /&gt;If I check the result online it should be 0xD3D99E8B.&lt;/P&gt;&lt;P&gt;The code in crc.c is unchanged:&lt;BR /&gt;define POLY (0x04C11DB7)&amp;nbsp;&lt;BR /&gt;uint32_t CRC_32bits_calculate(uint8_t *data, uint32_t size)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;PCC-&amp;gt;PCCn[PCC_CRC_INDEX] |= PCC_PCCn_CGC_MASK; /* enable CRC clock */&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_TCRC(1); /* enable 32-bit CRC protocol */&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_TOT(1); /* Bits in a byte are transposed, while bytes are not transposed. */&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_TOTR(2); /* Both bits in bytes and bytes are transposed. */&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_FXOR(1); /* XOR on reading. */&lt;BR /&gt;CRC-&amp;gt;GPOLY = POLY;&lt;BR /&gt;CRC-&amp;gt;CTRL |= CRC_CTRL_WAS_MASK; /* Set CRC_CTRL[WAS] to program the seed value. */&lt;BR /&gt;CRC-&amp;gt;DATAu.DATA = 0xFFFFFFFF; /* seed value */&lt;BR /&gt;CRC-&amp;gt;CTRL &amp;amp;= ~CRC_CTRL_WAS_MASK; /* Clear CRC_CTRL[WAS] to start writing data values. */&lt;BR /&gt;for(;size--;)&lt;BR /&gt;CRC-&amp;gt;DATAu.DATA = *data++; /* write data values */&lt;BR /&gt;return (uint32_t) CRC-&amp;gt;DATAu.DATA;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Can any explain the difference.&lt;/P&gt;</description>
      <pubDate>Fri, 12 May 2023 10:55:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/CRC32-S32K144/m-p/1649355#M379</guid>
      <dc:creator>MadsNE</dc:creator>
      <dc:date>2023-05-12T10:55:37Z</dc:date>
    </item>
  </channel>
</rss>