<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinicのトピックi.MX6ULL Nand Flash Booting</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/i-MX6ULL-Nand-Flash-Booting/m-p/1635929#M371</link>
    <description>&lt;P&gt;I'm trying to boot IMX6ULL NAND Flash.&lt;/P&gt;&lt;P&gt;For your information, I succeeded in booting IMX6ULL NAND Flash using buildroot 2018_11_4. ( uboot 4.15 and linux 4.15 )&lt;/P&gt;&lt;P&gt;However, the current condition is u-boot-2020.04.&lt;/P&gt;&lt;P&gt;Both uboot and linux use version 5.10.&lt;/P&gt;&lt;P&gt;There was no detailed explanation of the modifications caused by NAND booting in the NXP content, so I modified it with the contents of myir company.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;幀-Boot 2020.04-gad7247c882-dirty (Apr 19 2023 - 14:45:51 +0900)&lt;/P&gt;&lt;P&gt;CPU: i.MX6ULL rev1.1 900 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (-40C to 115C) at 39C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: i.MX6ULL Sample Board&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;DRAM: 256 MiB&lt;BR /&gt;board_init ok&lt;BR /&gt;NAND: 128 MiB&lt;BR /&gt;MMC:&lt;BR /&gt;Loading Environment from NAND... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: CPU Net Initialization Failed&lt;BR /&gt;No ethernet found.&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;NAND read: device 0 offset 0x600000, size 0xa00000&lt;BR /&gt;10485760 bytes read: OK&lt;/P&gt;&lt;P&gt;NAND read: device 0 offset 0x1000000, size 0x100000&lt;BR /&gt;1048576 bytes read: OK&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x8d1f08 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 83000000, end 8300b3c2&lt;BR /&gt;Modify /soc/aips-bus@2200000/epdc@228c000:status disabled&lt;BR /&gt;ft_system_setup for mx6&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;---------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;The problematic symptom for me is that the kernel does not come up after the 'Starting kernel' message.&lt;/P&gt;&lt;P&gt;I don't use Yocto and UUU.&lt;BR /&gt;Because I didn't understand the content.&lt;/P&gt;&lt;P&gt;So I downloaded and built Buildroot, Uboot, and linux, respectively.&lt;/P&gt;&lt;P&gt;Also, I am writing on the board using mfgtool.&lt;/P&gt;&lt;P&gt;So I need a guide on fixes to configure NAND boot for the latest version or 5.10.&lt;/P&gt;&lt;P&gt;Would it be possible to get some help?&lt;/P&gt;</description>
    <pubDate>Wed, 19 Apr 2023 06:15:50 GMT</pubDate>
    <dc:creator>mjay</dc:creator>
    <dc:date>2023-04-19T06:15:50Z</dc:date>
    <item>
      <title>i.MX6ULL Nand Flash Booting</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/i-MX6ULL-Nand-Flash-Booting/m-p/1635929#M371</link>
      <description>&lt;P&gt;I'm trying to boot IMX6ULL NAND Flash.&lt;/P&gt;&lt;P&gt;For your information, I succeeded in booting IMX6ULL NAND Flash using buildroot 2018_11_4. ( uboot 4.15 and linux 4.15 )&lt;/P&gt;&lt;P&gt;However, the current condition is u-boot-2020.04.&lt;/P&gt;&lt;P&gt;Both uboot and linux use version 5.10.&lt;/P&gt;&lt;P&gt;There was no detailed explanation of the modifications caused by NAND booting in the NXP content, so I modified it with the contents of myir company.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;幀-Boot 2020.04-gad7247c882-dirty (Apr 19 2023 - 14:45:51 +0900)&lt;/P&gt;&lt;P&gt;CPU: i.MX6ULL rev1.1 900 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (-40C to 115C) at 39C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: i.MX6ULL Sample Board&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;DRAM: 256 MiB&lt;BR /&gt;board_init ok&lt;BR /&gt;NAND: 128 MiB&lt;BR /&gt;MMC:&lt;BR /&gt;Loading Environment from NAND... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: CPU Net Initialization Failed&lt;BR /&gt;No ethernet found.&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;NAND read: device 0 offset 0x600000, size 0xa00000&lt;BR /&gt;10485760 bytes read: OK&lt;/P&gt;&lt;P&gt;NAND read: device 0 offset 0x1000000, size 0x100000&lt;BR /&gt;1048576 bytes read: OK&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x8d1f08 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 83000000, end 8300b3c2&lt;BR /&gt;Modify /soc/aips-bus@2200000/epdc@228c000:status disabled&lt;BR /&gt;ft_system_setup for mx6&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;---------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;The problematic symptom for me is that the kernel does not come up after the 'Starting kernel' message.&lt;/P&gt;&lt;P&gt;I don't use Yocto and UUU.&lt;BR /&gt;Because I didn't understand the content.&lt;/P&gt;&lt;P&gt;So I downloaded and built Buildroot, Uboot, and linux, respectively.&lt;/P&gt;&lt;P&gt;Also, I am writing on the board using mfgtool.&lt;/P&gt;&lt;P&gt;So I need a guide on fixes to configure NAND boot for the latest version or 5.10.&lt;/P&gt;&lt;P&gt;Would it be possible to get some help?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 06:15:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/i-MX6ULL-Nand-Flash-Booting/m-p/1635929#M371</guid>
      <dc:creator>mjay</dc:creator>
      <dc:date>2023-04-19T06:15:50Z</dc:date>
    </item>
  </channel>
</rss>