<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SB32 RDB2 support TEE? If yes, how can I activate TEE on RDB2? in Embedded Software and Tools Clinic</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/SB32-RDB2-support-TEE-If-yes-how-can-I-activate-TEE-on-RDB2/m-p/1611227#M353</link>
    <description>&lt;P&gt;Hello, Team.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is TEE(op-tee) supported on S32 RDB2 board?&lt;/P&gt;&lt;P&gt;I can not find the guidance or example for that.&lt;/P&gt;&lt;P&gt;And I just tried to set TZ memory address for the board but it shows me error message like below&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTICE: BL2: v2.5(release):bsp33.0-2.5-dirty&lt;BR /&gt;NOTICE: BL2: Built : 14:01:09, Jun 15 2022&lt;BR /&gt;NOTICE: BL2: Booting BL31&lt;BR /&gt;E/TC:0 0 crypto_driver_init:369 Firmware not found&lt;BR /&gt;E/TC:0 0 call_initcalls:24 Initcall __text_start + 0x0005d200 failed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and op-tee client is pending when SESSION_OPEN when I used optee-examples or xtest?&lt;/P&gt;&lt;P&gt;Any Help?&lt;/P&gt;</description>
    <pubDate>Wed, 08 Mar 2023 00:56:31 GMT</pubDate>
    <dc:creator>tylor</dc:creator>
    <dc:date>2023-03-08T00:56:31Z</dc:date>
    <item>
      <title>SB32 RDB2 support TEE? If yes, how can I activate TEE on RDB2?</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/SB32-RDB2-support-TEE-If-yes-how-can-I-activate-TEE-on-RDB2/m-p/1611227#M353</link>
      <description>&lt;P&gt;Hello, Team.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is TEE(op-tee) supported on S32 RDB2 board?&lt;/P&gt;&lt;P&gt;I can not find the guidance or example for that.&lt;/P&gt;&lt;P&gt;And I just tried to set TZ memory address for the board but it shows me error message like below&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTICE: BL2: v2.5(release):bsp33.0-2.5-dirty&lt;BR /&gt;NOTICE: BL2: Built : 14:01:09, Jun 15 2022&lt;BR /&gt;NOTICE: BL2: Booting BL31&lt;BR /&gt;E/TC:0 0 crypto_driver_init:369 Firmware not found&lt;BR /&gt;E/TC:0 0 call_initcalls:24 Initcall __text_start + 0x0005d200 failed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and op-tee client is pending when SESSION_OPEN when I used optee-examples or xtest?&lt;/P&gt;&lt;P&gt;Any Help?&lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 00:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/SB32-RDB2-support-TEE-If-yes-how-can-I-activate-TEE-on-RDB2/m-p/1611227#M353</guid>
      <dc:creator>tylor</dc:creator>
      <dc:date>2023-03-08T00:56:31Z</dc:date>
    </item>
  </channel>
</rss>