<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinic中的主题 Re: T4241 processor + DDR Issue : Waiting for D_INIT timeout. Memory may not work.</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1604984#M349</link>
    <description>&lt;P&gt;I am not an expert but the error message "T4241 processor + DDR Issue: Waiting for D_INIT timeout" typically indicates a problem with the DDR memory initialization process. Here are some steps that you can try to resolve this issue:&lt;/P&gt;&lt;P&gt;Check the DDR memory configuration: Make sure that the DDR memory is properly configured in the hardware design and in the software. Ensure that the memory type, speed, and timings are all correctly set.&lt;/P&gt;&lt;P&gt;Check the DDR memory connections: Ensure that the DDR memory is connected properly to the processor. Check the connections and ensure that there are no shorts or opens.&lt;/P&gt;&lt;P&gt;Check the DDR memory power supply: Verify that the DDR memory power supply is within the acceptable voltage range. Ensure that the power supply is stable and free of noise.&lt;/P&gt;&lt;P&gt;Check the DDR memory initialization sequence: Verify that the DDR memory initialization sequence is correctly implemented in the software. Ensure that the DDR memory controller is properly initialized and that the DDR memory is correctly configured.&lt;/P&gt;&lt;P&gt;Try resetting the system: If the above steps do not resolve the issue, try resetting the system. Power off the system and then power it back on.&lt;/P&gt;&lt;P&gt;Consult the manufacturer's documentation: If none of the above steps resolve the issue, consult the manufacturer's documentation or contact their support team for further assistance. They may be able to provide additional guidance on how to resolve the issue.&lt;/P&gt;&lt;P&gt;I hope this would help you up to some extent.&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;A href="https://usps-track.us" target="_self"&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;USPS tracking&lt;/FONT&gt;&lt;/A&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 24 Feb 2023 05:16:00 GMT</pubDate>
    <dc:creator>dav72</dc:creator>
    <dc:date>2023-02-24T05:16:00Z</dc:date>
    <item>
      <title>T4241 processor + DDR Issue : Waiting for D_INIT timeout. Memory may not work.</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1291393#M191</link>
      <description>&lt;P&gt;Dear Experts,&lt;/P&gt;&lt;P&gt;We have a custom-designed board with T4241 processor with DDR memory.&lt;/P&gt;&lt;P&gt;By following similar forum threads reduced the DDR clock frequency using&amp;nbsp;RCW[MEM_PLL_RAT] option,&amp;nbsp;from 8:1 to 5:1. Still the observation is same.&lt;/P&gt;&lt;P&gt;U-Boot log as follows,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot 2016.012.0+ga9b437f (Jun 11 2021 - 10:37:47 +0530)&lt;/P&gt;&lt;P&gt;CPU0: T4241, Version: 2.0, (0x82400020)&lt;BR /&gt;Core: e6500, Version: 2.0, (0x80400120)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU0:1800 MHz, CPU1:1800 MHz, CPU2:1800 MHz, CPU3:1800 MHz,&lt;BR /&gt;CPU4:1800 MHz, CPU5:1800 MHz, CPU6:1800 MHz, CPU7:1800 MHz,&lt;BR /&gt;CPU8:1800 MHz, CPU9:1800 MHz, CPU10:1800 MHz, CPU11:1800 MHz,&lt;BR /&gt;CCB:600 MHz,&lt;BR /&gt;DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:150 MHz&lt;BR /&gt;FMAN1: 700 MHz&lt;BR /&gt;FMAN2: 600 MHz&lt;BR /&gt;QMAN: 300 MHz&lt;BR /&gt;PME: 466.667 MHz&lt;BR /&gt;L1: D-cache 32 KiB enabled&lt;BR /&gt;I-cache 32 KiB enabled&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0c080012 0e12120e 00000000 08000000&lt;BR /&gt;00000010: 04360848 30547a00 ec03f000 f9000000&lt;BR /&gt;00000020: 00080000 00000000 00000000 0003e000&lt;BR /&gt;00000030: 00000000 50000000 00000000 00000038&lt;BR /&gt;I2C: ready&lt;BR /&gt;Board: T4241, SERDES Reference Clocks:&lt;BR /&gt;SERDES1=125MHz SERDES2=125MHz&lt;BR /&gt;SERDES3=100MHz SERDES4=100MHz&lt;BR /&gt;SPI: ready&lt;BR /&gt;DRAM: Initializing DDR&lt;/P&gt;&lt;P&gt;DDR Size: 100000000&lt;/P&gt;&lt;P&gt;Waiting for D_INIT timeout. Memory may not work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 12:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1291393#M191</guid>
      <dc:creator>kumar_086</dc:creator>
      <dc:date>2021-06-11T12:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: T4241 processor + DDR Issue : Waiting for D_INIT timeout. Memory may not work.</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1593818#M343</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Have you been resolve this problem. I had the trouble the same as you with coustom board use b4860&lt;/P&gt;&lt;P&gt;Thanks and brgs&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 08:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1593818#M343</guid>
      <dc:creator>sonminh</dc:creator>
      <dc:date>2023-02-06T08:58:54Z</dc:date>
    </item>
    <item>
      <title>Re: T4241 processor + DDR Issue : Waiting for D_INIT timeout. Memory may not work.</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1604984#M349</link>
      <description>&lt;P&gt;I am not an expert but the error message "T4241 processor + DDR Issue: Waiting for D_INIT timeout" typically indicates a problem with the DDR memory initialization process. Here are some steps that you can try to resolve this issue:&lt;/P&gt;&lt;P&gt;Check the DDR memory configuration: Make sure that the DDR memory is properly configured in the hardware design and in the software. Ensure that the memory type, speed, and timings are all correctly set.&lt;/P&gt;&lt;P&gt;Check the DDR memory connections: Ensure that the DDR memory is connected properly to the processor. Check the connections and ensure that there are no shorts or opens.&lt;/P&gt;&lt;P&gt;Check the DDR memory power supply: Verify that the DDR memory power supply is within the acceptable voltage range. Ensure that the power supply is stable and free of noise.&lt;/P&gt;&lt;P&gt;Check the DDR memory initialization sequence: Verify that the DDR memory initialization sequence is correctly implemented in the software. Ensure that the DDR memory controller is properly initialized and that the DDR memory is correctly configured.&lt;/P&gt;&lt;P&gt;Try resetting the system: If the above steps do not resolve the issue, try resetting the system. Power off the system and then power it back on.&lt;/P&gt;&lt;P&gt;Consult the manufacturer's documentation: If none of the above steps resolve the issue, consult the manufacturer's documentation or contact their support team for further assistance. They may be able to provide additional guidance on how to resolve the issue.&lt;/P&gt;&lt;P&gt;I hope this would help you up to some extent.&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;A href="https://usps-track.us" target="_self"&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;USPS tracking&lt;/FONT&gt;&lt;/A&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Feb 2023 05:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/T4241-processor-DDR-Issue-Waiting-for-D-INIT-timeout-Memory-may/m-p/1604984#M349</guid>
      <dc:creator>dav72</dc:creator>
      <dc:date>2023-02-24T05:16:00Z</dc:date>
    </item>
  </channel>
</rss>