<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinic中的主题 NXP QorIQ T4240 PCIE 64 bit descriptor not working</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/NXP-QorIQ-T4240-PCIE-64-bit-descriptor-not-working/m-p/1472607#M276</link>
    <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I'm trying to use PCIe 64 bit descriptors and transfer data to processor DDR.&lt;/P&gt;&lt;P&gt;Here is the device tree I'm using&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;	pci0: pcie@ffe240000 {
		reg = &amp;lt;0xf 0xfe240000 0 0x10000&amp;gt;;
		num-lanes = &amp;lt;8&amp;gt;;
		ranges = &amp;lt;0x03000000 0 0xa0000000 0xc 0x00000000 0x0 0x20000000
			  0x01000000 0 0x00000000 0xf 0xf8000000 0x0 0x00010000&amp;gt;;
		pcie@0 {
			ranges = &amp;lt;0x03000000 0 0xa0000000
				  0x02000000 0 0xa0000000
				  0 0x20000000

				  0x01000000 0 0x00000000
				  0x01000000 0 0x00000000
				  0 0x00010000&amp;gt;;
		};
	};&lt;/LI-CODE&gt;&lt;P&gt;I am able to see the data in DDR offset when i use 32 bit ddr offset (Ex:0xDEC0_0000) in descriptors and when I change the address of DDR offset to 64 bit&amp;nbsp;(Ex:0x1_0000_0000). PCIe bandwidth is showing that it is writing the data but i cant able to see data in the DDR. How to i use 64 bit descriptor address?&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Balaji.G&lt;/P&gt;</description>
    <pubDate>Mon, 13 Jun 2022 04:46:10 GMT</pubDate>
    <dc:creator>immbalu</dc:creator>
    <dc:date>2022-06-13T04:46:10Z</dc:date>
    <item>
      <title>NXP QorIQ T4240 PCIE 64 bit descriptor not working</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/NXP-QorIQ-T4240-PCIE-64-bit-descriptor-not-working/m-p/1472607#M276</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I'm trying to use PCIe 64 bit descriptors and transfer data to processor DDR.&lt;/P&gt;&lt;P&gt;Here is the device tree I'm using&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;	pci0: pcie@ffe240000 {
		reg = &amp;lt;0xf 0xfe240000 0 0x10000&amp;gt;;
		num-lanes = &amp;lt;8&amp;gt;;
		ranges = &amp;lt;0x03000000 0 0xa0000000 0xc 0x00000000 0x0 0x20000000
			  0x01000000 0 0x00000000 0xf 0xf8000000 0x0 0x00010000&amp;gt;;
		pcie@0 {
			ranges = &amp;lt;0x03000000 0 0xa0000000
				  0x02000000 0 0xa0000000
				  0 0x20000000

				  0x01000000 0 0x00000000
				  0x01000000 0 0x00000000
				  0 0x00010000&amp;gt;;
		};
	};&lt;/LI-CODE&gt;&lt;P&gt;I am able to see the data in DDR offset when i use 32 bit ddr offset (Ex:0xDEC0_0000) in descriptors and when I change the address of DDR offset to 64 bit&amp;nbsp;(Ex:0x1_0000_0000). PCIe bandwidth is showing that it is writing the data but i cant able to see data in the DDR. How to i use 64 bit descriptor address?&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Balaji.G&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jun 2022 04:46:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/NXP-QorIQ-T4240-PCIE-64-bit-descriptor-not-working/m-p/1472607#M276</guid>
      <dc:creator>immbalu</dc:creator>
      <dc:date>2022-06-13T04:46:10Z</dc:date>
    </item>
  </channel>
</rss>