<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools ClinicのトピックNXP88W8887 bluetooth SDIO interface in Android 10</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/NXP88W8887-bluetooth-SDIO-interface-in-Android-10/m-p/1459838#M261</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Using the WYSAGVDXG Wifi-BT combo module with the chipset of NXP88W8887 in the Imx8qxp board.&lt;/P&gt;&lt;P&gt;We are testing the Bluetooth interface&amp;nbsp;through the SDIO interface provided by the NXP. (SD-BT-CHAR-8887-U16-MMC-15.26.19.p38-C4X14113_A2-GPL-src.zip) and using the fwimage (SD-WLAN-SD-BT-8887-U16-MMC-W15.68.19.p38-15.26.19.p38-C4X15659_A2-MGPL.zip)&lt;BR /&gt;&lt;BR /&gt;Follow the procedure based on the attached document of Android integration for NXP based modules (EMMY-W1, LILY-W1 and JODY-W2)&lt;BR /&gt;Below logs are attached.&lt;BR /&gt;&lt;BR /&gt;BT: Loading driver&lt;BR /&gt;BT Request firmware: nxp/sd8887_bt_a2.bin&lt;BR /&gt;random: crng init done&lt;BR /&gt;BT: FW download over, size 202940 bytes&lt;BR /&gt;Fail to poll firmware status: firmwarestat=0x2&lt;BR /&gt;SDIO Func0 (0x0-0x9): 43 03 04 04 05 00 00 02 03 00&lt;BR /&gt;mx8-img-md: Can't find i2c client device for ov5640_mipi@3c&lt;BR /&gt;SDIO Func2 (0x0-0x9): 00 00 00 00 3f 00 00 00 00 00&lt;BR /&gt;SDIO Func2: (0x58)00 (0x59)00 (0x5c)0d (0x60)01 (0x64)00 (0x70)00 (0x71)5c (0x72)05 (0x73)c0 (0xd8)10 (0xd9)00 (0xda)00&lt;BR /&gt;mx8-img-md: Unregistered all entities&lt;BR /&gt;Init Status Reg (0xa0-0xa5): 00 00 00 00 00 00&lt;BR /&gt;BT: FW failed to be active in time!&lt;BR /&gt;FW failed to be download!&lt;BR /&gt;BT Firmware Init Failed&lt;BR /&gt;mx8-img-md: Registered mxc_isi.0.capture as /dev/video3&lt;BR /&gt;mx8-img-md: Registered mxc_isi.4.capture as /dev/video4&lt;BR /&gt;sdio_bt: probe of mmc0:0001:2 failed with error -1&lt;BR /&gt;mx8-img-md: Can't find i2c client device for ov5640_mipi@3c&lt;BR /&gt;mx8-img-md: Unregistered all entities&lt;BR /&gt;BT: Driver loaded successfully&lt;BR /&gt;&lt;BR /&gt;/dev/mbtchar0 was not created&lt;BR /&gt;&lt;BR /&gt;Please give me the support of the module driver code or please provide the working driver of NXP88W8887 driver inegration in the Android 10.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;SanthanaKumarS&lt;/P&gt;</description>
    <pubDate>Wed, 18 May 2022 08:09:41 GMT</pubDate>
    <dc:creator>santhana_kumar</dc:creator>
    <dc:date>2022-05-18T08:09:41Z</dc:date>
    <item>
      <title>NXP88W8887 bluetooth SDIO interface in Android 10</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/NXP88W8887-bluetooth-SDIO-interface-in-Android-10/m-p/1459838#M261</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Using the WYSAGVDXG Wifi-BT combo module with the chipset of NXP88W8887 in the Imx8qxp board.&lt;/P&gt;&lt;P&gt;We are testing the Bluetooth interface&amp;nbsp;through the SDIO interface provided by the NXP. (SD-BT-CHAR-8887-U16-MMC-15.26.19.p38-C4X14113_A2-GPL-src.zip) and using the fwimage (SD-WLAN-SD-BT-8887-U16-MMC-W15.68.19.p38-15.26.19.p38-C4X15659_A2-MGPL.zip)&lt;BR /&gt;&lt;BR /&gt;Follow the procedure based on the attached document of Android integration for NXP based modules (EMMY-W1, LILY-W1 and JODY-W2)&lt;BR /&gt;Below logs are attached.&lt;BR /&gt;&lt;BR /&gt;BT: Loading driver&lt;BR /&gt;BT Request firmware: nxp/sd8887_bt_a2.bin&lt;BR /&gt;random: crng init done&lt;BR /&gt;BT: FW download over, size 202940 bytes&lt;BR /&gt;Fail to poll firmware status: firmwarestat=0x2&lt;BR /&gt;SDIO Func0 (0x0-0x9): 43 03 04 04 05 00 00 02 03 00&lt;BR /&gt;mx8-img-md: Can't find i2c client device for ov5640_mipi@3c&lt;BR /&gt;SDIO Func2 (0x0-0x9): 00 00 00 00 3f 00 00 00 00 00&lt;BR /&gt;SDIO Func2: (0x58)00 (0x59)00 (0x5c)0d (0x60)01 (0x64)00 (0x70)00 (0x71)5c (0x72)05 (0x73)c0 (0xd8)10 (0xd9)00 (0xda)00&lt;BR /&gt;mx8-img-md: Unregistered all entities&lt;BR /&gt;Init Status Reg (0xa0-0xa5): 00 00 00 00 00 00&lt;BR /&gt;BT: FW failed to be active in time!&lt;BR /&gt;FW failed to be download!&lt;BR /&gt;BT Firmware Init Failed&lt;BR /&gt;mx8-img-md: Registered mxc_isi.0.capture as /dev/video3&lt;BR /&gt;mx8-img-md: Registered mxc_isi.4.capture as /dev/video4&lt;BR /&gt;sdio_bt: probe of mmc0:0001:2 failed with error -1&lt;BR /&gt;mx8-img-md: Can't find i2c client device for ov5640_mipi@3c&lt;BR /&gt;mx8-img-md: Unregistered all entities&lt;BR /&gt;BT: Driver loaded successfully&lt;BR /&gt;&lt;BR /&gt;/dev/mbtchar0 was not created&lt;BR /&gt;&lt;BR /&gt;Please give me the support of the module driver code or please provide the working driver of NXP88W8887 driver inegration in the Android 10.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;SanthanaKumarS&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 08:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/NXP88W8887-bluetooth-SDIO-interface-in-Android-10/m-p/1459838#M261</guid>
      <dc:creator>santhana_kumar</dc:creator>
      <dc:date>2022-05-18T08:09:41Z</dc:date>
    </item>
  </channel>
</rss>