<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinic中的主题 Re: AOSP 9 ADB over USB not showing up</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/AOSP-9-ADB-over-USB-not-showing-up/m-p/1431321#M254</link>
    <description>&lt;P&gt;It turned out that the serial number ro.serialno was not passed in as kernel command line argument. Once that was fixed in BoardConfig.mk, ADB over USB worked and the device showed up on both Linux and Windows hosts.&lt;/P&gt;</description>
    <pubDate>Mon, 21 Mar 2022 13:23:32 GMT</pubDate>
    <dc:creator>nxpsri</dc:creator>
    <dc:date>2022-03-21T13:23:32Z</dc:date>
    <item>
      <title>AOSP 9 ADB over USB not showing up</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/AOSP-9-ADB-over-USB-not-showing-up/m-p/1329008#M200</link>
      <description>&lt;P&gt;When I enable adb on my AOSP 9 imx6 device, on my Linux development host this happens:&lt;/P&gt;&lt;P&gt;'lsusb' output on my Linux laptop connected to the device via OTG-microUSB port:&lt;/P&gt;&lt;P&gt;BEFORE enabling ADB on device&lt;/P&gt;&lt;P&gt;(base) popossri@pop-os:~/ArcX/mercury_files/manifest/jenkins/Android$ lsusb&lt;BR /&gt;Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub&lt;BR /&gt;Bus 001 Device 003: ID 04f2:b685 Chicony Electronics Co., Ltd Chicony USB2.0 Camera&lt;BR /&gt;&lt;STRONG&gt;Bus 001 Device 021: ID 18d1:4ee1 Google Inc. Nexus/Pixel Device (MTP)&lt;/STRONG&gt;&lt;BR /&gt;Bus 001 Device 004: ID 8087:0aaa Intel Corp. Bluetooth 9460/9560 Jefferson Peak (JfP)&lt;BR /&gt;Bus 001 Device 010: ID 0403:6001 Future Technology Devices International, Ltd FT232 Serial (UART) IC&lt;BR /&gt;Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub&lt;/P&gt;&lt;P&gt;AFTER enabling ADB on device&lt;BR /&gt;(base) popossri@pop-os:~/ArcX/mercury_files/manifest/jenkins/Android$ lsusb&lt;BR /&gt;Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub&lt;BR /&gt;Bus 001 Device 003: ID 04f2:b685 Chicony Electronics Co., Ltd Chicony USB2.0 Camera&lt;BR /&gt;Bus 001 Device 004: ID 8087:0aaa Intel Corp. Bluetooth 9460/9560 Jefferson Peak (JfP)&lt;BR /&gt;Bus 001 Device 010: ID 0403:6001 Future Technology Devices International, Ltd FT232 Serial (UART) IC&lt;BR /&gt;Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub&lt;/P&gt;&lt;P&gt;On my Samsung phone, I have to enable USB debugging using special instructions before it can be used by ADB. I tried doing that by changing device.mk so that my /system/build.prop has the following entries:&lt;/P&gt;&lt;P&gt;persist.service.adb.enable=1&lt;BR /&gt;persist.service.debuggable=1&lt;BR /&gt;persist.sys.usb.config=mtp,adb&lt;/P&gt;&lt;P&gt;But the device doesn't show up in 'adb devices' .&lt;/P&gt;&lt;P&gt;TCP(ethernet) based adb connection works just fine.What else should I check and enable?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 02:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/AOSP-9-ADB-over-USB-not-showing-up/m-p/1329008#M200</guid>
      <dc:creator>nxpsri</dc:creator>
      <dc:date>2021-08-25T02:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: AOSP 9 ADB over USB not showing up</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/AOSP-9-ADB-over-USB-not-showing-up/m-p/1414549#M243</link>
      <description>&lt;DIV class=""&gt;&lt;P&gt;Based on what I read on other stackoverflow posts , I have enabled these properties:&lt;/P&gt;&lt;PRE&gt;:/ # getprop &lt;SPAN class=""&gt;**persist.sys.usb.config                                    
ptp,adb**&lt;/SPAN&gt;

:/ # getprop | grep usb                                                
[&lt;SPAN class=""&gt;init.svc.usb-hal-1-1&lt;/SPAN&gt;]: &lt;SPAN class=""&gt;[running]&lt;/SPAN&gt;

[&lt;SPAN class=""&gt;init.svc.usbd&lt;/SPAN&gt;]: &lt;SPAN class=""&gt;[stopped]&lt;/SPAN&gt;

[&lt;SPAN class=""&gt;persist.sys.usb.config&lt;/SPAN&gt;]: &lt;SPAN class=""&gt;[ptp,adb]&lt;/SPAN&gt;

[&lt;SPAN class=""&gt;ro.boottime.usb-hal-1-1&lt;/SPAN&gt;]: &lt;SPAN class=""&gt;[11083523334]&lt;/SPAN&gt;

[&lt;SPAN class=""&gt;ro.boottime.usbd&lt;/SPAN&gt;]: &lt;SPAN class=""&gt;[11451505001]&lt;/SPAN&gt;


&lt;SPAN class=""&gt;**[sys.usb.config]: [ptp,adb]**&lt;/SPAN&gt;

[&lt;SPAN class=""&gt;sys.usb.configfs&lt;/SPAN&gt;]: &lt;SPAN class=""&gt;[2]&lt;/SPAN&gt;

[&lt;SPAN class=""&gt;sys.usb.controller&lt;/SPAN&gt;]: &lt;SPAN class=""&gt;[ci_hdrc.0]&lt;/SPAN&gt;


[&lt;SPAN class=""&gt;sys.usb.ffs.ready&lt;/SPAN&gt;]: &lt;SPAN class=""&gt;[0]&lt;/SPAN&gt;

[&lt;SPAN class=""&gt;sys.usb.mtp.device_type&lt;/SPAN&gt;]: &lt;SPAN class=""&gt;[3]&lt;/SPAN&gt;
&lt;SPAN class=""&gt;**[service.adb.tcp.port]:   [-1]**&lt;/SPAN&gt;
&lt;SPAN class=""&gt;                               
[vendor.usb.config]: [ci_hdrc.0]&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;Also, I have enabled 'USB debugging' in developer settings. But despite setting [sys.oem_unlock_allowed]: [1], I could not enable OEM unlocking'. Perhaps its because we're using a custom bootloader, not U-boot?&lt;/P&gt;&lt;P&gt;Finally, adb devices -l on a Ubuntu host connected to the device does not list the AOSP9 device and ADB over USB hasn't worked so far.&lt;/P&gt;&lt;P&gt;What can I try next to resolve this?&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 16 Feb 2022 15:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/AOSP-9-ADB-over-USB-not-showing-up/m-p/1414549#M243</guid>
      <dc:creator>nxpsri</dc:creator>
      <dc:date>2022-02-16T15:26:22Z</dc:date>
    </item>
    <item>
      <title>Re: AOSP 9 ADB over USB not showing up</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/AOSP-9-ADB-over-USB-not-showing-up/m-p/1431321#M254</link>
      <description>&lt;P&gt;It turned out that the serial number ro.serialno was not passed in as kernel command line argument. Once that was fixed in BoardConfig.mk, ADB over USB worked and the device showed up on both Linux and Windows hosts.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 13:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/AOSP-9-ADB-over-USB-not-showing-up/m-p/1431321#M254</guid>
      <dc:creator>nxpsri</dc:creator>
      <dc:date>2022-03-21T13:23:32Z</dc:date>
    </item>
  </channel>
</rss>