<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools ClinicのトピックDiscrepancy in IMXRT1010 RM and software</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Discrepancy-in-IMXRT1010-RM-and-software/m-p/1411030#M240</link>
    <description>&lt;P&gt;According to the&amp;nbsp;i.MX RT1010 Processor Reference Manual Rev 0 Page 176, the Serial NOR configuration block has 52 bytes of reserved data at offset 0x1CC. However, the evkmimxrt1010_flexspi_not_config.h file has the following&lt;/P&gt;&lt;PRE&gt;uint32_t pageSize; //!&amp;lt; Page size of Serial NOR&lt;BR /&gt;uint32_t sectorSize; //!&amp;lt; Sector size of Serial NOR&lt;BR /&gt;uint8_t ipcmdSerialClkFreq; //!&amp;lt; Clock frequency for IP command&lt;BR /&gt;uint8_t isUniformBlockSize; //!&amp;lt; Sector/Block size is the same&lt;BR /&gt;uint8_t reserved0[2]; //!&amp;lt; Reserved for future use&lt;BR /&gt;uint8_t serialNorType; //!&amp;lt; Serial NOR Flash type: 0/1/2/3&lt;BR /&gt;uint8_t needExitNoCmdMode; //!&amp;lt; Need to exit NoCmd mode before other IP command&lt;BR /&gt;uint8_t halfClkForNonReadCmd; //!&amp;lt; Half the Serial Clock for non-read command: true/false&lt;BR /&gt;uint8_t needRestoreNoCmdMode; //!&amp;lt; Need to Restore NoCmd mode after IP commmand execution&lt;BR /&gt;uint32_t blockSize; //!&amp;lt; Block size&lt;BR /&gt;uint32_t reserve2[11]; //!&amp;lt; Reserved for future use&lt;/PRE&gt;&lt;P&gt;ipcmdSerialClkFreq should be the last member in this struct, as per the Reference Manual (The manual also lists it as 4 bytes)&lt;/P&gt;&lt;P&gt;Where does this additional information come from? Is there a more up to date Reference Manual?&lt;/P&gt;</description>
    <pubDate>Wed, 09 Feb 2022 13:41:17 GMT</pubDate>
    <dc:creator>ShadowPig</dc:creator>
    <dc:date>2022-02-09T13:41:17Z</dc:date>
    <item>
      <title>Discrepancy in IMXRT1010 RM and software</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Discrepancy-in-IMXRT1010-RM-and-software/m-p/1411030#M240</link>
      <description>&lt;P&gt;According to the&amp;nbsp;i.MX RT1010 Processor Reference Manual Rev 0 Page 176, the Serial NOR configuration block has 52 bytes of reserved data at offset 0x1CC. However, the evkmimxrt1010_flexspi_not_config.h file has the following&lt;/P&gt;&lt;PRE&gt;uint32_t pageSize; //!&amp;lt; Page size of Serial NOR&lt;BR /&gt;uint32_t sectorSize; //!&amp;lt; Sector size of Serial NOR&lt;BR /&gt;uint8_t ipcmdSerialClkFreq; //!&amp;lt; Clock frequency for IP command&lt;BR /&gt;uint8_t isUniformBlockSize; //!&amp;lt; Sector/Block size is the same&lt;BR /&gt;uint8_t reserved0[2]; //!&amp;lt; Reserved for future use&lt;BR /&gt;uint8_t serialNorType; //!&amp;lt; Serial NOR Flash type: 0/1/2/3&lt;BR /&gt;uint8_t needExitNoCmdMode; //!&amp;lt; Need to exit NoCmd mode before other IP command&lt;BR /&gt;uint8_t halfClkForNonReadCmd; //!&amp;lt; Half the Serial Clock for non-read command: true/false&lt;BR /&gt;uint8_t needRestoreNoCmdMode; //!&amp;lt; Need to Restore NoCmd mode after IP commmand execution&lt;BR /&gt;uint32_t blockSize; //!&amp;lt; Block size&lt;BR /&gt;uint32_t reserve2[11]; //!&amp;lt; Reserved for future use&lt;/PRE&gt;&lt;P&gt;ipcmdSerialClkFreq should be the last member in this struct, as per the Reference Manual (The manual also lists it as 4 bytes)&lt;/P&gt;&lt;P&gt;Where does this additional information come from? Is there a more up to date Reference Manual?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Feb 2022 13:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/Discrepancy-in-IMXRT1010-RM-and-software/m-p/1411030#M240</guid>
      <dc:creator>ShadowPig</dc:creator>
      <dc:date>2022-02-09T13:41:17Z</dc:date>
    </item>
  </channel>
</rss>