<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic eIQ ToolKit Remote Devices in Embedded Software and Tools Clinic</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/eIQ-ToolKit-Remote-Devices/m-p/1356971#M223</link>
    <description>&lt;P&gt;I want to validate a deep learning model on imx8mp.&lt;BR /&gt;I'm using the eIQ ToolKit.&lt;/P&gt;&lt;P&gt;I cannot add imx8mp from the Remote Devices tab.&lt;BR /&gt;"Validation Error: Could not find devices." Is displayed.&lt;/P&gt;&lt;P&gt;I want to solve this problem, but I don't know where to suspect the problem.&lt;/P&gt;&lt;P&gt;By the way, the device is connected to the PC with a LAN cable.&lt;BR /&gt;It is possible to connect to device with ssh from the command line of the PC.&lt;/P&gt;</description>
    <pubDate>Mon, 18 Oct 2021 06:47:29 GMT</pubDate>
    <dc:creator>HT_MOB</dc:creator>
    <dc:date>2021-10-18T06:47:29Z</dc:date>
    <item>
      <title>eIQ ToolKit Remote Devices</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/eIQ-ToolKit-Remote-Devices/m-p/1356971#M223</link>
      <description>&lt;P&gt;I want to validate a deep learning model on imx8mp.&lt;BR /&gt;I'm using the eIQ ToolKit.&lt;/P&gt;&lt;P&gt;I cannot add imx8mp from the Remote Devices tab.&lt;BR /&gt;"Validation Error: Could not find devices." Is displayed.&lt;/P&gt;&lt;P&gt;I want to solve this problem, but I don't know where to suspect the problem.&lt;/P&gt;&lt;P&gt;By the way, the device is connected to the PC with a LAN cable.&lt;BR /&gt;It is possible to connect to device with ssh from the command line of the PC.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Oct 2021 06:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/eIQ-ToolKit-Remote-Devices/m-p/1356971#M223</guid>
      <dc:creator>HT_MOB</dc:creator>
      <dc:date>2021-10-18T06:47:29Z</dc:date>
    </item>
    <item>
      <title>Re: eIQ ToolKit Remote Devices</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/eIQ-ToolKit-Remote-Devices/m-p/1575805#M328</link>
      <description>&lt;P&gt;Were you able to resolve that issue? I am also facing the same issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Dec 2022 09:14:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/eIQ-ToolKit-Remote-Devices/m-p/1575805#M328</guid>
      <dc:creator>_asif_muhammed_</dc:creator>
      <dc:date>2022-12-30T09:14:23Z</dc:date>
    </item>
  </channel>
</rss>