<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinicのトピックble pheripheral doesn't stop advertising after connection from central</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/ble-pheripheral-doesn-t-stop-advertising-after-connection-from/m-p/1345639#M207</link>
    <description>&lt;P&gt;Hello, Experts,&lt;/P&gt;&lt;P&gt;I am working on kw36 chip. What I want to do is to implement a pheripheral device which support multi connections. But in the current example project temperature sensor, the advertising will stop automatically when one connection is established. So, is there a way to disable this behavior, or I must call Gap_StartAdvertising in the gConnEvtConnected_c event.&lt;/P&gt;</description>
    <pubDate>Fri, 24 Sep 2021 07:14:12 GMT</pubDate>
    <dc:creator>xfning</dc:creator>
    <dc:date>2021-09-24T07:14:12Z</dc:date>
    <item>
      <title>ble pheripheral doesn't stop advertising after connection from central</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/ble-pheripheral-doesn-t-stop-advertising-after-connection-from/m-p/1345639#M207</link>
      <description>&lt;P&gt;Hello, Experts,&lt;/P&gt;&lt;P&gt;I am working on kw36 chip. What I want to do is to implement a pheripheral device which support multi connections. But in the current example project temperature sensor, the advertising will stop automatically when one connection is established. So, is there a way to disable this behavior, or I must call Gap_StartAdvertising in the gConnEvtConnected_c event.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 07:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/ble-pheripheral-doesn-t-stop-advertising-after-connection-from/m-p/1345639#M207</guid>
      <dc:creator>xfning</dc:creator>
      <dc:date>2021-09-24T07:14:12Z</dc:date>
    </item>
    <item>
      <title>Re: ble pheripheral doesn't stop advertising after connection from central</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/ble-pheripheral-doesn-t-stop-advertising-after-connection-from/m-p/2276196#M600</link>
      <description>&lt;P&gt;On the KW36, advertising stops by default when a connection is established. Similar to how an &lt;A href="https://instaupapkdl.com/" target="_self"&gt;Instagram auto-like app&lt;/A&gt; needs continuous background activity, to support multiple connections you either need to enable multi-connection support in the BLE stack or call Gap_StartAdvertising() in the gConnEvtConnected_c event to resume advertising.&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jan 2026 12:47:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/ble-pheripheral-doesn-t-stop-advertising-after-connection-from/m-p/2276196#M600</guid>
      <dc:creator>yisey</dc:creator>
      <dc:date>2026-01-05T12:47:59Z</dc:date>
    </item>
  </channel>
</rss>