<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can these tools be configured to run on Linux? in Embedded Software and Tools Clinic</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Can-these-tools-be-configured-to-run-on-Linux/m-p/912444#M2</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James,&lt;/P&gt;&lt;P&gt;The lab can definitely be run in Windows and Non-Windows platforms. Just keep in mind that in order to run the labs, you need to extract the "eIQ Update.exe" file from&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-344227"&gt;eIQ ML Software Clinic - Lab and Software Files&lt;/A&gt;, which is a Windows executable. This is because that is an installer that requires you to accept a license agreement.&lt;/P&gt;&lt;P&gt;If you already accepted the license for those files, you can copy the files into your Linux/Unix system and proceed with the labs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-JC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Aug 2019 14:22:34 GMT</pubDate>
    <dc:creator>jc_pacheco</dc:creator>
    <dc:date>2019-08-27T14:22:34Z</dc:date>
    <item>
      <title>Can these tools be configured to run on Linux?</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Can-these-tools-be-configured-to-run-on-Linux/m-p/912443#M1</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Lab notes alude to non-windows platform where in steps 11 and 12 they both start with "If on Windows,"...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Certainly, Git, Python, Tensorflow are all originally from *nix platforms, and there is MCUxpresso for Linux, but&lt;/P&gt;&lt;P&gt;packaging of eIQupdate as a .exe file means that a Linux install is either discouraged or difficult.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ask this because I have been unable to get MCUxpresso to talk to either of my 1060 or 1064 EVK boards although both the OSX and Linux versions talk to them just fine...&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Guidance?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 14:12:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/Can-these-tools-be-configured-to-run-on-Linux/m-p/912443#M1</guid>
      <dc:creator>jtmiii</dc:creator>
      <dc:date>2019-08-27T14:12:44Z</dc:date>
    </item>
    <item>
      <title>Re: Can these tools be configured to run on Linux?</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Can-these-tools-be-configured-to-run-on-Linux/m-p/912444#M2</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James,&lt;/P&gt;&lt;P&gt;The lab can definitely be run in Windows and Non-Windows platforms. Just keep in mind that in order to run the labs, you need to extract the "eIQ Update.exe" file from&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-344227"&gt;eIQ ML Software Clinic - Lab and Software Files&lt;/A&gt;, which is a Windows executable. This is because that is an installer that requires you to accept a license agreement.&lt;/P&gt;&lt;P&gt;If you already accepted the license for those files, you can copy the files into your Linux/Unix system and proceed with the labs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-JC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 14:22:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/Can-these-tools-be-configured-to-run-on-Linux/m-p/912444#M2</guid>
      <dc:creator>jc_pacheco</dc:creator>
      <dc:date>2019-08-27T14:22:34Z</dc:date>
    </item>
  </channel>
</rss>