<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinic中的主题 Yocto project building is failed. ERROR:pango_1.46.2.bb:do_compile</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Yocto-project-building-is-failed-ERROR-pango-1-46-2-bb-do/m-p/1290430#M189</link>
    <description>&lt;P&gt;I'm trying to implement a Yocto-generated image on i.MX 8M PLUS.&lt;/P&gt;&lt;P&gt;Therefore, the following image is built in Yocto project, but an error occurred. Do you know how to resolve this error?&lt;/P&gt;&lt;P&gt;Host PC: ubuntu16.04&lt;BR /&gt;Rev: LF5.10.9_1.0.0&lt;BR /&gt;MACHINE: imx8mpevk&lt;BR /&gt;DISTRO: fsl-imx-wayland&lt;BR /&gt;image: imx-image-full&lt;/P&gt;&lt;P&gt;↓ Details of the error&lt;/P&gt;&lt;P&gt;ERROR: Task (virtual: native: /home/jrcm/source/NXP_iMX8MPLUS/imx-yocto-bsp_v2/sources/poky/meta/recipes-graphics/pango/pango_1.46.2.bb:do_compile) failed with exit code '1'&lt;/P&gt;</description>
    <pubDate>Thu, 10 Jun 2021 05:34:42 GMT</pubDate>
    <dc:creator>HT_MOB</dc:creator>
    <dc:date>2021-06-10T05:34:42Z</dc:date>
    <item>
      <title>Yocto project building is failed. ERROR:pango_1.46.2.bb:do_compile</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/Yocto-project-building-is-failed-ERROR-pango-1-46-2-bb-do/m-p/1290430#M189</link>
      <description>&lt;P&gt;I'm trying to implement a Yocto-generated image on i.MX 8M PLUS.&lt;/P&gt;&lt;P&gt;Therefore, the following image is built in Yocto project, but an error occurred. Do you know how to resolve this error?&lt;/P&gt;&lt;P&gt;Host PC: ubuntu16.04&lt;BR /&gt;Rev: LF5.10.9_1.0.0&lt;BR /&gt;MACHINE: imx8mpevk&lt;BR /&gt;DISTRO: fsl-imx-wayland&lt;BR /&gt;image: imx-image-full&lt;/P&gt;&lt;P&gt;↓ Details of the error&lt;/P&gt;&lt;P&gt;ERROR: Task (virtual: native: /home/jrcm/source/NXP_iMX8MPLUS/imx-yocto-bsp_v2/sources/poky/meta/recipes-graphics/pango/pango_1.46.2.bb:do_compile) failed with exit code '1'&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 05:34:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/Yocto-project-building-is-failed-ERROR-pango-1-46-2-bb-do/m-p/1290430#M189</guid>
      <dc:creator>HT_MOB</dc:creator>
      <dc:date>2021-06-10T05:34:42Z</dc:date>
    </item>
  </channel>
</rss>