<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools ClinicのトピックP1020 NAND flash support, for a board which uses NOR flash for booting.</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/P1020-NAND-flash-support-for-a-board-which-uses-NOR-flash-for/m-p/1287738#M188</link>
    <description>&lt;P&gt;I am looking for information on either u-boot for the p1020 series, or for a linux driver which allows for use of a NAND flash device, in a situation were there is NOR flash used for standard booting processes.&lt;BR /&gt;&lt;BR /&gt;When we implemented the board, we put both types of flash on the board, and now I have need to use the 256M NAND flash device.&lt;BR /&gt;&lt;BR /&gt;Since the original board did not use the NAND flash the u-boot image does not contain any intitialization for it, and it appears that the linux driver does not get the correct OF device tree settings, to 'see' the device.&lt;BR /&gt;&lt;BR /&gt;The current yucktoe package does not go that 'far back' in processors to support getting the current u-boot package and figuring this out.&lt;/P&gt;</description>
    <pubDate>Fri, 04 Jun 2021 21:02:15 GMT</pubDate>
    <dc:creator>johnclark</dc:creator>
    <dc:date>2021-06-04T21:02:15Z</dc:date>
    <item>
      <title>P1020 NAND flash support, for a board which uses NOR flash for booting.</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/P1020-NAND-flash-support-for-a-board-which-uses-NOR-flash-for/m-p/1287738#M188</link>
      <description>&lt;P&gt;I am looking for information on either u-boot for the p1020 series, or for a linux driver which allows for use of a NAND flash device, in a situation were there is NOR flash used for standard booting processes.&lt;BR /&gt;&lt;BR /&gt;When we implemented the board, we put both types of flash on the board, and now I have need to use the 256M NAND flash device.&lt;BR /&gt;&lt;BR /&gt;Since the original board did not use the NAND flash the u-boot image does not contain any intitialization for it, and it appears that the linux driver does not get the correct OF device tree settings, to 'see' the device.&lt;BR /&gt;&lt;BR /&gt;The current yucktoe package does not go that 'far back' in processors to support getting the current u-boot package and figuring this out.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 21:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/P1020-NAND-flash-support-for-a-board-which-uses-NOR-flash-for/m-p/1287738#M188</guid>
      <dc:creator>johnclark</dc:creator>
      <dc:date>2021-06-04T21:02:15Z</dc:date>
    </item>
  </channel>
</rss>